Skip navigation

community

Black Box Network Services

2 Posts tagged with the rack tag
0

Networking equipment—especially servers—generates a lot of heat in a relatively small area. Today’s servers are smaller and have faster CPUs than ever. Because most of the power used by these devices is dissipated into the air as heat, they can really strain the cooling capacity of your data center. The components housed in a medium-sized data center can easily generate enough heat to heat a house in the dead of winter!

 

So cool you must, because when network components become hot, they’re prone to failure and a shortened lifespan. Damage caused by heat is not always immediately evident as a catastrophic meltdown—signs of heat damage include node crashes and hardware failures that can happen over a period of weeks or even moths, leading to chronic downtime.

 

It’s also important to ensure that individual cabinets used for network equipment provide adequate ventilation. The temperature inside a cabinet is affected by many variables, including door perforations, cabinet size, and the types of components housed within the cabinet.

 

The most direct way to cool network equipment is to ensure adequate airflow. The goal is that every server, every router, every switch has the necessary amount of air no matter how high or low it is in the cabinet. It takes a certain volume of air to cool a device to within its ideal temperature range. Equipment manufacturers provide very little guidance about how to do this; however, there are some very basic methods you can use to maximize the ventilation within your cabinets.

 

Open it up

Most major sever manufactures recommend that the front and back cabinet doors have at least 63% open area for airflow. You can achieve this by either removing cabinet doors altogether or by buying cabinets that have perforated doors. Because most servers, as well as other network devices, are equipped with internal fans, open or perforated doors may be the only ventilation you need as long as your data center has enough air-conditioning to dissipate the heat load. You may also want to choose cabinets with side panels to keep the air within each cabinet from mixing with hot air from an adjacent cabinet.

 

Equipment placement

Don’t overload the cabinet by trying to fit in too many servers—75% to 80% of capacity is about right. Maintain at least a 1.5” clearance between equipment and the front and back of the cabinet. And finally, ensure all unused rack space is closed off with blank panels to prevent mixing of hot and cold air.

 

Fans and fan placement

You can increase ventilation even more by installing fans to actively circulate air through cabinets. The most common cabinet fans are top-mounted fan panels that pull air from the bottom of the cabinet or through the doors. For spot cooling, use a fan or fan panel that mounts inside the cabinet.

 

For very tightly packed cabinets, chose an enclosure blower—a specialized high speed fan that mounts in the bottom of the cabinet to pull a column of cool air from the floor across the front of your servers or other equipment. An enclosure blower requires a solid or partially vented front door with adequate space—usually at least 4 inches—between the front of your equipment and the cabinet door for air movement.

 

When using fans to cool a cabinet, keep in mind that cooling the outside of a component doesn’t necessarily cool its inside. The idea is to be sure that the air circulates where your equipment’s air intake is. Also, beware of installing fans within the cabinets that work against the small fans in your equipment and overwhelm them.

 

Air conditioning

Air-conditioned cabinets keep equipment cool and save energy because you cool just the cabinet and not the entire room or IT center. ClimateCab models are perfect for harsh environments and remote locations without cooling infrastructures.

 

Temperature monitoring

To ensure that your components are operating within their approved temperature range, it’s important to monitor conditions within your cabinets. The most direct method is to put a thermometer into your cabinet and check it regularly. This simple and inexpensive method can work well for small installations, but it does have its drawbacks—a cabinet thermometer can’t tell you what the temperature inside individual components is, it can’t raise the alarm if the temperature goes out of range, and it must be checked manually.

 

Another simple and inexpensive addition to a cabinet is a thermostat that automatically turns on a fan when the cabinet’s temperature exceeds a predetermined limit.

 

Many network devices come with SNMP or IP-addressable internal temperature sensors to tell you what the internal temperature of the component is. And, there are also cabinet temperature sensors that can alert you over your network.

 

The AlertWerks Environmental Monitor System not only monitors temperature within a cabinet, but also humidity, the presence of water or smoke, airflow, and security as well.

 

It’s easy!

Keeping your data and server cabinets cool doesn’t have to be complicated. Just remember not to overcrowd the cabinets, be sure to provide adequate ventilation, and always monitor conditions within your cabinets.

0

Given the heat wave so much of the country is experiencing (deepest sympathy to those readers in Richmond, VA that may experience a heat index of 118 degrees today); we had an itch to talk about cooling. That is, cooling in the data center.

 

Did you know that legacy data centers waste at least 50% of the energy they consume managing heat generated by IT systems? Most data centers are not new; they are housed in buildings that are using practices that could be 20 years old and have not yet caught up with the latest trends.

Fully populated racks can dissipate as much as 7–25 kW of heat per rack. High-end servers can dissipate more than 40 kW per rack. This level of density requires data centers to provide power and cooling densities that exceed typical current capabilities.

Furthermore, most legacy data centers have not been designed to use their maximum capabilities, best practices have not been implemented, and the cooling methods of IT equipment have been considerably less than optimal. This has created a common situation, as identified by the Uptime Institute, where data centers consume 2.0 to 2.6 times the cooling required by the IT equipment, thus wasting energy and power and further reducing the amount of IT that can be housed in the structure.

By implementing best practices and optimizing the performance of the existing air cooling infrastructure, data center operators can improve the performance of the specified cooling infrastructure to 70% efficiency. The question data center owners must ask themselves is if their current air cooling is acceptable at 70% or if they can continue to sustain that performance as computing technologies push power and cooling beyond their current requirements.

What can operators expect from their environment if cooling requirements exceed 12 kW to up to 25 kW per rack? Read our entire Extending the Life of Your Data Center white paper. Or, check out our storage technologies to help keep IT equipment cool and to cut rack power and cooling costs by as much as 50%. Nothing cools like chilled water!

 

Did you know you can reduce your utility bills in other ways, too? Eight ways to reduce power consumption.