Skip navigation

community

Black Box Network Services

2 Posts tagged with the vga tag
0

We sat down with Eric Farkas, Senior Research & Development Engineer here at Black Box, and asked him a couple of questions about what kind of media player is needed for digital signage deployments.

 

There is much confusion in the industry about the kind of “media player” needed for a digital signage deployment. Many screen manufacturers now have PCs embedded into the screen– so is the need for a separate media player less in today’s market?
I think the thing to keep in mind is that it's still a media player either way. You can call it an embedded PC in the display, but it is still a media player. What the screen manufacturers don't necessarily tell you is that built-in media players typically suffer from heat-related issues, have smaller storage capacities, and have less processing power. I think cleaning up the cabling mess by integration does add some value, but losing the freedom to size the hardware resources appropriate to your hardware outweighs it. Also I'm wondering where the guarantee is that this slot will be available on the next generation of displays. If I buy embedded PCs for my signage and a few years from now I need to replace displays due to EoL or I desire to upgrade, can I still use them? External hardware is a pretty definite yes.

 

Doesn’t the embedded PC act as the media player?
Yes.

And don’t some content management software platforms run on Windows, so they need a full PC/player in each screen, not just a "media player"?

That’s a good question, and frankly, a lot of us suffer from the same confusion as those who ask this question. A media player to me is a PC whether embedded or external, and it has all the same attributes one would associate with a PC. To answer the question, complex digital signage requires an operating system and an application running on PC style hardware. There is technology that simply decodes a network stream or plays a loop from some type of flash storage, but I'm not sure this fits the current definition of digital signage. I guess it begs the question, is a DVD or Blu-ray player digital signage? Is a digital photo frame digital signage? If your answer is yes, then the PC is no longer required but if it's no...

There are now a lot of low-cost, high-definition digital signage media appliances that support third party open source digital signage software as well as offer the ability to input from physical media like Compact Flash. But how does the user tell them apart?
There are many aspects that influence the right digital signage system for your needs, and I feel the most important is your definition or vision of what digital signage is. If you want to show pictures, movies, slideshows, or flash and wish to update the content on-site, a physical media player is probably acceptable. Most physical media players cannot incorporate dynamic content (HTML, RSS, widgets, social media, etc.), interactivity (touchscreen, gesture control, facial recognition, etc.), nor can their content be updated through network-based distribution. In most cases, this also eliminates the integration of emergency management systems and localized content as well.

What about output capability? Is HDMI and/or VGA output needed?
HDMI appears to be the front runner as far as adoption, but it is not without its problems. Compatibility and no method to securely fasten it are the leading issues. VESA has officially announced the end of support for VGA and placed DisplayPort as its successor. I believe the ability to support multiple screens on a single bus will give DisplayPort an edge in the future, but it will struggle to compete with HDMI.

What is the role of the media player in remote playlist updating, scheduling, interactive syncing, and even zoning for digital media and advertising needs?
In the simplest terms, the media player displays the media it is presented with or has cached on the display. However, as digital signage evolves, the need for interactivity and localized playout control/content selection is increasing. Synchronization can be important in some environments, but in most cases, good planning and implementation is a better choice than trying to synchronize content on multiple screens.

How should the systems integrator, or end user, start to separate what is needed–and what’s available–in media players for digital signage?
Ask good questions during the design phase and understand the features of the products you sell intimately. By laying out a matrix of features and price levels, the customer can easily pick the level of signage they desire and can afford. Be sure to focus on the features one level above what they pick and stress their value. If these features are truly unimportant, then the customer probably picked well. If there is hesitation, be sure the features hesitated on can be added later or make it clear that only a forklift upgrade will get them to the next level. Some customers realize the potential of digital signage only after it is implemented and the features outside of the original scope are not available in the solution they deployed.

0

When VGA (Video Graphics Array) was introduced by IBM® in 1987 for PC video display, it was a huge improvement over the earlier EGA DB9 connector. VGA, the basic format, supports resolutions up to 640 x 480 with 256 colors. You can find it on many video cards and computer monitors.

 

SVGA (Super VGA), EGA, and later formats continued the drive to provide ever-sharper images and greater color depth. Plus, over the years, VESA standards have brought structure and interoperability to a market that was becoming a mixture of often incompatible SVGA graphics cards.

 

Later formats supported even higher resolutions—oftentimes, rivaling those of digital 1080i and 1080p displays. These later formats include SXGA (1280 x 1024), UXGA (1600 x 1200) and WUXGA (1920 x 1200).

 

Other analog video connectors:

Composite video—Typically presented as a yellow RCA connector, the analog Composite interface has been the standard interface for consumer TV equipment. As its name suggests, Composite video has the luminance (black and white), chrominance (color) and sync pulses combined in one signal.

 

S-Video—Also called Y/C video, S-Video was introduced to overcome some shortfalls associated with Composite video. It’s a less encoded video format, transmitting color (C) and luminance (Y) information separately to produce a sharper image.

 

Component video—This YCbCr connector separates the signal more than S-Video for less interference and improved video. In addition to Y (luminance) signals, it transmits color information as two signals: B-Y (Blue minus luminance, also called Cb or Pb) and R-Y (Red minus luminance, also called Cr or Pr).

 

Go Long! Alternatives to analog video cable extension

Extending video long distances isn’t often possible or practical using standard VGA or coax cabling. With Composite, Component, and other analog video cabling, frequency losses result in deteriorated video quality. Generally, with these cables, the shorter distance the better.

 

Extenders that extend analog video over UTP copper or fiber optic cable solve this problem, enabling you to use backbone or horizontal wiring for your long-distance extensions. Depending on the extender model, video input can be VGA, Component, S-Video, Composite, or BNC coax. They’re a great alternative to using analog video or coax cables, which often can’t be easily pulled through tight conduits and can be more difficult to terminate. What’s really nice is, in most buildings, copper or fiber cabling is already installed to service data communications.

 

Fiber-based extenders provide higher bandwidth and interference-free extensions at distances much farther than copper-type CATx extenders. But there’s the matter of cost. CATx extenders that use cabling and connectors cost considerably less than fiber cabling components.

 

Another thing to consider: Coax- or VGA-cabled extension installations usually require a separate RS-232 or other line for transmitting the control signal for the display—yet another cable to fit into the conduit. CATx cable, however, delivers both the video and control signals through a single transmission medium.

 

But what if you have long runs of coax installed? An extender like the MediaCento RF that uses low-cost RF cabling to broadcast video to remote HDTV screens may be the answer. Supporting both VGA and Component video source input, the MediaCentro RF encodes and modulates signals for single-channel RF transmission over existing coax wiring. The QAM tuner at the screen enables the reception of the high-definition MediaCentro RF channel, so no set-up box or other piece of hardware is required.

 

Resources

Buyer’s Guide: Analog Extenders