Skip navigation

community

Black Box Network Services

5 Posts tagged with the video tag
0

Today’s new digital video formats like HDMI and DVI provide uncompressed digital audio and video with a sharp, crystal-clear image quality. No more flickering and blurry pictures. However, even the best inventions have their limitations. Digital video signals require a huge amount of bandwidth to be transmitted properly. Using low-quality cabling or distribution equipment may lead to problems. Here are the five most common:

 

Problem #1: Black screen (no picture at all).

Possible cause:

  1. Bad cable or one that’s too long, causing either the video signals or EDID/HDCP control signals not to be transmitted properly. Make sure that you use good-quality, high-speed HDMI® cables—they don’t even have to be expensive ones—or try an HDMI extender.
  2. HDCP is unsupported. Does the display support HDCP? DVI displays usually don’t.

 

Problem #2: “Sparkles” in the picture.
Usually caused by:
Too long or inferior HDMI cable. Use a video extender, and/or buy quality HDMI cables from a reputable supplier.

 

Problem #3: RGB color tint.

Usually caused by:

A color encoding issue, a common problem when using a DVI display with an HDMI source. If you’re using a splitter or an extender between your source and the link, make sure it handles EDID correctly—all Black Box® HDMI products do. If possible, force the source (for instance, a Blu-ray player) to output HDMI video with RGB color encoding instead of Component (YPbCr) video encoding.

 

Problem #4: White noise, or just “snow,” for a picture.

Usually caused by:
An HDCP issue. This is actually what the encrypted video looks like. It happens when your display (or any active component, like an extender or a splitter, used in the transmission) doesn’t support HDCP. The display, in turn, isn’t able to decrypt the video stream. Be sure to use equipment that supports HDCP.

 

Problem #5: Flickering, unstable, or blinking image.

Can be caused by:
Electromagnetic or radio frequency interference (EMI/RFI), bad cable, or cable that’s too long. These all can cause issues with HDCP or the video signal, resulting in flickering or the video randomly disappearing then reappearing after a second. The solution: Use certified high-speed HDMI cables instead of standard HDMI cables, or if you need to transmit longer distances, try an extender from Black Box. If you’re already using an extender, try changing to shielded CAT6 solid-core bulk cable.

0

Our VGA Wireless Video Presentation System is back and better than ever! Stop swapping cables every time an individual is ready to present. Go wireless! If you have a meeting room with a VGA projector and you want a roomful of people to have a simple way to share their screens with others, then this affordable, plug-and-play receiver is your solution.

 

This latest version of the popular Wi-Fi receiver not only supports presentation sharing through 4-to-1 split-screen and 1-to-4 projection, it also provides 802.11n Wi-Fi support—delivering up to five times the throughput and greater range of earlier Wi-Fi technology. The 802.11b/g/n compatibility means it can communicate with the latest mobile devices, too. This includes computers, PDA’s or any wireless mobile hand held device running with windows mobile. Plus, the system works as a wireless access point, so laptop users can even access and stream information from the Internet or a wireless LAN.

 

Ideal for college classrooms, auditoriums, business meetings, places of worship, presentations, and video conferencing. It even boasts a range of 300 feet and includes a kit that contains the necessary equipment for wall mounting. For more information on this simple way to improve collaboration in large meeting rooms, go to blackbox.com/go/VPS or watch the demo video below.

 

0

When VGA (Video Graphics Array) was introduced by IBM® in 1987 for PC video display, it was a huge improvement over the earlier EGA DB9 connector. VGA, the basic format, supports resolutions up to 640 x 480 with 256 colors. You can find it on many video cards and computer monitors.

 

SVGA (Super VGA), EGA, and later formats continued the drive to provide ever-sharper images and greater color depth. Plus, over the years, VESA standards have brought structure and interoperability to a market that was becoming a mixture of often incompatible SVGA graphics cards.

 

Later formats supported even higher resolutions—oftentimes, rivaling those of digital 1080i and 1080p displays. These later formats include SXGA (1280 x 1024), UXGA (1600 x 1200) and WUXGA (1920 x 1200).

 

Other analog video connectors:

Composite video—Typically presented as a yellow RCA connector, the analog Composite interface has been the standard interface for consumer TV equipment. As its name suggests, Composite video has the luminance (black and white), chrominance (color) and sync pulses combined in one signal.

 

S-Video—Also called Y/C video, S-Video was introduced to overcome some shortfalls associated with Composite video. It’s a less encoded video format, transmitting color (C) and luminance (Y) information separately to produce a sharper image.

 

Component video—This YCbCr connector separates the signal more than S-Video for less interference and improved video. In addition to Y (luminance) signals, it transmits color information as two signals: B-Y (Blue minus luminance, also called Cb or Pb) and R-Y (Red minus luminance, also called Cr or Pr).

 

Go Long! Alternatives to analog video cable extension

Extending video long distances isn’t often possible or practical using standard VGA or coax cabling. With Composite, Component, and other analog video cabling, frequency losses result in deteriorated video quality. Generally, with these cables, the shorter distance the better.

 

Extenders that extend analog video over UTP copper or fiber optic cable solve this problem, enabling you to use backbone or horizontal wiring for your long-distance extensions. Depending on the extender model, video input can be VGA, Component, S-Video, Composite, or BNC coax. They’re a great alternative to using analog video or coax cables, which often can’t be easily pulled through tight conduits and can be more difficult to terminate. What’s really nice is, in most buildings, copper or fiber cabling is already installed to service data communications.

 

Fiber-based extenders provide higher bandwidth and interference-free extensions at distances much farther than copper-type CATx extenders. But there’s the matter of cost. CATx extenders that use cabling and connectors cost considerably less than fiber cabling components.

 

Another thing to consider: Coax- or VGA-cabled extension installations usually require a separate RS-232 or other line for transmitting the control signal for the display—yet another cable to fit into the conduit. CATx cable, however, delivers both the video and control signals through a single transmission medium.

 

But what if you have long runs of coax installed? An extender like the MediaCento RF that uses low-cost RF cabling to broadcast video to remote HDTV screens may be the answer. Supporting both VGA and Component video source input, the MediaCentro RF encodes and modulates signals for single-channel RF transmission over existing coax wiring. The QAM tuner at the screen enables the reception of the high-definition MediaCentro RF channel, so no set-up box or other piece of hardware is required.

 

Resources

Buyer’s Guide: Analog Extenders

0

How you set up your network for voice, data, video, and audio transmission can mean the difference between a network that operates efficiently and transparently to users and one that’s slow and tedious.

 

Think of your network as a river of data. You have a steady current of data moving smoothly down the channel. All your network users are like tiny tributaries branching off the main river taking only as much water (bandwidth) as they need to process data. When you start to multicast voice, video, data, and audio over the LAN, those streams suddenly become the size of the main river. The result is that each user is basically flooded with data and it becomes almost if not impossible to do any other tasks. This scenario of sending transmission to every user on the network is called broadcasting, and it slows the network down to a trickle. But there are network protocol methods that alleviate this problem.

 

Unicasting vs. multicasting

Unicasting is sending data point-to-point, from one network device to another. Multicasting is transmitting data from one network device to multiple users.

 

When multicasting with Layer 2 switches, all attached network devices receive the network packets, whether they want them or not. When you multicast with Layer 3 switches (with multicast support), you send the network packets to only the exact client/receives who want them. You control where the river of data goes and put up locks to keep the river out of other user streams.

 

Unicasting technical details

Every device on a network has a MAC address and an IP address. In a typical network, we usually see a lot of unicast packets going from one device to another. The unicast packet header will contain the destination IP address of the device it needs to reach and typically resembles a Class C IP address ranging from 192.0.0.0 all the way to 223.255.255.255. These unicast packets are generated from a single source and are sent to a single receiving device. The source nodes, also known as network switches and routers, have a built-in routing table, which enables the unicast packet to find its destination by taking the shortest hop from one switch to another.

 

In a typical unicast network, you’ll find that Layer 2 switches are used because they’re very cost effective and can easily support these types of network communications.

 

Multicasting: Layer 2 vs. Layer 3 switches

In multicasting, a single device will transmit a network packet out to many, but not all, devices that are actively tuned in and want to receive the packet. A multicast IP address is a Class D address, which means it has a range of 224.0.0.0 to 239.255.255.255. The IP address range typically designated for multicasting protocols is between 224.0.0.0 through 224.0.0.255.

 

Multicasting with Layer 2 switches. Because a multicast head does NOT have a destination IP address, an average network switch (a Layer 2 switch without supported capabilities) will not know what to do with it. So the switch sends the packet out to every network port on all attached devices. When the client or network interface card (NIC) receives the packet, it analyzes it and discards it if not wanted.

 

Multicasting with Layer 3 switches. To solve the problem of sending packets to every device on the network, use a Layer 3 switch that supports IGMPv2 or IGMPv3 and packet forwarding (Internet Group Management Protocol [IGMP] supports multicasting on the physical network level).

 

The Layer 3 switch multicasts network packets only to devices that have tuned into the stream. It does not send the multicast packets to devices that don’t want it. This makes multicasting with Layer 3 switches much more efficient than with Layer 2 switches.

 

The value of IGMP and Layer 3 switches

If you had a Layer 2 switch that didn’t support IGMPv2 or IGMPv3 snooping, the switch would be able to handle only a few devices sending multicasting packets.

 

Layer 3 switches with IGMP support, however, are smart enough to know who wants to receive the multicast packet and who doesn’t. When a client/receiving device want to tap into a multicasting stream, it responds to the multicast broadcast with an IGMP report. That’s the equivalent of saying, “I want to connect to this stream.” The IGMP report is only sent in the first cycle and initializes the connection between the multicast stream and receiving device.

 

If the client/receiving device was previously connected to the stream, it sends a grafting request to the Layer 3 switch. Grafting enables the IGMP-supported switch to remove the temporary block on the unicast routing table. The switch can then send the multicast packets to newly connected members of the multicast group.

 

When the client/receiving device no longer wants to receive the multicast packets, it sends a pruning request to the IGMP-supported switch, which temporarily removes the device from the multicast group and stream.

 

Basically what we’re saying is…

If you plan on using multicasting protocols on your network, make sure you have routers or Layer 3 switches that support the IGMP protocol. Without this support, your network devices will be receiving so many multicasting packets, they will not be able to co communicate with other devices using different protocols, such as FTP.

 

Also, if you’re planning to send video from multiple sources over a LAN, a feature-rich, IGMP-supported Layer 3 switch also will give you the bandwidth control you need.

 

Be sure to configure the IGMP-supported switches for the particular application. Most Layer 3 switches right out of the box have IGMP support disabled.

Resources

Global Centralized KVM Server Management White Paper

Video: Go KVMoIP to save time, money

KVM Selector (A tool to configure your ultimate ServSwitch KVM solution)

0

Simplify the routing of high-resolution video between multiple sources and DVI display devices with new DVI-D Matrix Switches (XPT-DVI4X4, XPT-DVI4X8, XPT-DVI8X4, XPT-DVI8X8). Available in 4 x 4, 4 x 8, 8 x 4, and 8 x 8 matrix port configurations, these DVI single-link switches help you save time because they eliminate having to disconnect and reconnect different DVI video sources for output to LCDs, plasma screens, and projectors.

 

 

Any input can be directed to any output, making the switches ideal for point-to-point and multipoint applications. They’re particularly ideal for frequently rerouting source input for output to multiple digital signage screens. Switch ports electronically from a remote RS-232 console or from an Ethernet TCP/IP network, or manually using front-panel buttons.

 

 

These switches support resolutions up to 1920 x 1200 at 60 Hz, including HDTV resolutions of 720p, 1080i, and 1080p. Deploy them for high-definition video switching in multimedia conference rooms, healthcare imaging applications, and command and control centers with a number of high-resolution monitors.

 

 

They can also be used with the newest panels featuring EDID capabilities, with each input port on devices supporting EDID emulation. Plus, they support HDCP feed-through in point-to-point applications.

 

 

What’s more, the switches also enable you to set up extended DVI cabling runs to source devices. A built-in equalizer preserves video quality on switch-to-source runs as long as 114.8 feet (35 m), for instance, from the switch to servers or media players backracked in a secure room.

 

Questions? Contact our FREE Tech Support at 1-877-877-2269 for an expert in less than 20 seconds.