Skip navigation

community

ChallengeDownUnder

4 Posts tagged with the prototype tag
0

CCHS GGHC: CCHS element14 group

 

Team moment of the week

We had a great evening last night rounding out the project, with most of the team members able to join in on the last tasks to complete the project. There were many highlights during the evening, including getting the final product working in its nice shiny enclosure:

http://geekscape.github.com/aiko_arduinolab/openlab_device.jpg P5036256sml.JPG

 

however the highlight of the night was team member Rob's unveiling of the secret experiment: a Ruben's Tube:

 

P5036203sml.JPG

we've designed OpenLab's hardware so that it will be able to drive a Ruben's Tube from the available outputs:

 

 

Key Thoughts and Observations

We considered a number of times whether our ambitions had gotten the better of us, and perhaps they had. But in the end, we've gotten to a first alpha prototype product, with lots of potential to expand it. This is by far the most feature rich and complex project we have undertaken together as a hackerspace. It stretched our skills as a group and as individuals. We found that our core team members were severely taxed, and it took the efforts of the entire team to get us to a final working product. A stellar effort from all the crew: congratulations everyone, but particular thanks go out to our friends at Freetronics for their support and assistance, and to the team: Andy, Luke, Marc, Stuart, Antoinette, Bernd, George, Rob and Clifford for your hard work and commitment.

 

We're very excited by what we've built, and the potential to improve it going forward. We're already looking at presenting this to the local Science Teachers association.

 

 

 

 

Next Steps and post-project activities

There are various activities we intend to investigate, including:

     - Organise further school trials.

     - Establish a way for schools to purchase the project in various forms, including as a partially built kitset, or as a complete finished product ready to use.

     - Present to the local Science Teachers Association conference

     - Improve the hardware in second version update

 

IMG_1848 (Medium).JPG

 

Spotlight: The OpenLab

Our finished product is a general science and physics project platform, usable by schools to more easily conduct and monitor various experiments. Our working title during the competition was ArduinoLab, but as you can see in the pictures we've now settled on the name OpenLab.

 

P5046292sml.JPG

 

The OpenLab platform provides a number of things:

 

- A damage proof, protected, experimentation environment where the circuits are designed to protect the inputs and outputs from damage.

- An onboard Lithium Ion battery, providing mobility and portability of the lab around the classroom.

- Charging of the portable power source over USB, enabling the OpenLab to be powered and charged from a computers USB port, from a multi-port USB hub, or from mains power using an adaptor wall plug with USB socket.

- Graphics LCD display, enabling waveforms to be displayed.

- Intuitive navigation using buttons and control knobs, using a soft-label menu system.

- A built-in Arduino: an Atmega 28p, lowering the cost of purchasing the microprocessor separately.

- A Xbee header, enabling the addition of communications features using any of the "bee" form factors modules: Xbee, GPSBee, RFbee, BluetoothBee, etc.

- A multi-tasking screen/ application handling framework.

- The ability to monitor multiple sensor inputs and to generate multiple outputs simultaneously.

- based on a design using easy to source and well known components, enabling the project to be replicated internationally.

 

P4306101sml.JPG

P5036154sml.JPG

 

P5036219sml.JPG

P5036241sml.JPG

 

Documentation

We'v used this blog pretty much exclusively for our updates and information on our project.

We've also uploaded some video to the agentsilverfox FTP server, so keep an eye out for that footage appearing at some stage.

In a few weeks we'll have a project entry updated on the Hack Melbourne Project Page

If you'd like to follow our progress on the software, have a look at the software repository here on github.

And github also provides a walkthrough of the software structure, use, etc.

And if you want to review the hardware work, or see where version two goes next, see the previously mentioned hardware design repository here on github.

And and walkthrough of the hardware structure was in a previous blog post.

 

Closing comments

Well, it's been tiring but it's been a real blast! Congratulations to all the other Hackerspace teams who have joined in the challenge: we've enjoyed reading about your projects and your progress. We hope you've enjoyed hearing about ours just as much.

 

And if you're ever in Melbourne, come and look us up. And if you can't make it in person, drop by the website from time-to-time to see what we're up to, or look us up on IRC.

 

 

Happy Hacking from the Connected Community HackerSpace (Melbourne)

http://hackmelbourne.org

0

CCHS GGHC: CCHS element14 group

 

Team moment of the week

Phew! What a crazy, fun-filled and tiring week it's been! And so many great moments too I'll pick a few to highlight.

 

The PCB's arrived! Straight after the Easter break, on Wednesday 27th April, the courier arrived and we were holding our sleek looking boards in our hot hands. We kind of felt like proud parents, and I guess it's true we're biased, but aren't these just the greatest looking bundles of joy?:

 

P4275882sml.JPG

 

It's been frustrating having the hardware delay, but it was great to finally be able to jump into populating the first few boards and begin testing our prototype software. We proceeded to make up for lost time with a week of late nights and grabbing any spare moment we could find during our regular daily lives.

 

P4275920sml.JPG

 

 

Progress this week

Project: Lots of movement on all fronts. Hardware assembly, software implementation, enclosure package layout and design, and documenting the project. We had a few parts we ordered from element14 that still haven't arrived, however they're not critical components (an SMT trimpot for the LCD contrast and some 102 caps).

 

Requirements: Our main requirements focus has been to review the enclosure layout for usability. We've settled on a first prototype layout that works, however we'd like to make further improvements to simplify the user experience. We've also refined the software requirements a little based on the feedback and learnings from working with the LCD prototype boards, and we have needed to flex a little from our original software requirements to reflect the compressed timeframes due to the delayed hardware arrival. .

 

Design: We're taking the initial outline software deisgn and itereating that through design --> build --> test cycles, working collaboratively using github. We've also taken a similar approach with the case layout work, running through design-->paper prototype-->walkthrough-->refine & adjust cycles.

 

Build: We got the first few Motherboards assembled, followed by the Daughter and Buttonboards. We have a nice framework running to handle the various "applets" that the lab will run, with a number of prototype applications running in test mode. We have also completed the front-panel artwork for the enclosure, and have begun the final work on the case to mark it up for drilling.

 

Plan & Schedule: We only have a couple of days left to go! Still lots to do, and we're all feeling under immense pressure. We've settled for a reduced set of functions from those we originally envisaged, but that simply reflects a reduced set of software: something that can be improved with updates after the competition.

 

P4276080sml.JPG

 

Key Thoughts and Observations

We're finding we have too many concurrent threads to close out in the remaining days. We can see the end in sight, but there are a number of tasks to complete, none of which are particularly problematic by themselves, but leave uncertainty around the final product. We'll be working very hard to make the deadline, and feel confident we'll make it with a first alpha protype version of a product that has lots of real-world applicability and potential.

 

Here's a look at the enclosure artwork that team members Marc and Antoinette have been working on, and a first enclosure cut to suit

IMG_1805 (Medium).JPG

IMG_1811 (Medium).JPG

 

Next Steps and post-project activities

There are various activities we intend to investigate, including:

     - Finish the basic application environment, with a couple of example applications

     - Finish the enclosure cutting and assembly.

     - Attch and tst the secret experiment we spoke about in an early blog post.

 

P5026142sml.JPG

 


 

Spotlight: Surface-mount soldering

We had fun with help from our friends at Freetronics, doing a couple of solder mount assembly sessions. the first focused on getting the few boards poulated and ready for testing, the second a demonstration/ tutorial for the general hackerspace membership to be involvd in.

 

P4275985sml.JPG

We used solder paste, an stereo microsope and a toaster oven to make some magic happen. It really isn't as hard as folks might think it is to do SMT work, and we'd strongly encourage everyone to give it a go and learn the requisite skills.

 

P4276076sml.JPG

P4275966asml.JPG

 

 

 

Well, one more post to go! See you soon!

 

 

Happy Hacking from the Connected Community HackerSpace (Melbourne)

http://hackmelbourne.org

0

CCHS GGHC: CCHS element14 group

 

Over the last couple of weeks, the electronic design for our microcontroller-based electronics experimenter's instrument has been completed, I've completed the PCB layout and sent the CAM files off to the PCB fab, we've sorted out the BOM lists, and we've ordered a whole bunch of components from our friends at element14 and Digi-Key.  We've sourced essentially all our components from element14 and Digi-Key... but these vendors aren't the only vendors that sell the components needed... these are almost all very common components available from many suppliers.

 

ArduinoLabMotherboardPCB.png

Above: The PCB layout of the main board.

 

Right now, tentatively, its working title is the ArduinoLab. (I'm considering calling it the Mystik Spiral project... because we're thinking of changing the name. )

 

So, I thought that now, while we're waiting for the delivery people to bring our PCBs after the Easter holiday, might be a good time to look at the electronics designed by Marc Alexander and myself, and go over how it all works.

 

Microcontroller

 

At the heart of it all we have a microcontroller... the Atmel ATmega328. This is undoubtedly a familiar microcontroller to many readers. It is, of course, the same AVR microcontroller used as the basis of the Arduino system, in most cases. This widely available, popular microcontroller is surrounded by several other core components of the microcontroller system on the system's main "motherboard".

 

Microcontroller.png

 

To give us the most flexibility when it comes to packaging up the finished PCBs into an enclosure, and because I'm using the free "light" license for Eagle, which limits the PCB dimensions, our best option actually turned out to be dividing up this system across several PCBs, instead of putting it all on a single monolithic PCB. We'll take a look at these peripheral PCBs in a moment.

 

The AVR is running at a clock frequency of 16 MHz... the same most Arduino devices. This board is intended to be fully compatible with the Arduino system - the Arduino bootloader and the Arduino IDE - for easy programming and software development. And of course, just like Arduino, everything is open-source too, for hackability, repairability, and expandability, as well as for the educational value of open-source. We're writing firmware for the device based on the Arduino system, running on top of the Arduino bootloader, so the firmware is easy to understand and easy to change.

 

Because this board is almost entirely based on compact surfact-mount components, a QFN-32 version of the ATmega328 is used. This has the added advantage that it gives us a couple of extra I/O pins - the AVR's 7th and 8th analog inputs. These inputs are present on the chip die, but they are not broken out to pins on the DIP version of the chip.

 

Included on the motherboard is the popular FT232RL USB virtual-UART IC, just like on the Arduino Duemilanove, providing USB connectivity for programming and communications with your PC. We've also included a reset button for the AVR, too. A USB mini-B connector is used for the USB interface on this board instead of the traditional USB 'B' connector, which is excessively tall and bulky.

 

For even more expandability, flexibility and hackability, I've also added some pads surrounding the AVR, in a standard Arduino "Shield" footprint. This provides lots of exciting hacker-friendly potential for expansion and access into the microcontroller pins!

 

Power Supply

 

So, basically, it's just like an Arduino, right? Well, not exactly. There are some further features we've implemented in this case, whilst still maintaining a high degree of Arduino compatibility.

To start with, we need some portable power. I've included a 3.6 V lithium-ion AA cell on the board, for convenient wireless power and portable operation, with no wall-warts, power cables or batteries dangling off. A Microchip MCP73831 Li-ion charge management IC is used to charge the cell from power supplied by a USB host device, or a 5 V mains power supply (a plugpack or wall-wart) with a USB connector.  There is no need to remove the battery and plug it into a battery charger - you simply plug it into a USB host, and it charges the battery. User friendly, no-fuss, uninterrupted portable power that just works - just like your laptop or cellphone.

 

The lithium cell's nominal 3.6 V is stepped up to 5 V using a Texas Instruments TPS61202 buck/boost converter IC. This allows us to run the microcontroller's positive supply rail at 5 V, which is a common, familiar choice for most Arduino-like devices, and gives us a little more flexibility than a 3.3 V supply rail. One small disadvantage of this device, however, is that it is a very small QFN-10 SMD package. Probably going to have to bust out a stereomicroscope for this one.

 

Since the MCP73831, the FT232RL and the TPS61202 are only available as surface-mount devices, we could really make use of the extra 2 ADC channels on the ATmega328, and we need to fit a relatively large amount of electronics onto a relatively small PCB, we have decided to make the system's motherboard almost entirely built from SMD components.  For realistic electronic engineering projects today, with nontrivial devices, one needs to learn to stop worrying and love surface-mount technology, because you just can't get many interesting and valuable ICs in DIP packages.

 

PowerSupply.png

 

Graphical Display

 

Next up, we've got the LCD display. Here, we've decided to step up a little from our traditional choice of the common HD44780 character displays, and we've chosen a nice little 128 x 64 graphical LCD based on the common KS0108 chipset, with white images on a blue backlit background. In fact, with a little shopping around in Asia, we've found that these graphical LCDs are no more expensive than similar 20x4 HD44780 alphanumeric LCD display modules.  But we don't have very many spare pins to play with on our AVR... so how are we going to wire up this LCD display, with its 8-bit data bus and several extra control lines compared to a traditional HD44780? In order to do more with less microcontroller pins, I've used a cascaded pair of cheap and readily available CD4094 8-bit shift registers (or HEF4094... or whatever. You could use any 4094 from one of the different digital logic families), to let us latch the data and instructions out to the LCD display in a serial fashion, using relatively few microcontroller pins.

 

GraphicsLCD.png

 

We're going to write some modified KS0108 libraries which are compatible with existing Arduino libraries for KS0108 displays, so they can be plugged into existing programs, but which drive the LCD via the shift registers. This is relatively slow, but saves many microcontroller pins for other uses.

 

The KS0108 128x64 LCD displays we are using are essentially the same as those used for ladyada's delightful MONOCHRON clock. This gives you a good idea of what they look like:

 

contrastmid_t.jpg

(This image belongs to Limor Fried and Adafruit Industries. Used in good faith. Thanks!)

 

Lots of interesting peripherals

 

A header footprint for a Digi XBee 802.15.4 module (or any compatible 3.3 V serial module, such as those GPS, Bluetooth and RF communications "bee" modules available from Seeed Studios) and a corresponding 3.3 V regulator are also available on the board, as is a piezo buzzer for audible feedback to the user.  We've also got a digitally-controlled adjustable DC voltage output. MOSFET Q1 is switched by the microcontroller, and the resulting PWM waveform is smoothed out with the big-ass capacitor C2. Shunt resistor R11 lets us use the AVR's ADC inputs to measure the current flowing in the output circuit. This simple low-current power supply is really convenient for all kinds of electronics and physics experiments. Suppose that we want to measure the V-I curve of a diode. Well, over a certain range at least. We can program the system appropriately, attach the diode, and sweep the positive bias voltage from 0 to 5 volts while we're measuring the current flowing, and we can send the result to a plot on the graphics LCD! (Well, theoretically at least. I haven't tested this yet.)

 

Analog Data Acquisition

 

We've also got a couple of potentiometers for analog input from the user, as well as a couple of terminals for analog voltage measurements from external circuits or devices. To make sure that nothing gets blown up by students who are experimenting, these analog input ports are attenuated in a 4:1 ratio by voltage dividers, and clamped with 5.6 V zener diodes, making these inputs nicely hardened to prevent damage to the unit. The main 5 V rail is also clamped to 5.6 V by a 5 W zener diode to make sure that the ICs cannot be damaged if an excessive voltage is applied to the 5 V rail. Because the ADC inputs are attenuated in 4:1 ratio, the maximum analog voltage that can be measured by these analog inputs is approximately 20 V.  One of these digital inputs is connected to both a digital input on the AVR and an ADC input, so we can do things like pulse counting and digital data recording in the digital domain, as well as the measurement of analog signals. Lots of possibilities for experiments and educational activities!

 

Lots of buttons to push

 

We've also got some other bits and pieces, on the peripheral PCBs.  We've got a set of six pushbutton switches, for user input, control and navigation through the software menu system displayed on the LCD. These six pushbuttons are connected through a string of resistors, forming a voltage divider with an output voltage that changes as different buttons are pressed. By reading this voltage with of the the AVR's ADC inputs, we can receive input from a whole bunch of pushbuttons using only a single microcontroller pin.  This simple pushbutton pad is on its own little PCB - and this design is one that I suspect will probably have future value for all kinds of different microcontroller and Arduino projects. This board is connected back to the main board using three wires - the 5 V rail, ground, and the analog output. Since the component density is not especially high on this board and no specialised components are used, common through-hole components are used exclusively on this board, and it is a single-sided board, making it relatively simple even for beginners to solder together, adding another aspect of potential educational value.

 

PushbuttonPCB.png

 

Digital Outputs

 

The final one of the three PCBs in this system contains three digital open-collector transistor outputs, and an output for analog waveform synthesis. The main reason that a separate PCB was used here is because of the limitations on board dimensions in the free-as-in-free-beer "Light" edition of CADsoft Eagle, which I used to lay out the PCBs.  Three of the AVR's PWM-capable output pins are bought out to three BJTs, with 1 k pull-up resistors that be switched on and off, allowing either digital outputs or true open-collector outputs. 1N5819 diodes are used in the pull-up part of the circuit for protection of the circuit, preventing the 5 V rail from being pulled up too high if the pull-up switch is closed and an excessively large voltage is applied to the output. An 18 ohm resistor is included in the emitter to protect the transistor from overcurrent, and a 1N4004 diode is connected to the output to protect the transistor from back-EMF from an inductive load.

 

TransistorSwitch.png

 

Analog Synthesiser

 

One of these PWM output channels also has a second function - it is also used for analog waveform synthesis. An input PWM signal is filtered through a second-order low-pass RC filter, creating an analog waveform. A second-order Chebyshev LC filter might have a bit sharper transfer function here, but resistors are much cheaper and smaller than inductors, as a rough general rule, and the RC filtering gives good enough performance characteristics for our purposes.  To synthesis sinusoidal waveforms, for example, a sine lookup table will be pre-computed and incorporated into the microcontroller firmware, avoiding the relatively computationally intensive task of calculating sines in realtime.

 

DDS.png

 

The analog output is then buffered with a voltage follower, an Burr-Brown OPA340 rail-to-rail opamp. A rail-to-rail opamp is really valuable here, since we only have a  unipolar 5 V power supply. An AC coupling capacitor can be switched into the circuit to remove any DC offset - or bypassed if some DC component is actually desired. Another toggle switch is used on the output side in order to choose between either the analog synthesis output or the transistor output.  Hopefully these features, along with other hardening and protection measures in the circuit, make this device fairly hard to break electrically.  Like the pushbutton input panel, the nature of the components on this board and the density of these components did not justify the use of surface-mount components, and it uses only through-hole components, making it easy to assemble, even for beginners.

 

I've included portions of our hardware schematics in this post... but of course the entire thing is open-source. If you want to get the whole lot, in full, glorious high-resolution, feel free to check out the contents of my repository for this project over on GitHub - you'll find everything there. If you're not familar with git (and GitHub) it's a great thing to learn - it's not just for greybeard programmers.

 

Happy Hacking,

 

Luke Weston,

Connected Community Hackerspace, Melbourne, Australia.

http://hackmelbourne.org

0

CCHS GGHC: CCHS element14 group

 

Team moment of the week

With the exception of the PCB's, we finally got hold of the hardware components! It was kind of exciting to see all the little packages arrayed before us: it was kind of like Christmas (except it was Easter). In particular, the much anticipated arrival of the LCD's was a big hit: they're nice displays

P4225857sml.JPG

 

Progress this week

Project: Unfortunately, the schedule woes continued to plague us this week. The PCB's didn't make it to us prior to Easter. This meant the prototype hardware rigs took on increased importance as an enabler for software development. We managed to get up and running on various fronts: the software work, the hardware prototypes and we made a start on reviewing the enclosure layout. We also obtained all the remaining hardware components with the exception of the potentiometers (we can source those locally).

 

Requirements: We're exploring usability concerns around the enclosure and software layout and navigation. Further exploration is underway of the experiments we'll use to demonstrate the Lab.

 

Design: This week, the design effort shifted to focus predominantly on the software. We had an excellent planning and design session Tuesday night, and began working through the activities to realise the first key design elements over the Easter weekend.

 

Build: Given the situation with the PCB's, the prototype rigs became critical items. We completed these in short order, constructing a couple of different rigs. We bought a few additional through-hole components to make breadboarding the rigs easier: these will be replaced by surface-mount equivelants on the final PCB's. We also came up with the idea of using Arduino Pro Mini's for the breadboard rigs in the absence of the 328p's on the PCB's: more on that later.

 

Plan & Schedule: Despite our best efforts, the PCB's didn't arrive before the Easter long weekend. The disappointing news was that by Thursday they'd made it as far as Sydney - so close, yet just far enough to #fail . By mid week, it was looking likely they wouldn't make it, so we began planning alternative strategies for the Easter weekend using prototype hardware rigs and focusing on software development. We'll have a good chunk of time during the final weekend of the challenge to complete hardware assembly, as this is our regular scheduled monthly hackerspace weekend meeting. However, we now have a large number of concurrent tasks on the go that all need to come together smoothly in the last week. I guess we're not calling it a "Hackerspace Challenge" for nothing .

 

 

Key Thoughts and Observations

We're working in parallel as much as is possible and practical. Tuesday evening was a great example of this with software design planning, initial hardware prototype rig creation and enclosure layout work all happening at the hackerspace concurrently. Andy lead us through the software design thinking, and Antionette took the lead on having a look at the revised enclosure layout. Elsewhere, team member Rob did some great work building a prototype for one of the experiments we're hoping to demonstrate with the completed Lab

IMG_2070_smudge_sml.JPG

IMG_2066sml.JPG

 

The hardware prototyping work continud over the Easter weekend, and Luke got three prototype rigs up and running in collaboration with hackerspace member Clifford Heath. We also established a github repository to enable current, distributed software development work, and Andy and Paul began working together in that repo.

IMG_2074_sml.JPG

 

This concurrent, collaborative activity is extremely important for a few reasons. First, it enables better use of the limited time available on such a short-term, part-time project as this. Second, it enables assumptions to be explored early, and associated adjustments and corrections to be incorporated into the project while there is still time. Third, it enables fantastic collaboration and skill transfer to occur as team members with different skills and experience pair up and work together.

 

We feel strongly that working concurrently on activities by involving multiple team members, enabling collaboration between those team members and offering team members involvement across the breadth activities is a winning combination. It helps us to drive out issues early, learn, have fun and deliver a well-socialised result.

 

Rough Milestones for next week

For week six, we’ll be focused on bringing all the remaining pieces together into at least one completed prototype product. To do that, amongst other things, we'll:

     - Build the first couple of ArduinoLab boards

     - Organise and run a surface-mount build day for the remaining boards

     - Complete the Software development, including testing

     - Take the enclosure layout from prototype through to a first working solution

     - Build the demonstration experiments

     - Organise a school trial at the end of the competition.

 

Spotlight: prototype test boards

As mentioned, we built three prototype test rigs to explore the hardware and enable early test and validation of the software design.

P4225871sml.JPG

 

The first rig included the shift register setup to drive the Graphic LCD. To build this, we picked up some through-hole equivelants of the surafce mount shift registers used on the PCB. To this prototype, Clifford added the button board rig, enabling us to confirm the button design works to generate reliable values for button pushes through the resistor combinations.

P4225865_sml.JPG

 

We also built two rigs using Arduino Pro Mini's that would enable us to explore the existing GLCD Arduino library using direct control from an Arduino. Although this isn't the same as the shift register control we'll be using on the finished PCB, this approach has a few nice benefits. First, we're testing against the same MCU as the target PCB, so we can confirm many elements such as memory use, CPU speed etc. Second, we can confirm the existing LCD library works with this MCU and this LCD. Third, we can get straight into the higher-level application design using the existing functions provided in the library, and then work on an approach to convert the lower-level library functions to work with the shift registers. Team member Andy has been thinking through what needs to be done, and has a good plan of attack to make that happen.

P4225874sml.JPG

 

If you'd like to follow our progress on the software, have a look here on github.

And if you want to review the hardware work, see the previously mentioned repository here on github.

 

 

We're coming into the home stretch, and yes, as previously mentioned, it's extremely busy: even more than we'd expected, if that's possible!

Stay tuned for our final updates!

 

Happy Hacking from the Connected Community HackerSpace (Melbourne)

http://hackmelbourne.org