Load Google Translate Create and manage categories in DEMMEL PRODUCTS iLCD. Removing a category will not remove content.
Create and manage announcements in DEMMEL PRODUCTS iLCD. Try to limit the announcements to keep them useful.
| Subject | Author | Date | Actions |
|---|
Enter your announcement details below, including when you would like it to become active and expire. By default, announcements will become active immediately and expire in 7 days.
Loading...
Owned by: gschattmann
Tags: lcd, display, panel, touch, graphic, tft, demmel, ilcd, intelligent_display, windows_fonts, dcp3080, dcp3050, dpp-ct1060, dpp-ct8048, dpp-ct4827, dpp-ct6448, dpp-ct3224-2, dpp-cts2440, dpp-dts2432, dpp-at3224, dpp-at2412, dpp-atp3224, evaluation-kit, starter-kit, 10.2", 7", 4.3", 3.5", 3.0", 2.8", 4.8"
Group Type:
Members Only
Created: Mar 3, 2011
| Color iLCD Panels | ||
|---|---|---|
| > | 240x320 Pixel with Touch | |
| > | 240x400 Pixel with Touch | |
| > | 320x240 Pixel with Touch | |
| > | 480x272 Pixel with Touch | |
| > | 640x480 Pixel with Touch | |
| > | 800x480 Pixel with Touch | |
| > | 1024x600 Pixel with Touch |
| Monochrome iLCD Panels | ||
|---|---|---|
| > | 240x128 Pixel with Touch | |
| > | 320x240 Pixel with Touch | |
| - PDA Size | ||
| - Diagonal 5.7" |
| Starter/Evaluation-Kits |
|---|
| Accessories |
|---|
| Setup Software |
|---|
| Web site: | http://www.demmel.com http://www.ilcd.info http://www.ilcd.org http://www.ilcd.biz |
| Voice phone: | +43-1-689 47 00-0 |
| Fax: | +43-1-689 47 00-40 |
| Location: | demmel products Radnitzkygasse 43 A-1100 Vienna, Austria |
| Feb. 24, 2011 | ||
| Continuous Innovation of Intelligent Displays iLCD from demmel products at Embedded World 2011 | ||
The innovative iLCD design enables you to store any Windows font, static and animated graphics, text templates and macros on the iLCD controller’s flash memory. By using iLCD technology, electronic developers can develop appliances including a touch panel display with up to 10.2" within a few days even if the application is run on a 50 cent processor. You can quickly and easily realize any formatted text messages, display static and animated graphics or draw frames and lines for to make up an attractive screen layout. All demmel product’s iLCD panels offer USB, RS232, I2C and SPI interfaces. An optional TCP/IP interface board accelerates the development process and connects the iLCD to the net. Color iLCD panels are available from 2.8" (240x320 pixel) to 10.2" (1024x600 pixel) and are subject to constant further development. As a result, the 5.7" iLCD DPP-CT3224-x was replaced by the new DPP-6448 supporting full VGA resolution (640x480). Hence it offers the quadruple number of pixels with nearly the same outline dimensions for the same price. To simply adapt applications, new commands for scaling of coordinates, fonts and graphics are available. Take a look at our new video to see our latest products and learn more about the simple handling of iLCD. We look forward to meeting with you at our Booth 541 in Hall 12 at the Embedded World 2011 in Nuremberg, Germany, from March 1 ~ 3, 2011. |
Demmel News-Archive:
![]() Save Time and Money with iLCD | Cut Your Development Costs and Save Money With iLCD | ||
|
Why iLCD Nowadays in times of esthetic and functional screen layouts, well known by users of mobile phones and organizers, people are expecting an informative and attractive graphic display layout on their heating or machine controls, instead of just a simple text display. The use of proportional fonts and graphical elements, like animated icons, cause very high development costs, and require a costly micro controller with more memory and processing speed to satisfy the additional requirements for the LCD control. Using the iLCD product family dramatically cuts the development costs on one hand, on the other hand, you can still use a low cost micro controller or any SPS, as all required fonts, static and animated graphics, text templates and macros can be easily stored to the flash memory of the iLCD Controller via our free iLCD setup software. Even complex screen layouts can be controlled by sending a few bytes then. | ||
|
|
Need a demo about iLCD ? 1 year ago | by gschattmann |
|
|
|
The advantages and cost saving potential of Demmel intelligent displays 1 year ago | by Alistair Winning |
|
|
|
News 1 year ago | by gschattmann |
|
© 2009 Premier Farnell plc. All Rights Reserved
Premier Farnell plc, registered in England and Wales (no 00876412), registered office: Farnell House, Forge Lane, Leeds LS12 2NE