Skip navigation

community

Embedded Systems

4 Posts tagged with the altera tag
0

Here is a short video that explains the procedure for booting VxWorks OS on Stratix III Dev. Kit using MP32 IP core.

The video does not have audio instructions.  We are in the process of updating the video with audio instructions. 

Coming soon: video with audio instructions.

 

 

 

 

More Information at: http://www.slscorp.com/pages/mp32.php

0

The title should not be a surprise  here in the USB Community since SuperSpeed USB is now in the market.   Still this is a news for developers working on this.

 

Talking  about SuperSpeed USB, the USB 3.0 standard claims that it is 10 times  faster than USB 2.0.  The  theoretical speed is 4.8Gbps (600MBps).   However looking at various  realistic speed test reports made available  by more than one developers,  it has been concluded that 3.2 Gbps  (400MBps) is the maximum achievable  speed for this standard.

 

The   core efficiency is dependent on a number of factors like 8b/10b   encoding, packet structure and framing, link level flow control and   protocol overhead.

 

Various tests performed with SLS SuperSpeed USB core indicate the speed of 400MB/s in an embedded system.

 

At   5Gbps signalling rate with 8b/10b encoding, the raw throughput is   500MBps.  When link flow control, packet framing, and protocol overhead   are considered, it is realistic for 400MBps or more to be delivered to   an application.

 

What speed can I have in my new product with SuperSpeed interface?

 

If  you have this question in your mind, you are at the right place.  One  of our clients evaluating the USB 3.0 core practically achieved the  speed of 2.5Gbps for IN operation and 2Gbps for OUT operation.

 

The raw throughput of 500MBps can be observed on the USB 3.0 Development Board (between FPGA and PHY).  The picture below shows the board:

 

DSC_0504-with-SMA copy copy-1.jpg

 

2Gbps speed is achieved on this board using SLS USB 3.0 Device core.  The block diagram of the core is given below:

 

usb30sfbd.1.jpg

0

Here is a short video explaining how one can create a new design for NAND Flash controller.

 

 

For more information on NAND Flash Controller, you can visit http://www.slscorp.com/pages/iponficntrlr.php

 

OR

 

Contact info@slscorp.com mentioning your query/request for information.

0

Here is a sample application that we have created using the CoreCommander board for mass storage on Altera FPGA.

 

The video given below does not have voice.  You can read the comments and view the mass storage implementation.