Skip navigation

community

Embedded Systems

2 Posts tagged with the codewarrior tag
1

By Jim Trudeau

 

Sometimes real gems are hiding in plain sight. We are bombarded by  data, and who knows what brilliant discoveries we miss in the cacophony  of noise. A friend might point out something. “Hey, have you seen…” and  call our attention to an item. We take a look and, lo and behold, that  magic something emerges – a piece of music, an idea, a book, a tool that  fills a real need. You wonder how you lived without it, and it has been  in front of you all along.

 

FreeMASTER may be such a discovery for you. It has been available in Freescale’s  roster of development tools for years. Really. With almost no fanfare or  publicity, this little gem has been startling discoverers and  generating smiles on the face of its users. So, what is it?

 

FreeMASTER is a real-time debug monitor. Ho hum? Let’s define the  problems it solves. You’re writing software for a real-time system,  like: a motor running an appliance; the engine control in a car; the  sensors in an airbag; the control surface of an airplane; or anything  that has a feedback loop. Now, try to debug that dynamic system  real-time. Yes, sometimes you need to stop the system to study its  state. More often you need to see it operate dynamically, to control it  dynamically, to see why it goes wrong as it works! You cannot do that with a normal debugger. You need FreeMASTER.

 

 

Data visualization

With FreeMASTER you establish a communication channel to the target.  You monitor variables of interest in real-time, at sampling rates you  determine. You can modify those variables real-time, that is, you can  push data down the pipe to the target to modify the behavior of the  system dynamically.

The native data visualization display within FreeMASTER is the  oscilloscope. You can display multiple variables, and have all the  control options you’d expect of a scope.

Figure one shows FreeMASTER tracking two simple variables. One is a  short value rising to maximum and falling to zero. The other generates a  sine waveform by reading data from a table. I changed the step  increment about halfway through to show you that you can push values to  the target.

 

Figure 1. FreeMASTER tracks and displays variable values real-time

Figure 1: FreeMASTER tracks and displays variable values real-time.

 

But it gets much better.

The display area is arbitrarily extensible via HTML. If you master  FreeMASTER, you can add third-party instrumentation “widgets” based on  ActiveX and embed them in the display area. You can wire them up to  variables analogous to the way the oscilloscope works, reading and/or  changing values. In this way you can create as elegant or complex a  dashboard as you like to represent the system you are testing or  demonstrating. This open-ended design makes FreeMASTER an  extraordinarily flexible and powerful tool. Figure 2 is an example  screenshot of an animated display representing engine knock behavior and  feedback control as handled by our Qorivva MCUs based on Power Architecture technology.

Figure 2. The data visualization area of the FreeMASTER tool is arbitrarily extensible

Figure 2: The data visualization area of the FreeMASTER tool is arbitrarily extensible.

 

As they say with Ginsu knives, “but wait, there’s more…”. You can  embed slide shows, presentations, data sheets, or entire packages of  information around a product or a problem. We do it. A really solid  example is the FreeMASTER project for the Tower System for Automotive Sensors that I wrote about here. That has data sheets, block diagrams, and prebuilt scopes for all the sensors, all inside a single FreeMASTER project.

 

 

Data recording

FreeMASTER also implements a data trace capability called the  Recorder. The Recorder uses an on-target buffer to store data readings  and then downloads the buffer to the data display. It captures data at a  higher and more reliable sampling rate than the oscilloscope (near  ten-microsecond resolution). Clearly this can have some impact on the  real-time performance of your application, but the data capture can be  invaluable for analysis. You identify the variables (up to eight) you  want to capture, and specify the size of the on-target buffer.

You also specify a trigger event to start the sample.

 

In the “real time” analysis that you can do with the scope, you see  things as they happen. That is actually a relatively coarse view with a  fair degree of interpolation in the data visualization. You have no  ability to zoom into the data to analyze it at a fine level of  granularity. The sampling rate is not precisely consistent. A lot can  happen during the intervals between the samples. For example, if we were  to pull that same sine wave data at a high increment “real-time,” it  would get pretty ugly. Figure 3 hardly looks like a sine wave at all  and, depending on how fast your data is changing, this display may not  be adequate for you.

Figure 3. Real-time in the oscilloscope has its limitations

Figure 3: Real-time in the oscilloscope has its limitations.


The resolution of the recorder, at microsecond level, is much finer.  In Figure 4 you can see a data trace using the same high increment. That  sine wave looks pretty smooth at millisecond resolution.

Figure 4. The data recorder captures data at fine time resolution

Figure 4: The data recorder captures data at fine time resolution

 

Even still, everything is relative. Figure 5 shows you that you can  zoom in on data. When looking at the data at microsecond resolution, you  can see the stepwise increases induced by the fact that we are pulling  data from a table of values.

Figure 5. A conceptual representation of the FreeMASTER zoom capability.

Figure 5: A conceptual representation of the FreeMASTER zoom capability.

 

All of this should demonstrate that you can use FreeMASTER to study  your data as you need, at the level of detail demanded by your  application. You can also capture the data to a text file for later  analysis in other tools if you wish. Setting up the data trace is typically a matter of configuring the  recorder in FreeMASTER to specify what variables you want to trace. If  you want to change the default buffer size, then you’ll modify a header  file. It is pretty simple stuff.

 

 

Platform support and connections

Real-time data monitoring does not come without some performance  price. It takes cycles to read or store data and push it up the pipe.  But, FreeMASTER has multiple ways of communicating, some of which are  very-low intrusion, such as OSBDM. Others require an on-target driver.  The Table below summarizes platform support and connection protocols.  The BDM connections are very near to zero-intrusion on the running  software. The data trace we were just talking about requires a target  driver.

Table 1. Where and how you can use FreeMASTER.

Table 1: Where and how you can use FreeMASTER.

 

 

Hardware-in-the-loop-simulation

Perhaps the most exciting capability of the tool is that the data  output can be retargeted. Like the design of the data visualization  engine, the data stream itself is not restricted to FreeMASTER. The data  is accessible through an ActiveX interface to any application that can  consume ActiveX services, such as MATLAB®, Excel, Internet Explorer,  PERL, VBScript, Jscript, and so on. What you can do is limited only by  your imagination.

 

Here are two high level use cases involving FreeMASTER feeding data into MATLAB or Simulink.

You might use real-time, real world data rather than theoretical data  to feed input into a complex simulation, and see how the model would  respond.

Alternatively, take a set of identical inputs and run them  simultaneously in both the processor and the model, using FreeMASTER to  stream the results out of the processor. Compare the results from the  two systems to see how the model does against reality, thus establishing  whether the model is valid, and if so, under what conditions.

FreeMASTER enables both of these scenarios for testing models of  highly complex dynamic and non-linear systems. Talk about way cool.

If you’ve read this far, I think I’ve got you hooked. However, here’s one more facet on the gem.

Integrating FreeMASTER with the CodeWarrior tools is simple.

 

Since there is typically an on-target driver involved, you often will  add source code and integrate it into your project. This gives you the  flexibility, as noted above, to do things like change buffer sizes  really easily. When you configure FreeMASTER itself for your  visualization displays, you’ll save the information in a FreeMASTER  project file. I added that FreeMASTER project file into the related  CodeWarrior project by drag and drop, done. Double click inside the  CodeWarrior tools, FreeMASTER launches. Simple and sweet, no need to go  hunting for anything.

True to our overall enablement philosophy, of course you aren’t  required to use a particular development environment. FreeMASTER is a  separate application. You can download it, and the required  communication driver software, here. You can build them in other development environments, like the IAR tools for example.

Also, true to its name, FreeMASTER is complimentary. Seriously. This much functionality at this price?

I told you it was a gem.

0

Earlier this week a friend told us he was having hard times when installing his codewarrior on a brand new PC...

"maybe he were doing something bad" you might think, but no...

After a few tries (and failures), we start thinking this was related to something "else"

regarding, some funny virus scan from his McAfee antivirus appeared each time:

 

Yesterday we found McAfee Antivirus and Code Warrior Special Edition Download forum entry

and we tried its solution... now, our codewarrior installer already did its job, and he is now debugging

 

Basically, the work around is to disable the antivirus while you install the application,

once is installed, you can turn on the McAfee software... pretty easy... right? (after three days) ¬¬°

 

The past couple of days were quite interesting, trying to understand the missing step (you know, we engineers are quite stubborn)

We asked some friends on Freescale, and it seems this bug is affecting Code Warrior 7.2, on all Windows OS versions,

but ONLY with McAfee antivirus...if you find it is affecting some other OS or antivirus, please let us know!