Skip navigation

community

Embedded Systems

1 Post tagged with the i.mx tag
1

By Robert Thompson

 

Last week, Google announced the launch and availability of Android  4.0, Ice Cream Sandwich. The first product that will use the new  operating system will be the Galaxy Nexus from Samsung, which was  created in direct collaboration with Google to enable an optimized  hardware and software experience. Both smartphones and tablets are  expected to follow as Google recombines the OS tree to provide a unified  user experience and toolkit for developers for both form factors.

 

What does 4.0 deliver to the user? For me, it breaks into three main categories: personalization, communication and sharing.

 

The ability to personalize the user interface has always been one of  Android’s main strengths. This 4.0 flavor improves personalization to  allow the user to do things like re-size widgets and flip through the  entire calendar without launching the app. Users can group apps from  home screen folders. A new voice-to-text feature allows for extended  dictation in multiple languages — I’m not entirely sure how this will  compare to Siri, the new iPhone assistant. To meet the needs of users  with tiered or metered data plans, Android 4.0 adds new controls for  managing network data usage. However, the main new addition for  personalization is “Face Unlock,” which is based on facial recognition  and allows the users to unlock their device with their faces.

 

Communication improvements center on the new “People app,” which  connects social networks including Google+, and new camera capabilities.  The camera interface has been redesigned to include built-in panorama  mode and the ability to shoot video in 1080p. New camera features  include “Live Effects,” which allows the user to change backgrounds, and  “Silly Faces,” which speaks for itself. Once the images are stored, the  user is able to edit photos inside the gallery using a range of new  editor tools. These images can also be viewed directly from the home  screen via a new Picture Gallery Widget.

 

The ability to share data and apps from an Android device, a much  sought-after usage model as people look to replace traditional content  services, is enabled a number of ways via Ice Cream Sandwich. Android  Beam, a Near Field Communications technology, allows people to instantly  exchange their favorite apps, contacts, music, videos by just touching  two Android-powered devices together.  Looking to share data with  non-Android devices? Use Wi-Fi Direct, which allows for connection to  other devices via Wi-Fi for sharing of files, photos or streaming video  to audio, enabling for the Android device to be the home hub for  entertainment. Finally, as Android expands beyond consumers, the  addition of Bluetooth Health Device Profile will enable users to connect  with a range of devices from wireless medical devices and sensors in  hospitals, machines in fitness centers and energy management devices in  the home.

 

Most of the reviews of Android 4.0 have focused on the new end user  features (for good reason). These are numerous, and will deliver a much  improved experience over Android 2.3 and 3.0. However, 4.0 also delivers  a number of improvements for developers. To enable developers to  explore and add functionality to their apps, Google has released APIs  for social, calendar, visual voicemail, keyboard, spell checker and text  to speech. The new sharing features from Android to Bluetooth Health  Device Profile also allow developers new ways for end users to interact  with their apps and share between users. Android has not forgotten about  the enterprise with keychain and VPN APIs for managing credentials and  connections, and a new administrator policy for disabling the camera.  However, most importantly is the unified user interface toolkit,  including components, styles and capabilities that will enable  developers to simplify code and resources and streamline development and  deployment of apps across all devices.  This is critical as the fight  for developers across the different mobile ecosystems is far from over.  Android needs to continue to entice developers to work with Android:  Revenue from the Android apps is still a challenge for the majority of  developers, however sweet the latest OS might be for end users.