One of the first components we made was a resistor. Our first couple were VERY simple: 14-gauge solid copper wire soldered to the legs of a standard 1/4W resistor with a glob of polymer clay molded around it.
It worked, sort of. The solder joints were fragile, and there was nothing in the design to keep rotational force on the legs from being transferred directly to the solder joints, which caused them to fail pretty much as soon as they started being used.
We also experimented with a slightly reinforced model, with the resistor being inside a piece of plastic tubing (I'm sorry, I don't know what kind of tube it was, other than to say NOT PVC). We tried to build up a structure around the outside with polymer clay to provide a more convincing physical shape but the plastic softened too much during the bake cycle (polymer clay must be baked at about 275F/150C), deforming and warping and looking in the end not at all like a resistor (or even a cylinder, for that matter).
Team members Karin and Jon finally hit upon what became the best solution: an armature of wood with the heavy gauge wires wrapped around and threaded through holes in the wood. An extruded sheet of polymer clay was wrapped around this and molded into the right shape; smaller strips of polymer clay of the appropriate color were made into the bands to be wrapped around the outside.
Obviously, that's not a resistor- it's an electrolytic capacitor. The principle is the same, though- the main difference is that, with the capacitor, we bring both leads out one end and the resistor they depart in opposite directions.
This technology can be used to form the inside of any small, leaded component: diodes, capacitors, resistors, transistors, etc. Below are some images of various completed and uncompleted components:
So, here we have demonstrated a number of methods for making these components. Naturally, other methods exist: we discussed (and discarded) silicone mold resin casting as too expensive and complex, but that would be a good solution for making a lot of components quickly (perhaps as a maker-based business). Wrapped layers of taped might be a cheap and easy solution, or paper with a single layer of tape on the outside. Pieces of pipe with the component inserted, and subsequently backfilled with plaster of paris, would be a less portable but still very durable and inexpensive option.
In short, anywhere one can find (or bring, or scavenger, or order) the innards of the components, the larger-scale parts can be constructed cheaply and easily.