Skip navigation

community

Currently Being Moderated

Big Board wrap-up 4: Making components (LED)

Posted by UptownMaker on May 2, 2011 11:50:32 PM

Any devotee of electronics will speak fondly of the "blinking LED" experience- that is, the first time a new microcontroller or circuit fires up and you successfully blink an LED. Of course, in order to provide that, we needed to make some large-scale LEDs.

 

We experimented with a couple of methods- the first being a simple piece of nylon rod with the end sanded into a dome and a hole drilled in the bottom that fitted a smaller LED. While this worked quite well, getting a good dome top proved difficult, and reinforcing the bottom and getting good, solid large scale leads was also challenging.

 

We experimented also with a couple of other methods- crumpled paper in plastic wrap, a plastic cup, vacuum forming over a machined mold. None of these things provided the cachet we were looking for. Eventually we settled on using a clear plastic resin to cast a larger LED around a smaller one.

 

The results were spectacular.

 

 


https://lh3.googleusercontent.com/_aPICB9yeZMQ/Tb-DZKHXVLI/AAAAAAAAFMA/J5QSHnX8FTk/s400/DSC03681.JPGhttps://lh6.googleusercontent.com/_aPICB9yeZMQ/TbxUbSxofCI/AAAAAAAAFIU/YUFn3xRAqP0/s400/DSC03658.JPG

Cast LED with the lights off. This is at about 20mA drive current- well

within the drive range of CMOS logic common in microcontrollers, 555

timers, etc.

Three cast LEDs with the lights on. You can see the rough surface finish

which is due to the mold being made from a carved foam positive; some

buffing with a Dremel tool cleans thes up nicely. The top center device is

a common anode RGB.

https://lh4.googleusercontent.com/_aPICB9yeZMQ/Tb-Dt7SZ9KI/AAAAAAAAFPk/EAPbz1LqkQ8/s400/DSC03708.JPGhttps://lh4.googleusercontent.com/_aPICB9yeZMQ/Tb-DhF-ECMI/AAAAAAAAFNg/e1G616cCqL8/s400/DSC03692.JPG

Another construction method: machined nylon rod with a hole in the end

that has the LED inserted into it. This gives nice results but getting the

dome right is hard, as is attaching the thicker leads.

An LED in process. The mold was made by hanging the carved foam

positive dome-down in a plastic cup and up-filling with RTV silicone

around it. Note that the thick leads are pre-attached to the LED;

doing this provides a nice strain relief to the solder joints.

https://lh5.googleusercontent.com/_aPICB9yeZMQ/Tb-Dfrb7jYI/AAAAAAAAFNI/wVnFqa_0CAw/s400/DSC03689.JPGhttps://lh6.googleusercontent.com/_aPICB9yeZMQ/Tb-Dh_kP2gI/AAAAAAAAFNo/Um3tHO7yD14/s400/DSC03693.JPG

The carved foam positive after it was used to make the mold. This was

carved on team member Pete's DIY CNC machine.

Mass cast polyester resin, available from IASCO/TESCO here in

Minneapolis (or online). It's noxious stuff- ventilate well!

 

We are very please with these results; if cosmetic appeal is less important, other methods can be easily used. Another possibility is the use of jumbo LEDs directly; 10mm devices seem to be reasonable available (the white LED inside the nylon rod is a 10mm unit acquired locally at the Ax-man surplus store).

Attributes

Comments (0)