Skip navigation

community

Lighting

2 Posts tagged with the 3d tag
1

UPSD-holographic-display-MIT-buildings.x.png

 

DARPA has announced its "Urban Photonic Sandtable Display" (UPSD) will allow for viewing glasses free 3D images in real time. The display supports monochrome and color. The colors, shown in the image above, represent the various heights of terrain or building structures. Up to 20 viewers can see and interact with the display, allowing for rotation, zoomed, and frozen. The display is scalable going from 6 inches to 6 feet, diagonally. 12 inches of depth can be viewed in the display. For clarity, that 12 inches would represent the height of the tallest structure in the image, if scaled to its maximum.

 

 

The UPSD currently works in tandem with DARPA's3D LIDAR, Light Detection and Ranging, used in the high altitude imaging system LIDAR Operations Experiment HALOE. HALOE is being used in Afghanistan providing high-resolution 3D data. The UPSD will allow for the exploration of that data. Now after completing a 5 year research project, DARPA is taking the UPSD to 3 different military installations to start its use in real world applications.

 

 

Just like in the movies.

 

 

Eavesdropper

 

pic via DARPA.

0

Luneburg-2-300x140.jpg

They said it could be done and now they’ve done it. What’s more, they did it with a GRIN. A team of researchers with the U.S. Department of Energy, Lawrence Berkeley National Laboratory, and the University of California, Berkeley, have carried out the first experimental demonstration of GRIN (for gradient index) plasmonics, a hybrid technology that opens the door to a wide range of exotic optics, including superfast computers based on light rather than electronic signals, ultra-powerful optical microscopes able to resolve DNA molecules with visible light, and ‘invisibility’ carpet-cloaking devices. Working with composites featuring a dielectric material on a metal substrate, and ‘grey-scale’ electron beam lithography, a standard method in the computer chip industry for patterning 3-D surface topographies, the researchers have fabricated highly efficient plasmonic versions of Luneburg and Eaton lenses. A Luneburg lens focuses light from all directions equally well, and an Eaton lens bends light 90 degrees from all incoming directions. GRIN plasmonics combines methodologies from transformation optics and plasmonics, two rising new fields of science that could revolutionize what we are able to do with light. In transformation optics, the physical space through which light travels is warped to control the light’s trajectory; similar to the way in which outer space is warped by a massive object under Einstein’s relativity theory. In plasmonics, light is confined in dimensions smaller than the wavelength of photons in free space, making it possible to match the different length-scales associated with photonics and electronics in a single nanoscale device. Like all plasmonic technologies, GRIN plasmonics starts with an electronic surface wave that rolls through the conduction electrons on a metal. Just as the energy in a wave of light is carried in a quantized particle-like unit called a photon, so, too, is plasmonic energy carried in a quasi-particle called a plasmon. Plasmons will interact with photons at the interface of a metal and dielectric to form yet another quasi-particle, a surface plasmon polariton. “Applying transformation optics to plasmonics allows for precise control of strongly confined light waves in the context of two-dimensional optics. Our technique is analogous to the well-known GRIN optics technique, whereas previous plasmonic techniques were realized by discrete structuring of the metal surface in a metal-dielectric composite,” said Xiang Zhang, a principal investigator with Berkeley Lab's Materials Sciences Division and director of UC Berkeley's Nano-scale Science and Engineering Center.


Zero