Those light-emitting diodes marketed as safe, environmentally preferable alternatives to traditional lightbulbs actually contain lead, arsenic and a dozen other potentially hazardous substances, according to newly published research. “LEDs are touted as the next generation of lighting. But as we try to find better products that do not deplete energy resources or contribute to global warming, we have to be vigilant about the toxicity hazards of those marketed as replacements,” explained Oladele Ogunseitan, chair of UC Irvine's Department of Population Health & Disease Prevention. He and fellow scientists at UCI and UC Davis crunched, leached and measured the tiny, multicolored lightbulbs sold in Christmas strands; red, yellow and green traffic lights; and automobile headlights (non-flaming) and brake lights. Their findings? Low-intensity red lights contained up to eight times the amount of lead allowed under California law, but in general, high-intensity, brighter bulbs had more contaminants than lower ones. White bulbs had the least lead, but contained high amounts of nickel. Lead, arsenic and many additional metals discovered in the bulbs or their related parts have been linked in hundreds of studies to different cancers, neurological damage, kidney disease, hypertension, skin rashes and other illnesses. The copper used in some LEDs also poses an ecological threat to fish, rivers and lakes.
Risks are present in all parts of the lights and at every stage during production, use and disposal, the study found. Consumers, manufacturers and first responders to accident scenes ought to be aware of this, Ogunseitan said. When bulbs break at home, residents should sweep them up with a special broom while wearing gloves and a mask, he advised. Crews dispatched to clean up car crashes or broken traffic fixtures should don protective gear and handle the material as hazardous waste. Currently, LEDs are not classified as toxic and are disposed of in regular landfills. Ogunseitan has forwarded the study results to California and federal health regulators. He cites LEDs as a perfect example of the need to mandate product replacement testing. The diodes are widely hailed as safer than compact fluorescent bulbs, which contain dangerous mercury. But, he said, they weren't properly tested before being marketed as the preferred alternative to inefficient incandescent bulbs, now being phased out under California law. Ogunseitan continued, “I'm frustrated, but the work continues. Every day we don't have a law that says you cannot replace an unsafe product with another unsafe product; we're putting people's lives at risk. And it's a preventable risk."
Eavesdropper