The introduction of LED grow light
LED grow light ,also called plant grow light,at present, the main part of the production was made of LED lighting beeds.lookinging at picture below.and it also be can designed in different colors.
LED grow lights are special lamps and lanterns. According to the importance role of lunar sun to plant,Cidly have developed its LED grow light on base of this principle.
Feature:
1.it have many kind of wavelength, which can coinciding with the spctral of plant photosynthesis
2.It can focus on specific wavelength of light to illuminate balanced plant;
3. Not only can adjust flowering crops and fruit, but also control plant height and nutrition;
4.The system of LED grow light produce less heat, taking up less space ,it can be used for cultivation three-dimensional multi-layer combination system, and realize low heat load and production space miniaturization;
Application:
It is the new production cidly have developed.After application testing,the wavelenght of LED grow light is very suitable for plants grow、blossom and fruit.,as we know, flowers will be fade if we put them in the room for a long time,the main reason it is lack of lunar lighting.,so cidly developed its new technoledgy,by means of the spectrum plants needed ,cidly use the LED grow light illuminate the plant , not only can promote its on the grower,but also can extend the flowering, as well as improve the quality of the flowers.see these picture as an example. We use LED grow light instead of lunar lighting,it also can grow well.
As cidly declare,these LED grow light have three basic advantage .
As the light supplement,the light can enhance its effective lighting time in any time,no matter in the evening or night it can lengthen and control the light which plant needed.
In greenhouse or laboratory ,it can completely replace natural light and promote plant grower.
Working principle
Light environment is important physical factor to the plant development, it is the most important technology to adjustment the light quality and control plant morphological in the field of culture
Miya
Skype:cidly57
Icq:629926940
Email:sales57@cidly.com