Skip navigation

community

Lighting

11 Posts tagged with the lighting tag
0

A wide range of consumer users, the choice of lightingcrystal chandelierscrystal chandeliers  style, without taking into account the effect of the overall home design resulting in a unified style home was destroyed. Fact, the lighting in the home life plays a very important role, whether it is the performance of the light shape,crystal chandeliers crystal chandeliers or a light color can affect the overall effect of home design. Under normal circumstances, a whole series of lights lighting with the form will make the home's overall style is more coordinated, but also play a finishing touch on the overall effect of the design.crystal chandelierscrystal chandeliers

0

Bridgelux-Array-Product-Family-2-300x225.jpg

The speed at which LED lumen output is increasing is staggering. Bridgelux has just released an LED with 135 lumen/W. They were able to get commercial grade performance from a silicon substrate LED for the first time in the industry. A single 1.5mm diameter LED operated at 350mA has output 135 lumens (4730K) at 2.9V. In the industry silicon carbide and sapphire substrates used to create epitaxial wafer, but the materials and process are expensive. Bridgelux went with low cost gallium nitride, grown, wafers from 150 - 300 mm diameters, with a 75% reduction in cost, in comparison.


 

The Bridgelux CEO, Bill Watkins, has this to say about the tech, "The significantly reduced cost-structures enabled by Silicon-based LED technology will continue to deliver dramatic reductions in the up-front capital investment required for solid state lighting. In as little as two to three years, even the most price-sensitive markets, such as commercial and office lighting, residential applications, and retrofit lamps will seamlessly and rapidly convert to solid state lighting.”


 

We will see these emerge in 2-3 years.


 

Eavesdropper

0

CreeMTG.jpgCreeMTG2.jpg

Cree is pushing a "Good Enough, is not Good Enough" campaign in their latest LED lighting replacement. Their goal is to directional MR16 halogen lamps with their XLamp MT-G multi-die LED. These new luminaries are meant for store lighting, museums, art galleries, parks, track, and accent lighting. Able to output 560 lumens at 1.1A (85degrees C), the MT-G can be cranked up to 1525 lumens at 4A (85degrees C, 3000K). Being the first binned a 85degrees C give the luminary the advantage of easy design calculations and fast product development. This definitely makes it more good than just enough. Director of marketing at Cree, Paul Thieken, gives a basic overview, "Until now, LED-based MR16 lamps have been a tremendous challenge in terms of both light output and color consistency, due to their small size and limited capacity for thermal management. Cree developed this LED from the ground-up with applications like these in mind.”


 

Cree also provides a MR16 lamp reference design to help is quick development. Even more "good" than expected. The product is available now!

 


Eavesdropper

0

PhilipsLightingBefore021711.jpg

Original bulb style lighting of the A44

 

PhilipsLightingAfter021711.jpg

LED illuminated A44

 

Philips has donated 294 high brightness LEDs to the Netherlands in conjunction with the RWS (Dutch Highway Authority the Rijkswaterstaat. Used to illuminate 17KM of the A44 highway, the SpeedStar LED solution is the first of its kind. Estimated to save 180,000 kWh per year, approximately energy consumption of 50 households, it saves over 40% of the energy that was used to light the highway's old lamps. “The aim for our collaboration with the Rijkswaterstaat is to implement lighting solutions that both save energy and require less maintenance work on the roads,” comments Frank van der Vloed, General Manager, Philips Lighting Benelux. “Together, we will help provide a safe night time driving experience while helping to lower energy consumption.”


Remote monitoring allows the installation to be dimmable, saving energy during slow periods, and brightened as traffic increases in the evening. Unfortunately, this section of highway is an experiment only at this time. I'm sure the trend will continue. When LEDs are good enough for car headlights, then it's finally bright enough for streetlights.


Eavesdropper

 

source Phillips PR

0

jeweltonedor.jpg

University  of Michigan researcher Jinsang Kim and his team demonstrated a material that shines with phosphorescence in an organic compund. Normally this effect is only seen in artificial metalic compounds, the team's organic crystals radiate a green, blue, yellow, and orange color under ultraviolet light. To show different colors the chemical composition is altered. They are hoping that this discovery will help improve the current OLED (organic LEDs) and SSL. The quantum yield of this new phosphoric device approaches 55%. This is a measure of the efficienct of converting energy to photon. This material is primarily based on Aromatic Carbonyls (carbon and oxygen) that form strong halogen bonds. The molecules get tightly packed in the crystal, supress vibration, and heat losses as the excited electrons move states. The goal is to use this tech in OLED to replace the current use of precious metals in fabrication. Good luck Kim!



Eavesdropper

0

Realizing that consumers have long trusted the Energy Star brand for products that will save them energy and money, the two agencies responsible for the joint program, the U.S. Environmental Protection Agency (EPA) and the U.S. Department of Energy (DOE), currently are taking steps to strengthen and improve it.

 

Last month, for example, EPA released the Final Draft of a new Energy Star product specification for Luminaires, intended to replace the Residential Light Fixtures (V4.2) and Solid State Lighting Luminaires (V1.1) specifications.


This spec has an effective date of October 1, 2011.

 

As before, excluded from the new specs are lighting products such as LED tube lights intended to replace fluorescent lamps and LED fixtures intended to replace linear fluorescent fixtures. Street area and parking garage lights are currently excluded from the Energy Star category but efforts are underway to include these product groups in the future.

 

As well as finalizing the Luminaires specification, EPA has been engaged in the revision of Energy Star program elements for all product categories, so as to meet third-party certification requirements which took effect on January 1, 2011.

 

Until this year Energy Star was a self-declaration program where manufacturers could submit their own test reports directly to EPA. Now, as of Jan 1, the EPA will require that all new submissions from manufacturers participating in the Energy Star program be reviewed by a third party Certification Body (CB), and that qualification testing be performed under specific criteria using EPA recognized labs. The certification body will review and send the report to EPA.

 

Laboratory test results must be produced using the specific models of LED package, LED module or LED array and LED driver (i.e. LED light engine) that will be used in production.

 

Follow up verification testing will have to be conducted annually on 10% of qualified products in the Energy Star program to insure a product’s continued compliance with the requirement after its initial qualification. Each CB will manage verification testing of the product they have certified.

 

These test reports center on IES (Illuminating Engineering Society) LM (Lighting Measurement) -79 (Electrical and Photometric Measurements of Solid State Lighting Products) and LM-80 (Measuring Lument Maintenance of LED Light Sources).


These tests detail such specifications as efficacy, luminous flux, chromaticity coordinates, intensity distribution, CCT (Correlated Color Temperature) and CRI (Color Rendering Index) values at all tested temperatures. Rapid cycle stress tests, temperature and electrical surge and transient protection across all SSL products are also included.

 

As an example consider LED light engine efficacy. Installed in the luminaire the source must now meet or exceed 65 lm/W per LED light engine (Until Sept. 1, 2013) and 70 lm/W per (after Sept. 1, 2013).

 

Similarly, Solid State LED packages, LED arrays or LED modules must meet the following L70 (Electrical and Photometric Measurements of Solid-State Lighting Products) rated lumen maintenance life values:

 

25,000 hours for residential grade indoor luminaires;

35,000 hours for residential grade outdoor luminaires; and

35,000 hours for commercial grade luminaires

 

There is also a mandatory 6,000 hour lumen maintenance test, which equates to about a 9 month duration. However, EPA understands that waiting 9 months can create economic hardships so manufacturers will be allowed to apply for a conditional early label option at 3,000 hours of testing when they supply LM 80 test data and in situ temperature test data. The conditional label is based on subsequent completion of the rest of the test.

 

The full Energy Star Luminaires specification is available from the Energy Star Luminaires web page, which also carries comments on Draft 1 of the specification (released May 10, 2010) and Draft 2 (released October 4, 2010).

 

Information on third party partners, Accreditation Bodies, Certification Bodies, and Laboratories can be found here.

0

nano_in_farbe-m_tcm63-78626.jpg

 

Microscopically small nanostructured arrays of lenses that can record or project amazingly sharp images in brilliant colors are being demonstrated by Fraunhofer research scientists at the upcoming nano tech 2011 trade show in Tokyo. The image illuminating the wall of the Fraunhofer exhibition stand at the trade show will be produced by a luminous cube. The prototype of the new projector consists of an optical system just eleven millimeters square and three millimeters thick through which a powerful LED lamp shines. The images are amazingly sharp, the colors brilliant, all thanks to micro and nanotechnology. “The special thing about the new projection technology is that the image is already integrated in the microoptics. The pixels measuring just a hundred nanometers or so are stored in a chromium layer under the lens array. Such a microarray has around 250 microlenses, and under each lens there is a microimage. When all of them are projected onto the wall together, a high-quality complete image is produced from an extremely small projector,” say’s Marcel Sieler, physicist at the Fraunhofer Institute for Applied Optics and Precision Engineering IOF in Jena. The IOF scientists have also developed a projector that is not much bigger than a box of matches. It can project presentations, video clips and movies from a cell phone or laptop onto any wall – at home, in the office or out and about. Ultra-flat cameras that are ideal for area or production monitoring in exposed locations are another application which will be demonstrated in Tokyo.


Eavesdropper

2

Vintage-Ford-Model-T-Kerosene-Headlight-Lamp-w--Burner-for-sale_260684949805.jpg

Ford Kerosene Car Lamp

220px-Carbide_lamp_lit.jpg

Calcium Carbide Car Lamp

 

Original automotive headlights burned kerosene, had a chimney, needed to be lit and extinguished.  Headlight innovations around the same time gave calcium carbide generators, with a controlled water drip, produced Acetylene Gas, which, when burned, produced intense light, greatly improving a car's nighttime vision. 

 

Today we don't have to re-fuel our headlights. Instead we enjoy LED lamps rated at 50,000 hrs, or 5 years of continual operation. In the past 2-3 years the industry has made great strides in integrating high performance LEDs in all vehicles. From side markers, to taillights, to the interior LEDs are becoming the standard. Like the LED lightbulb replacing standard bulbs, all auto lamps are headed to obsolescence.

 

The "holy grail" of automotive lighting has been to replace headlight lamps with an LED solution. A legitimate LED swap has been completely unheard of until now. The doors have flung open with the recent milestone in LED brightness output of 100 lumens per Watt, and further with some manufacturers demonstrating 200 lm/W in laboratories. Cars need over 800 lumens for proper headlight usage, and these LEDs are up to the task. For example, a single Cree XLamp XP-G series LED can provide 400 Lumens at 1A and over 130 lm/W at 350mA. Driving the LED at 1A produces the maximum amount of heat, the number one issue with LED systems.

 

However, price has completely blocked the wide automotive adoption of LEDs. Just a few years ago, a single LED would cost $5.00 USD, in the past year has dropped to $1.00 USD. The sweet spot of price and ease of manufacturing should be hit in the coming 12 months. Despite initial cost, overall lifetime cost and environmental impact will over pay for itself. A regular halogen lamp, single beam, requires 55 watts (240 watts on high beam). The more efficient Xenon lamp needs 35 watts. Average power input need for LED lamps comes in at 28 watts per beam. The overall efficiency is only getting better. Volkswagen plans to introduce OSRAM Joule JFL2 LED systems into their headlamps promising only 19 watts per beam. Environmental impact also pushes adoption. On conventional cars, with LED lamps, 196 grams of carbon dioxide per 100Km (62 miles), compared to 768 grams per 100Km with halogen bulbs.

 

Plug-in and Hybrid vehicles benefit the most from LED lamp adoption. Up to 6 miles is added to a hybrid car's electric only range with the use of LED headlights. 19-28 watts is a far cry from the 55 - 240 watts needed with halogen bulbs. Toyota/Lexus was the first to offer LED lamps as an option, followed by Audi, Cadallac, and 2011 has most car manufacturers promising LED options. Most LEDs options are used for daytime running lights at the moment, but full beam implementation is close. As brightness levels increase and modules prices decrease, adoption for full headlight usage will become market standard. As of 2011, 3rd generation Toyota Prius, Nissan Leaf, and Mitsubishi i-MiEV will have full beam LED headlight options.

 

Efficiently driving and regulating an array of LEDs in a headlight is the main design difficulty. A few ICs are available now to drop right into the application. Linear Technologies has a DC/DC converter, LT3956, designed to operate as a constant-current and constant-voltage regulator, ideal for high brightness/high driving current LEDs. In particular, a 25 W white LED headlight lamp can be configures with 18 of the Cree XLamp XP (130lm/W at 350mA) series elements. The LT3956 outputs a PWM signal ranging from 100kHz to 1MHz, giving the user a dimmable ratio of 3000:1. Due to its tunable features, the LT3956EUHE#PBF is up to a 94% efficient. Drives LEDs in Boost, Buck Mode, Buck-Boost Mode, SEPIC or Flyback Topology. However the 6% in efficiency, or 1.5W (25W*0.06), is dissipated as heat, even with the UHE package (5mm x 6mm) heat-sinking is inevitable.

fig-1.jpgfig-2.jpg


 

Another option is the Renesas LED headlight driver, μPD168891, which can provide constant-current control for up to 12 LEDs in series. Renesas's IC has built in overcurrent protection, diagnostic functions, emergency shutoff to prevent current issues, and is in a 48-pin VQFN package to reduce heat generation.  A few others ICs exist, but no one chip is the end-all option in this fledgling industry. Choosing the right components is based on individual design requirements, and should be chosen accordingly.


A mere 100 years after the kerosene headlight, the automotive lighting has grown to be an over 10 Billion USD industry. Electrically efficient high lumen LEDs made it possible, and more of them are coming every quarter. With few components available in this relatively new automotive LED Lighting industry, the brave and the willing to get up to speed in a very short amount of time. Very few times in technological advances can someone start at the leading edge of an industry without extensive training. The building blocks are here, they just need someone to put them together.

 

Cabe

 

Personal automotive lighting design story:

 

I started in the automotive industry designing a side (turn) lamp systems for a future hybrid.  What I discovered is nothing more than V = I*R is needed for me to begin that career path. At first I was meticulous and cautions about power regulation, but eventually it came down to just matching a resistor to a LED ( R = V/I ). A later incarnation of my circuit used a driver IC like mentioned above, all I had was a datasheet. The prototype was finished and on its way to being part of the LED Auto Revolution. I will say with my first hand  experience, the industry needs more engineers.

0

arzak.jpg

 

Philips Design and Laboratorio Arzak have continued their collaboration ‘multi-sensorial gastronomy’ and will show their latest work at the 9th international gastronomy summit, madridfusion, 25 – 27 January 2011, in the form of interactive tableware that stimulate the senses through light, sound vibration and electrical current. Since the release of the first series of interactive plates at madridfusion 2010 the collaboration has looked at ways of altering the perception and enjoyment of food and drink by subtly stimulating adjacent senses at the same time.  The concepts challenge our associations of images and sounds with the sensations of hot, cold, sticky, dense, liquid, etc. Taste and the sensations triggered in the dining experience can be altered, expanding the repertoire of culinary stimuli and extending the experience of fine dining into a new dimension. “Last year Arzak and Philips Design introduced three bone china concepts which are designed to light-up when food is placed on the plate or liquid is poured into the bowl. With the new generation of tableware we touch the senses not only via light, but also via sound vibration and electrical current,” said Clive van Heerden, Senior Director Design-led innovation at Philips Design. The ‘eye of the beholder’ platter concept is a piece of interactive tableware designed for two or more people to eat from. A crystalline substructure changes appearance with moving images (evocative of fire, ice, water, etc.) which are designed to contrast or compliment the dishes served on the platter. Very sensitive temperature monitoring and an array of motion sensors responsive to the utensils and the food make the dining experience playful and surprising. Color, imagery and movement affect the appreciation of individual food items. The platter responds to a series of utensils that stimulate the lips and tongue in subtle ways. During the show, Arzak will show a prototype of a plate they created out of a PhotoFrame.


Eavesdropper

0

northernligh.jpg

 

The ‘Aurora in a Box’ which recreates the physics involved in the creation of the Northern Lights or Aurora Borealis, will be used to demonstrate how electrically charged particles in the atmosphere create the spectacle seen at the earth’s poles. Dr. Wild, a Physicist studying the space environment and the links between the Sun, the Earth and other planets, was awarded a grant from Research Councils UK to create the outreach tool to explain the research to non-specialist audiences. Dr Wild uses the model to help him explain his research to children in schools, at university events and at national science events. “For a start it’s just really interesting science, but it also has very practical uses. We use a lot of technology in space, like communications and positioning satellites, and those satellites are sometimes outside the protection of the Earth’s magnetic field. They’re therefore more vulnerable to changes in space weather and can be damaged or have their services disrupted. Being able to predict this would be very useful,” said Dr. Wild. The Aurora in a Box consists of glass tubes full of gas through which electrons move, causing the gas to fluoresce exactly as it does at the Earth’s poles. Auroras are linked to the solar wind, a flow of ions and electrons continuously flowing outward from the Sun. The Earth's magnetic field traps these particles, most of which travel toward the poles where they are accelerated towards the Earth. Collisions between these particles, and atmospheric atoms and molecules, causes energy releases in the form of streams or arches of colored light.


Zero

0

GeneralIllumination_pic1.png

 

Global Lighting Technologies is introducing a new range of LED-based edge-lit illumination solutions to expand its offerings beyond LCDs, keyboards and keypads and into areas of egress lighting and general illumination. GLT is enhancing the advantages of LED illumination with a new range of edge-lighting solutions utilizing high efficiency LEDs that focus the light into a high-performance backlight, or light guide. Because the LEDs are located on the edge of the light guide, there is better optical control for color and uniformity, fewer LEDs, better repeatability, and the thinnest possible lighting solution. These new illumination solutions from GLT include edge-illuminated LED backlight panels for egress lighting and exit signs, downlighting, as well as under-cabinet, splash, desk task lighting, refrigeration, and cabinet illumination solutions (such as medical cabinets). “Edge-lit LED illumination has moved well beyond its established turf in backlighting portable and handheld product displays, and so has GLT,” said VP & General Manager David DeAgazio, referring to the company’s long-established success in super-efficient, ultra-thin BLU (backlighting unit) designs for a wide range of backlit displays.


Eavesdropper