Skip navigation

community

Lighting

1 Post tagged with the media tag
0

1-osramledsfor.jpg

 

New, particularly high-performance light-emitting diodes (LEDs) from Osram make it possible to build mini projectors. These LEDs produce enough light to project images measuring over one meter in diagonal on a wall. The small, efficient light sources are the key components of a new pocket projector from 3M. Measuring just twelve by six centimeters, the projector fits easily in any handbag and can be connected to cell phones, laptops, or cameras. Very small light sources for mini and micro projectors can be produced using LEDs. The component used in the 3M MP180 projector, for example, contains blue, red, and green LED chips from Osram Opto Semiconductors and measures just five by six millimeters. In addition, the diodes heat up only very slightly and do not necessarily need to be cooled with a fan, which makes the projector smaller and quieter. Furthermore, the handy projectors can run on batteries because the LEDs require only a small amount of electricity. In the case of the 3M device, their optical performance is sufficient to produce images with a diagonal of up to 127 centimeters, depending on the lighting conditions. Another plus is that LEDs have a service life of roughly 20,000 operating hours, much longer than the few thousand hours of run time achieved by projector lamps. The 3M PocketProjector MP180 sells for $499 and can be found here: http://www.shop3m.com/3m-pocketprojector-mp180.html?WT.mc_ev=clickthrough&WT.mc_id=3M-com-GoogleOneBox-3M-POCKETPROJECTOR-MP180


Eavesdropper