Skip navigation

community

OmniCorpDetroit

8 Posts
0

5.3.2011 THE FINISHED PRODUCT OF THE LASER TAG SHIELD

 

Abstract:

 

OMNICORPDETROIT has completed its Lasertag shield for Arduino as part of the Great Global Hackerspace Challenge. We've taken this challenge and taken into consideration our specific location in the heart of the city of Detroit and how learning to create with a microprocessor and a portable power source could impact education, the way people learn and what they learn about. We feel the project is simple, yet complicated enough to the point where kids or students of any age could simply assemble their circuit board and play, but along the way learn how to code and program and what they can implement in efficient and creative ways. Our kit is relatively cheap, under $15 and can be sourced from an array of different suppliers; essentially they contain nothing fancy -- just snazzy.

 

****

 

1. OCD feels the Lasertag shield is very reproducible. The kit contains less than twenty parts and we've included all of our sources for each part. There is really nothing 'exotic' on these boards - LEDs, IR sensor, IR emmitor, vibrating motor, resistors, a piezo speaker and DC battery adapter and an Arduino. While the price of the Arduino more than doubles the net price of the kit, we chose to use Arduino because a lot of educational institutions already have or utilize the technology and have them available, as the Mt. Elliott Makerspace. And, this is a prototype - we plan on embedding an ATMEGA328 on newer versions of the board as to eliminate the Arduino. Minimal tools are required to produce Lasertag as well: Some wire strippers, a soldering iron and some solder. As with our Mt. Elliott Makerspace workshop, we had a group of about ten students complete their circuit build and playing lasertag within 2.5 hours. The kit fits inside of an Altoid tin.

 

As stated previously, we've built the kit so one could build it out once they're familiar with code and circuit building. We've allowed for the capability of adding more teams and a mother unit that would keep track of all games played. The infrared communication could very easily be adapted to other projects.

 

2. The OCD Lasertag Shield really has no out-of-the-ordinary parts and we think one should have no problem sourcing one or 100 of them. The only thing we see perhaps posing the problem in sourcing is the circuit board itself, but it was also made using a bread board and a protoboard with no problem. We've also contemplated constructing our circuit board out of cardboard (see: Paperduino at http://blog.makezine.com/archive/2009/05/paperduino.html?CMP=OTC-0D6B48984890). We've also included links to the original circuit board file (see previous post) and a link to the source code: http://omnicorpdetroit.com/blog/2011/05/04/hehe-well-explain-tomorrow/

 

3. We feel the low cost and reproducibility of the kit, at less that $15 (less than $750 for 50) are our projects real strong points. We feel teaching a man to fish is more important than giving a man a fish, therefore we've really put emphasis on simplicity with regards to curriculum and teachability and have given the workshop an aggressive hands-on approach. We didn't include packaging because we saw that as the real sourcing issue for different places around the world. While we have a Makerbot, we've recommend that, if anything, the kit be enclosed in the Altoids tin in which it comes.

 

4. The plans are very well documented with a good breakdown of all things needed to complete the kit. While actually still incomplete, we are going to fully develop and test its uses with more test workshops in the future. Seeing some other Web sites lead us to kick ourselves for not starting a wiki in the beginning (we think Metalab did quite an exceptional job documenting their builds!) But, we have a web site in the making that will consider all the resources we've used and then some.

 

During our workshop with the Mt. Elliott Makerspace, we took a lot of notes and have already been refining our teaching methods. Here is a video of our workshop: http://omnicorpdetroit.com/blog/2011/05/04/recap-of-the-laser-tag-workshop-held-at-mem/

 

5. Lasertag addresses plenty of gaps in modern education, but first and foremost we think it helps demystify technology for younger generations or people who may not have traditionally had access to things like Arduino. I've seen wonderful examples of Arduino used in very innovative ways from Smart Gardens (http://www.instructables.com/id/Garduino-Gardening-Arduino/) to coffee bean roasters (http://www.instructables.com/id/A-fully-automatic-coffee-bean-roaster-Arduino/) to OCD's Mind-Controlled Balloon popping machine, which reads one's brain waves and cues a pointed rod attached to a servo to pop a balloon. The infrared communication has very many uses as well including remote controlling devices and motion detection. They both would make great spin-off workshops as well as help to make a generation of students and young kids into creative entrepreneurs.

 

It's pretty inexpensive technology and can all be obtained for the price of one text book. There is a plethora of information and resources regarding the uses and progamming of Arduino. Some good Web sites include www.ladyada.net, www.adafruit.com and arduino.cc, among many others.

 

6.  We feel that while Lasertag already exists, it's a great medium for children to be able to learn about infrared communication and Arduino technology. It's exciting, easy to execute and provides portals into other realms of digital and physical making. Our three-person team essentially split all tasks, each helping with developent, administration and documentation.

 

****

 

Lasertag is still in development. Our workshop went really well, but with anything, there is room for improvement! This challenge got our brain thinkers flowing and now we're more excited than ever to get this workshop series off the ground. We have an educational Web site in the works, the manual's gonna be hot off the press and hopefully within a couple of weeks we'll be teaching lots of people how to have fun while also creating something useful!

0

DSC_0114 copy.jpg

 

Hello Hackers, hope the day finds all of you well!

 

It found us well April 30 when we brought the OCD Lasertag shield to the Mt. Elliott Makerspace so little makers could try a hand at playing around with assembling a shield and using it with Arduino - they loved it!

 

The workshop went very smooth and lasted about 2.5 hours. We passed out diagrams to eight students, some as young as 12, had them assembling their Lasertag shield and playing within no time at all.  We pre-programmed the Arduinos and only briefly touch on what code was, but we were inspired to consider writing cirriculum for an eight-week class in which we break down the shield, what programming is what one could do with it and what other things may be developed using the infrared communication technology, i.e. a remote control. We are developing a comprehensive manual which we will include in our final submission, and what I have given a sample of below and think that a comprehensive class would be not only fun but would inspire a lot more people to start thinking creatively about problem solving by using things like Arduino.

 

 

We see the project as being very reproducible, it has minimal parts and we even considered packaging it for around $20, not including the Arduino. Lasertag kits now are in the hundreds of dollars and professional ones can be up to $2,000. The OCD Lasertag Shield is a more crude version of the game, but our goal is to encourage users to acclimate themselves to writing simple code and develop the kit further to suit their needs. The kit includes everything we used to develop the shield, including the original PCB file, ready to edit, and sourcing suggestions for different parts of the world.

 

As you all know, the state of education (at least in America) is in shambles. OMNICORPDETROIT believes technology can play a huge part in education and can get youngsters interested and learning about things they never thought they could do. To teach someone an adaptable technology such as infrared communication and do so with a hands-on project is the key to getting the next generation's brain gears turning over things other than television!

 

Here is a link to the photoset on flickr - we are steadfastly working on a video of the build and students playing lasertag at the moment. http://www.flickr.com/photos/55168381@N06/sets/72157626633571716/ (sorry about the lack of color correction and the shakiness!!)

LASERTAG wkshp diagram.jpg

Above is the diagram we passed out to MEM students. It is very simple and the goal was to get them making and using their kits as soon as possible. The full-text manual is much more in-depth and is meant for a slightly older crowd.

 

 

 

... Please stay tuned for more of our project tomorrow and in a copy of our final submission!

0

Today OmniCorpDetroit brought the lasertig kit and instructions to the Mt. Elliott Makerspace. Needless to say, it was as exciting as it was a big day. We had about eight students, some as young as twelve, assemble and learn about their kits and how they work with Arduino. It went great! While we had one student struggle with its assembly, we helped him through it and it even got us thinking about turning the Lasertag Project into a six-to-eight week class and teach students about each component and the development of the shield.

 

Either way, we'll be editing video and photos tonight and putting the finishing touches on our manual. We'll have another blog post up at the end of the night with a little more stimulation of the visual and time-based nature. Meanwhile here's a preliminary photo of what the finished product looks like.

 

Cheers and good luck to all in the final days of the competition!

 

Lasertag.jpg

0

Circuit Board Funz

Posted by Achille Bianchi Apr 18, 2011

Well, after designing and printing OCD's Lasertag circuit board, we realize: "Hey! There really IS more to it that we thought."

 

Honestly though, we did have a complication on our circuit board, fresh from the mfg. -- had a shorted trace on it. I guess that's why you print test boards. We've temporarily fixed the problem and we're well on our way to have  A LOT more for next week when we'll be hanging with the fine folks at the Mt. Elliott Makerspace where we'll see what their mini-makers think of the project. We intend to get some feedback from the students over there to see how our designs and concepts are holding up. For $1,980 less than a professional kit, however, we think they'll be stoked and that they'll find some other useful projects to spin off from the kits we're offering.

 

Along the way, just a couple of days ago as a matter of fact, the OCD crew was thinking that it's actually a benefit that we're novices (with regards to our particular team) because we're all (ok, maybe just Achille) kind of new to Arduino - we actually think it works to our benefit, though. We really get a first hand experience on how simple our instructions need to be and our limits to what we can teach and inspire are clearly defined through the development of this project. We have everything worked out for the most part: our BOM is done, our parts are ordered and our finalized boards are being printed. We'll be assembling our workshop kits by the end of next week - just in time for the May 3 deadline!

0

Today (April 9) the OCD crew is completing the final design our circuit boards for the lasertag workshop kit and it's just in time because the pupils at the Mt. Elliott Makerspace are eager to try out our DIY version of neon stimulation. We are toying around with the idea of what our 'zapper' or 'gun' will look like and we've not ruled out the possibility of having another type of device that transmits infrared. Decisions, decisions.

 

We have our componenets lined up, we have our circuit board completed and we'll be sending it off to be made Monday. We've been toying with the idea of which components to include for price and replicability sakes. For the most part, we've been trying to figure out what size speakers to use, whether to actually include a laser or not for an extra $4 per kit (because lasertag is indeed based on IR communication), and whether or not to include a vibrating motor. As much as we've been developing this kit we're actually kind of reinventing the way it the entire system will be able to operate in the longrun. We be getting our boards printed with the options of having all these extras installed, and others so users will be able to build up their lasertag kits as they deem fit.

 

 

The next blog post we'll be informing you of how we plan to conduct our workshops with the Mt. Elliott Makerspace. We'll most likely to an OmniCorpDetroit-style workshop where we'll assemble pre-made kits where students will get to attach the components to the pcb, upload some pre-made code and learn about how it all works in the process.

 

We will be including a manual with the kit that will be broken down into color-coded 'sessions'. Green text will indicate the plug-n-play type of user experience, where lasertag makers will simply solder their boards toghether, plug in the code and play. Yellow text will indicate the more intermediate components of programming and have students do some extra learning on the side while they make their lasertag. Red text will highlight advanced processes and programming where students will be able to explore how the world of microcontrollers work and will mostly include suggestions and learning resources for diffrent projects. The entire manual is based around wanting students to not be intimidated by using microcontrollers like Arduino and will help layout for them a learning experience that's simple and straight forward, defining terms and processes along the way.

0

Who is OCD?

Posted by Achille Bianchi Mar 28, 2011

Better late than never! Har har.

 

Anyway - OMNICORPDETROIT is a group of all types and backgrounds, about 24 of us in total, and we like to get together, dork around and make fun things while also inspiring communities around us to do the same. The only hackerspace in the city of Detroit, we have a lot to offer to those looking to be productive and to exercise their skill sets in new, fun ways.

 

Here is a link to pictures from our Messenger Bag Making Workshop: http://www.flickr.com/photos/55168381@N06/with/5399314563/

We had our students ironing together plastic bags, which made a flexible yet durable material.

 

Check out some of our other activities on OCD's blog at www.omnicorpdetroit.com.

0

GGHC Update: 3.28

Posted by Achille Bianchi Mar 28, 2011

Hello from Detroit!

 

OmniCorpDetroit (OCD) is well on our way to developing an inexpensive version of DIY Lasertag.

 

We basing the project around a workshop-style kit with which users could become proficient and inspried by the different types of funtions a microcontroller may provide with a limited budget and little or no experience. We will be working with the Mt. Elliott Makerspace (MEM), located in Detroit, and will host our inaugural workshop with MEM's students.

 

Playing a game of lasertag this weekend thoroughly inspired us. Noting the actual lasertag packs one might find at Laser Edge are valued at around $2,000, OCD's prototype DIY kit is hovering at around $20 -- we're doing pretty well. We're basing our kit on the Arduino platform and a couple of basic IR components. As of Saturday, OCD was determining how to write the pack's protocol. We are documenting the stages of our code development and will include a step-by-step breakdown of how the code was written and what it all means, with examples and mini projects along the way. The goal is familiarize users with Arduino's functions in a logical, applied and graphic way.

 

Here is a fun video of our circuit build.

 

We want to inspire the students to use a pricepoint microcontroller kit in creative and useful ways. The kit, as inexpensive as it is, will have a somewhat limited functionality, but we're steering its development towards a platform that could eventually be customized and built out, enabling more and more functions as the user becomes comfortable and more experienced with advanced microcontroller programming.

0

OMNICORPDETROIT

Posted by Achille Bianchi Mar 23, 2011

Welcome to OMNICORPDETROIT's first blog post for the Great Global Hackerspace Challenege!

 

Tentative team members from the OCD clan include:

 

Achille Bianchi

Joshua Slominski

and

Rhita Boufelliga

 

For our project we plan to use the Arduino Duemilanove and a couple of assorted parts:

IR sensor

IR diode

5V vibrating motor

tentative 9V power source

plastic encasement for the IR sensors and diodes

 

After the development stage, we are going to try to apply the design to another application as well.

 

We are very excited about this project and the opportunity to collaborate on a global scale and we look forward to competing in San Francisco in May

 

cheers!

 

'til later



Recent Comments

No recent comments.

Filter Blog