Skip navigation

community

1 2 3 4 Previous Next

Robotics

53 Posts tagged with the on_campus tag
2

 

Human beings make tools. Animals make tools. A tool gives an advantage over adversity and guarantees survival. Will the same happen if a robot makes a tool?

 

 

Researchers at ETH Zurich are on a mission to not only have robots make tools, but they are teaching the bots how to use them. Their goal is to simplify the complexity of this type of robot, while at the same time giving it extraordinary capabilities like creating its own parts, fixing itself, and even creating other robots from printed parts and integrated motors.

 

 

So far, their robot consists of a mechanical arm with Hot Melt Adhesive (HMA) capabilities. This means that at the end of the mechanical arm is just a hot glue gun that can be used to create parts layer by layer. In their effort to avoid complexity, it has no manipulator mechanisms, instead it only uses the stickiness of the printed parts to move them and place them.

 

 

The project has only just been started. In a demonstration of their progress, ETH researchers showed that their robot is capable of creating tools and thus performing tasks that it would not be able to do otherwise. It took the robot about an hour, but it was able to create a cup with a handle to transport water, an impressive task for a robot with no hands.

 

 

Next, the team or researchers are working to give the robot perception capabilities to eventually achieve a completely autonomous robot. At the moment, the robot can only create simple shapes in about an hour’s time; a long way away from creating an entire mechanism, but even bots need to take it one HMA layer at a time.

 

Eavesdropper

0

keioplant.jpg

USB connected interactive plant (via AkihabaraNews & Keio University)

 

If the Japanese have not already created enough unusual devices, they have one more invention to add to their list. Researchers from Keio University have created plants that interact with their surroundings. The plants are programmed to show different emotions through their movements by using data collected from sensors. The movements that match with specific emotions were chosen by having many people show how they think a happy plant or an angry plant would move.

 

 

The plant sits in a square pot that would look like any other Japanese plant holder on the outside, but on the inside is where the plants mechanics and electronics lie. The plant moves by two stepper motors connected to its leaves and twigs by very thin cords. Additionally, it monitors its surroundings using a microphone and motion sensors. According to the input from the sensors the plant will move based on the movements it picks up and the tones it hears.

 

 

The Japanese were hoping to make plants seem more alive and have a greater presence in areas. They have conducted their research for almost a year now and have not had any plants die or wilt, although some research states otherwise. In the future, they look to bring bigger plants to life and possibly trees, they would like environments people travel through to be fully interactive. Technology may soon creep into every aspect of our surrounding world. (The world would hate us)

 

Video Via AkihabaraNews & partner Diginfo.tv

 

Eavesdropper

1

burrittobot1.JPGburritobot2.JPG

(Left) Burritob0t platform (Right) The bot does not print the tortilla, unfortunately (via Marko Manriquez)

 

Robots have been showing their love for making food over the past few years like Suzomo’s SushiBot which can pump out thousands of the tasty rolls and the MIT BakeBot that mixes up cookie batter ingredients from scratch. It seems all the major cuisines are being slowly represented from our mechanical friends, but none have the unique technique of printing up delicious burritos like that of Marko Manriquez’s Burritob0t.

 

The robot uses a Mechatronics/Gantry 3D printing system with RAMPS (RepRap Arduino MEGA Pololu Shield) electronics, based in-part from RepRap’s self-replicating manufacturing machine, as the robots base platform. To actually build a burrito, the robot needs a 3D model representation of the ingredients (cheese and beans) which is done through the use of ReplicatorG software that converts the STL/3D model to GCODE. Once the robot has the converted code, the ingredients are fed into two MakerBot Frostruder MK2 compressed air delivery syringes which pump out ingredients based on the 3D model onto a tortilla.

 

Marko designed Burritob0t for his thesis project at ITP (Interactive Telecommunications Program at NYU) as a way to examine the relationship between fast-food practices (conveyor-belt edibles) and human nutritional habits. While the robot does not actually build a burrito from scratch, it does print up 3D piles of tasty ingredients with digital perfection.

 

Cabe

http://twitter.com/Cabe_e14

1

arduino.jpg

Arduino robot used for promotion of RobotC (via RoboMatter)

 

Robotics and software coding can be daunting to a beginner, but software company RoboMatter works diligently to make these fields accessible to beginners and hobbyist. Their software is already compatible with LegoMindstorm and others platforms alike that aim at brining robotics to the main stream. Now, RobotC has announced they will expand their code to be compatible with one of the biggest development  board platform there is, Arduino.

 

 

RobotC has released a public BETA version of their code for Arduino. To use RobotC with your existing Arduino, the Arduino will have to be updated to version 3.12. Once this is done, the same version of RobotC is compatible with Arduino as well as NXT, Cortex. This new version will support the Diecimila, Duemilanove, MEGA 1280 and MEGA 2560 and UNO Arduino boards.

 

 

This BETA version is free for the public all summer long and can be downloaded from the RobotC website.

 

Cabe

http://twitter.com/Cabe_e14

1

ingestion-digestion.jpg  sludge-distribution.jpg

(Left) Egestion Vessel for the EcoBot III  (Right) Sludge and water distributor for EcoBot III (via Bristol Robotics Laboratory)

 

Robots are not only difficult to design and build, but they are also a challenge to handle after a project has ended. Robots are manufactured using resilient materials but many are toxic and non-biodegradable and so have a negative impact on the environment if they are not retrieved and disposed of safely.

 

 

Dr. Jonathan Rossiter from the University of Bristol and Dr. Ioannis Ieropoulos of the University of the West of England, are embarking on a project that will tackle this problem head on.

 

 

To do this, they have received a grant of over £200,000 from the Leverhulme Trust. The team will attempt to build a robot completely out of biodegradable materials. They will apply this technology to an existing project they call the "Ecobot," which is a robot that uses Microbial Fuel Cell (MFC) technology for energy. MFCs function by extracting electrons from the microbial metabolic processes as they feed on things like sugar, fruits or even insects. For this reason, the Ecobot is a perfect candidate to go full biodegradable.

 

 

Biodegradable robots will change the way robots can be used for research. Currently, a lot of effort must be put into keeping track of the robot and salvaging them once they are not operating. But if Rossiter and Ieropoulos are successful, researchers could unleash hundreds of robots with no worries of environmental damage after the robots stop functioning.

 

Eavesdropper

 


1

InIcePassBy_web.jpg

Concept of the crybot (via Stone Aerospace)

 

Exploring other planetary bodies is both costly and risky for human explorers. While money is a big factor in celestial exploration, the time and resources it takes for a human to travel extraplanetary is the biggest factor. How would we get the fuel to travel back to earth? What about food and what toll would it have on human bodies travelling that long, even to our closet neighbor Mars? These are some significant hurdles for us as humans, but not so much so for our mechanical robot friends when it comes to other-world exploration.

 

This is precisely what Stone Aerospace engineers are looking to do with Project VALKYRIE. The project, led by Bill Stone, is a collaborative effort that includes participants from CU, UCSC, LSU and Los Gatos Research to send a robot to explore the oceans on Jupiter’s moon Europa. The robot, called ‘cryobot’, the team will use is a 6 ft by 10 in cylinder that’s equipped with a high-powered fiber-optic 5000 watt laser to cut through Europa’s icy crust enabling the robot to get to the water underneath the surface.

 

The power source for the laser (unknown at this time) will remain on the moon’s surface tethered to miles of fiber-optic cabling, which would allow the robot to navigate the large sections of ocean. Cryobot will also feature an astrobiology sensor that will enable the robot to make an ‘educated’ guess of sorts at taking core samples that might contain life. It will also deploy a series of sensors to collect additional information for future return missions with a payload tailored for that particular mission. NASA has recently given the team $4-million in funding to field-test the autonomous robots capabilities at an Alaskan glacier where it will penetrate the ice at depths of 10 to 50 meters.

 

Final testing will then be done in Greenland where crybot will descend to depths of up to 200 meters using the fiber-optic laser. Successful testing will lead to a full-scale dress rehearsal on a South Pole lake which will approximate the feasibility of sending a science payload to Europa in the near future.

 

Cabe

http://twitter.com/Cabe_e14

2

 

As a generous charity for a fundraiser, one brave soul has volunteered to have his head shaved by a robot with three arms (looks similar to Dr. Octopus' extra arms from Spider-Man). The robot is a Multi-Armed Unmanned Ground Vehicle (UGV ), and was being controlled from an operator through a computer. The charity was for St. Baldrick's Foundation to help cure child hood cancer and the robotics firm helping with the fundraiser and providing their own robot for use was Intelligent Automation, Inc.

 

 

The program did a little more than raise money for charity. It demonstrated the flexibility to carry out tasks for their UGV robot. The robot yields three arms, all equipped with cameras, and 29 degrees of freedom. The camera and arm arrangement allows the user to move the arms relative to various frames of reference. As a result, the robot is capable of carrying out tasks that require complex movements and manipulations to objects.

 

 

The UGV used has many purposes it can serve. It has shown the ability to handle tools, inspect backpacks, tie knots, breach doors, and IDE disarming. Although the robot gave a far from perfect haircut, it gave a perfect example of how far along robots have come. Not to mention they did have a robot set up for emotional support and one to clean up the hair on the ground. Maybe next time a robot can wash our hair for us too.

 

Eavesdropper

2

 

Robots have been designed to do just about everything from serving food to bomb defusing, but they don’t typically have the free-range movement that humans do when it comes to navigating uneven terrain. Take climbing a mountainside, wide degrees of motion and agility allow humans (and animals) the ability to handle and obstacle. Bots can only watch.

 

Hume-biped.jpg

 

However, robotics engineers from the University of Texas and Meka Robotics (located in San Francisco) are looking to overcome this obstacle with the introduction of the Hume bi-pedal robot. The team, headed by Louis Sentis from the Human Centered Robotics Lab at UT, has designed the Hume robot to incorporate a HCHA (Human-Centered Hyper Agility) range of movement. To do this, the team used a series of elastic actuators (6 DOF SEA total)for each joint which provides the robot with 6 degrees of spatial movement (including lateral).These powerful modular actuators give the robot its strength,  speed, and a certain degree of agility. The Hume design is still in its infancy stage, as there is no internal power source and has yet to acquire feet, but it looks to be a step in the right direction for all-terrain bi-pedal robots. On the other hand, I don’t think robots will replace humans in the sport of Parkour anytime soon.

 

Also see PetMan from Boston Dynamics. (Hume designers should take note.)

 

Eavesdropper

2

 

Building projects with microcontrollers (especially Arduinos as of late) opens minds to an unlimited amount of innovations. Whether the projects are created for fun, or to serve specific purposes, they can always motivate others to be creative. The latest Arduino powered creation comes from Ekaggrat, an inspired individual with a strong interest in science.  

 

 

Ekaggrat has created a robotic arm that writes down the time by the minute on a dry-erase board. After a minute is up it erases the digit and rewrites the new time. It is driven by four servos that control the arm and hand movements. Two 9G metal gear RC servos move the arm while two 4.5G ultralight servos control the hand movements. Using servos makes it a little loud and noisy and limits the accuracy of the robotic hand writing. However, there still can be improvements to be made such as a change to stepper motors to improve accuracy.

 

 

Nonetheless, the creation is truly inspiring and the programming that it takes to complete a project such as this is difficult. Keeping track of the timing, 4 servos, and 7-segment display writing orientation in sync with one another is impressive for a hobby project. This goes to show that the amount of creations possible with technology is limitless.

 

 

Eavesdropper

2

geminoid-japanese-android.jpg

 

 

The Takashimiya department store in Japan decided a great promotion would be a lifelike female android mannequin seducing potential shoppers in their store window. Since its introduction, the bot has done nothing but startle customers and inspire robotics designers.

 

The creator of this mannequin is Dr. Hiroshi Ishiguro, who is well known for inventing the Geminoid-F Robot. The Geminoid is a bot designed to look as real as possible. If realistic is the goal, it will cost them $110,000 USD (10 million Yen) to wheel in the bot. The more recent Geminoid-DK takes realism to a completely new level. The DK was made to look exactly like its owner, Aalborg University Professor Henrik Scharfe. Hop over to the DK's website for more.

 

geminoid DK.JPG

Lifelike Geminoid DK in this image. Hard to tell it is fake. (via Geminoid DK)

 

The idea of the mannequin is to draw in more shoppers by intriguing them to see more and not to scare them from walking inside. The mannequin is the new idea of visual merchandising.  Dr. Ishiguro said that android mannequins will be the future of shop displays and the traditional mannequins "will be no more." The mannequin knows when someone is present; now that is creepy. It can also display a range of emotions while being able to nod, yawn, and wink at a passersby.

 

Although it may be freaky to see, it is not any more strange than the age-old tactic of real humans in the display windows.  Even that odd job is being taken over my machines. It's a tough world for us humans.

 

Eavesdropper

1

Truss Navigating Robot

Posted by Eavesdropper Mar 6, 2012

 

A group of researchers from Cornell Creative Machine Labs are currently developing an autonomous robot inspired from metabolisms of biological organisms. The goal is to be able to break down larger complex structures into smaller simpler pieces that may be reassembled to create a different type of structure.

 

 

The robot clamps onto a specially designed truss using rotational robot-lockable connectors and can traverse the three dimensional structure using three basic motions. Bi-directional gears on the robot allow it move between perpendicular planes, horizontally and vertically along a truss, and 180 degrees around a truss to move from the top to the bottom. In addition, reflectivity sensors are implemented into the robot which give it a sense of location relative to the truss structure, ultimately allowing it to function autonomously.

 

 

The sensors and movements are all controlled from on board the robot. The robot carries with it a sensor I/O board, a microcontroller, servo motors, and an on board battery. These simple electronics allow it detach truss beams with 100 percent success rate and reattach them with a 70 percent success rate.

 

 

While they would like to use the robot for building deconstruction and repair, that does not stop the researchers from thinking big. One day they hope that it could help repair and construct the space station or any other dangerous tasks associated with the outside of the space station or a shuttle. Meanwhile, the researchers will be working on improving the robot so it will be cable of carrying multiple truss beams at once, and they plan on re-working the algorithms that will allow it to traverse a path of most efficiency based on the final design. 

 

Eavesdropper

2

 

Many robots have been designed for the benefit of mankind taking over continuously repetitive tasks or in some cases battling other robots for entertainment purposes. However, recently experiments have been done that may allow humans to help out animal populations in times of danger.

 

 

Maurizio Porfiri and Stefano Marras from New York's Polytechnic institute have designed a biomimetic robot fish to help study collective fish behavior. The robot fish is the first of its kind engineered to simulate animal mobility. In recently conducted experiments, the robot fish was placed into a flowing stream of water with a real fish to analyze the behavior between the two. When the robot fish remained motionless in the water, the real fish seemed to ignore it and swim about in a sporadic pattern. On the other hand, when the robot fish was simulating natural fish movements and swimming in the water the real fish tended to align in a specific formation with the robot. As the robot swam in formation, the real fish's movements slowed, proving that the fish was saving energy by following along behind the robot. Additionally, this shows that groups of fish may be lead in certain directions by a robot fish. This can prove helpful when humans create ecological disasters such as oil spills that can wipe out endangered species of fish. Nevertheless, it can also help us better understand the behavior of fish.

 

 

Can the robot fish "Pied Piper" invasive species out of foreign waters?

 

 

Eavesdropper

3

kmel_nano_quads.jpg

Nano-quads (via KMEL Robotics)

 

Kmel Robotics may have one of the best promotions for their future flagship product, the mini quad-copter, via a collaboration with the University of Pennsylvania's GRASP Lab. The demonstration shows a series of synchronized flying patterns. The video gives the illusion of autonomous swam behavior. At the moment, both Kmel and GRASP are not letting out any information on the project.

The University of Pennsylvania researchers Alex Kushleyev, Daniel Mellinger, and Vijay Kumar put these quad-copters to the test. As the video shows, it was a very successful project. Like small remote control helicopters, we all received one Christmas in the past, these quad-copters will have a very limited battery power source. This is the only information released at the moment. As more develops, I will report back immediately.

 


 

Where can all this lead? To a better understanding of autonomous swarm control, rescue purposes, or continue to work together and impress like the Swarmanoids. Either way, these are sure to make an impact.

 

Cabe

http://twitter.com/Cabe_e14

0

 

Berthold Bauml would be to blame for with the downtrodden servatude of robots, or the impending robot uprising. He is the lead scientist in real-time dynamic motion planning at DLR. He developed a new advanced humanoid robot named, Agile Justin. It stands with a happy face on a terrorizing body.


Agile Justin is the new and improved sister of the older version named, Rollin’ Justin. Berthold stated, “…but with improved dynamical performance: 1.5x faster arms through different gear ratios; completely new wheel electronics and bus architecture, which allows a 500Hz control loop over all four wheels and steering DOFs on the mobile platform; 1kHz control loop for the arms, torso and hand DOFs,” when it comes to the improvements in Agile Justin.


The different feature from all the other humanoid robots and Agile is that it has full-body control. The full-body controls consist of, real-time coordination of hands, arms, torso, and mobile base for dynamic tasks. Phew, looks like I can out run this robot.


The technical details should be forthcoming in academic publications later this year along with demonstrations at Automatica 2012.


Even though I want to see technology advances, I hope Agile does not get a mind of her own.

 

Eavesdropper

0

 

University of Albany's robot in action

 

It was proven in 1997 that a computer’s computational abilities could outsmart a human when super-computer Deep Blue beat professional chess player Gary Kasparov at his own game. This match put the human brain against the software programming capabilities of a team of developers, but Deep Blue still needed human assistance in physically moving the chess pieces.

 

14 years later, roboticists hope to grant computers like Deep Blue the ability of playing an entire game of chess independent of human assistance. In 2010, a competition was held at the annual Association for the Advancement of Artificial Intelligence Conference in San Francisco. Roboticists from many places and universities presented robots that resembled those on an automotive assembly line.

 

Their robots ran into trouble trying to identify and then properly move the game pieces in accordance to the game rules. Some robots used cameras to locate pieces,  but none were programmed to identify them. Instead, memory of the initial position of each piece indicated which piece it was and how it could legally be moved around the chessboard. Despite all methods of movement, all had a tough time clearly identifying what moves were made and where exactly the pieces were placed. Furthermore, they were slow in making their moves, which only took them milliseconds to process and decide.

 

The winning robot was "Maxwell" from the University of Albany. The robot moved along its side and probably made generous use of its mobility to clearly see moves and piece placement from different angles.

 

While a robot’s arm-camera coordination still pales in comparison to a human’s hand-eye coordination, it is pertinent to note we developed those skills over hundreds of thousands of years. Roboticists and programmers have only been working on developing these skills in robots for only a few decades.

 

Cabe

http://twitter.com/Cabe_e14

1 2 3 4 Previous Next