Skip navigation

community

Blog Posts

Blog Posts

Items per page
Content Preferred Language: 1 2 Previous Next
0

 

Fear the doctor's needle no more. Injections can be applied without the use of metal penetrating the skin, instead high power jets of the drug can force its way through your skin. The medical industry has had this tech for some time, but due to the limited control over how deep the injected drug is applied, we have yet to see widespread use. MIT has taken the concept to the next logical stage, control how the drug is applied.

 

George N. Hatsopoulos Professor of Mechanical Engineering Ian Hunter, and his team, have applied precision control over the amount of and depth a drug is injected. Older jet-based systems use a spring loaded mechanism, Hunter's uses a Lorentz-force actuator. The actuator is a piston containing a magnet, and it is surrounded by a coil. When current is applied to the coil, it can move the magnet and the injection. Precision control the outcome, direct manipulation of the speed at which the drug is applied correlates to the depth, and, of course, the piston position can be precisely controlled, adjusting the dosage.

 

When used the MIT jet-based injector goes through two stages. One is the high-pressure stage that penetrates the skin to the required depth, and the other stage slowly pushed the drug into the surrounding tissue. Keep in mind, it is still penetrating the skin, it will still hurt. However, the size of the hole produced is the same a mosquito would inflict, or so says the team. How bad could that hurt? Hopefully, we will see this tech become the industry standard soon.

 

The team is also working on another innovation, powdered vaccines. To sidestep spoiling of vaccines that lose refrigeration (known as the "cold-chain problem"), this power need only be applied to water and administered. Developing countries are the main target for this innovation, countless lives will be saved for sure.

 

Cabe

http://twitter.com/Cabe_e14

0

nanowire gold.jpg

In yellow, scattering light from the silicon nano-wire. The dimmer areas are coated with gold, reducing the scattering of light - hence cloaking.

 

There has been so many developments involving ‘cloaking devices’ over the past few years that I’m starting to wonder if the invisibility devices found on sci-fi shows like Star Trek are close to becoming a reality. With this in mind, an engineering teams from Stanford University and the University of Pennsylvania have recently announced their development of a ‘plasmonic cloaking’ device. The invisible machine detects light and is capable of ‘seeing without being seen.' Plasmons, in basic terms, are plasma-quasiparticles with the oscillation of free-electron density relative to the stationary positions of ions in metals (metal being the key word here) at different frequencies that scatter light. This plays a huge role in the optical properties in metals when it concerns light-waves. The engineers picked up on this principle and used it to develop their device using silicon-based nano-wires encased in a thin sheet of gold which dissipate light-waves by adjusting the ‘metal to silicon ratio’ (tuning the geometries). This makes the device invisible to the naked eye, and since there is no known picture of the ‘device’ (as it’s invisible) we’ll just have to take Stanford’s word for it (joking of course).

 

The engineering teams found that it was by precisely fine-tuning, the gold-plated nanowires that the scattered light cancelled each other out through the metal and semiconductor (destructive interference). They found that much of the visible light spectrum could be dissipated no matter what angle you viewed the device from and that using other metals, like copper and aluminum, work just as well as gold at making the device invisible. The only mitigating factor is making the ‘dipoles’ (separation of positive and negative ion charges) are lined-up precisely. Otherwise, the desired effect is lessened or even cancelled outright.

 

The teams state that this new technology could be applied to solar-cells (generating a tremendous amount of electricity through light dissipation), solid-state lighting and even digital cameras (improving image quality by reducing motion-blur associated with light). Those seem so mundane compared to ‘cloaking’ my vehicle while parked in a no-parking zone or making my home invisible to uninvited guests.

 

Cabe

http://twitter.com/Cabe_e14

0

Customers who choose to use Micro USB2.0 connectors are faced with a multitude of connector options in horizontal PCB orientation. 

 

Horizontal orientation is perfect for handheld applications where the PCB runs parallel to the device (such as a cell phone) and where the I/O and battery connectors live at the ‘bottom’ of the device, however µUSB is prevalent in the market and used in many different applications, the right angle configuration does not suit everyone.


Working in co-operation with customers GCT designed a vertical thru hole Micro USB connector in B & A/B configurations, A/B allows USB O-T-G (On the Go) host functionality for peripherals, amongst other benefits.  GCT are the only company in the marketing today offering vertical thru hole Micro USB connector.

 

Vertical mount USB diagram.png

 

Since launch we received interesting enquiries from a wide spectrum of applications, examples include:  Gym Equipment, washroom products, bathroom showers, consumer products which detect movement forgaming applications and data loggers to measure the G-force soldiers are exposed to when improvised explosive devices are detonated.

 

Visit GCT to view the full µUSB connector offering including USB3105 and 3130 vertical types,  click here:  http://www.gct.co/usb-connectors/micro-usb-connectors.aspx

 

Newark (Americas) product links:

USB3130 Vertical µUSB B Type Vertical

USB3105 Vertical µUSB A/B Type Vertical

 

 

Farnell (EU and APAC) product links:

USB3130 Vertical µUSB B Type Vertical

USB3105 Vertical µUSB A/B Type Vertical


0

     It had been a busy weekend. On the Friday I'd been down to Mum's after work to pack some tiems away before the builders came. Saturday saw me off doing another of my weekend activities on Wensleydale Railway, where what I'd hoped to be a nice relaxing day saw track work at the crossing I was manning - so much for peace and quiet.

 

     On arriving home I found a couple of parts on my doorstep. Ah yes. Time to do a bit of repair work. My HF vertical had become poorly over the winter, it had gained rather a lopsided look. Plan A had been to sleeve where it was joined to the insulating section at the base, but when we took it into the workshop it was just two of the rivets that had loosened up. So these were drilled out and replaced. The feed point was doing most of the support work here, so we added another rivet here.

     Why not just bolt the thing together? Well unless you like to try to fit a nut and washer 12 inches inside a 2 1/2 diameter tube we didn't think there would be any point.

 

     Okay so what effect did it have? Well I landed 9A9RR on EU-136 with a 57 report despite me showing about a 2.5:1 SWR on 14.260MHz. Now the case was that the antenna had been tuned up at the digital portions of the bands (40, 20, 15 & 10) as that's my usual mode of working. So the conclusion is that it's now a lot happier, the bandwidth has dropped, possible as now the electrical connection between the feed and the element is somewhat better. There are tuned radials fitted, I've not adjusted them this time, and they are about 8 ft off the ground. This antenna is no longer made (EVX-4000) as it's required regular maintainance, plenty of silicone to stop water getting into the 20m trap and the plentiful use of self amalgamating tape where the tubes are jointed. I can't complain, I have 6 years use out of it so far and my squeeze a couple more out yet until I decide what to replace it with. My postage stamp garden suits this one, although when I lower it on the mast I haven't much room at the end of the garden to play with.

 

     Sunday was busy too - this time near Dent in Cumbria. To provide communications to the ambulance at the bottom of the hill at Lea Yeat, I was stationed not far from the summit of the Coal Road to Garsdale with my 6m/20ft portable mast and a talkthrough radio. In the end we only had messages relating to them arriving, setting up and finishing without incident, but they are in a hole radio wise.

 

     I haven't decided what to do with the temperamental 6m beam as yet. I will however give it another try before I think about getting rid and sorting a HB9CV for the band. I have one for 2m, it's been used portable, and got me into Southern England from home on the 20ft mast with 30W on SSB.

0

LED Blue 150W  in sunny chen的 博客

Posted by amsunny May 25, 2012

Fluorescent tubes have a wide range of applications, supermarkets, schools, office, city, subway, etc. in their daily lives, anything can appear with the public places, you can see the extensive use of the fluorescent How to make LED life and brightness reached to a satisfactory standard, a considerable significance of the topic! LED 400W  fluorescent lamp to maintain long life and high brightness problem to be solved are: power supply, LED light, heat, security, four key technologies.

A. Power supply

Power first and foremost requirement is a high efficiency, high-efficiency products, heat stability is bound to. Usually two options in the power supply section useful for isolation and non-isolated, isolated volume is too large, and less efficient in use, the installation will have a lot of problems, as non-isolated products in the market prospects, we mainly discussed in this non-isolated the driver program.

Two.high power led  light source

Taiwan sulfur Cummings patent structure of the LED light source, its chips placed on a pin, heat silver pin directly to the chip node tropical out, with the-line products, and traditional product placement in the heat qualitatively different from the chip junction temperature is not cumulative, in order to ensure good use of the light source lamp beads, to ensure the long life of the light source lamp beads, low light.

Traditional patch products, through the gold wire connection of the chip is negative, heat is also generated by the chip over gold wire to the silver feet, the conduction of heat and electricity conduction money long thermal accumulation time a direct impact on the life of the LED 200W tube.

3. Heat

Infrared radiation heat is introduced and applied to the fluorescent tube, is an important means to increase lamp life. In consideration of the heat, we will separate the heat of the LED strip lights  source lamp beads, cooling and power, without disturbing each other so as to ensure thermal reasonable.

There are three ways of heat conduction, convection, conduction and radiation. Achieve in a closed environment, convection and conduction is likely to be smaller, heat dissipation by radiation, is considered the focus of fluorescent tubes.

4. Security

Their safety security, this is mainly PC flame-retardant plastic tube, because the infrared heat can penetrate the PC pipe, we design considerations LED lights use can be considered more a physical plastic insulation, even in the use of non- The isolated power supply can absolutely guarantee the safety of use.

LED Blue 150W   lamp has a rather long time, from the energy-saving effect, the face of its future application is very broad, in addition to energy saving, safe, long-life use, we should be concerned!

Safety! Is the first element in the design of LED fluorescent, fluorescent lamp using a PC fire-retardant materials, address security issues, how to improve the life of the above proposed solution to the number of LED fluorescent tube manufacturers to provide more way of thinking!

 

 

0

led 280w in sunny chen的 博客

Posted by amsunny May 25, 2012

At present, the LED Power Supply used as garden lights, tunnel lights, and indoor places used in commercial lighting, office lighting, etc. are highly desirable. With the advances in LED technology, lower prices at the same time, the phosphor price increases and cost pressures on the traditional lighting, these provide a good opportunity for the LED Flood light 10W to enter the field of interior lighting.

Less concern, however, that the amount of radiation generated by the LED of each light point is not large, is far less than the HID (high intensity discharge) light source, but it can be a very small energy concentrated in a certain direction. This also means that, although the LED unlike the laser is not as strong, but the local light intensity hazard should also be given special attention.

Insiders pointed out that the LED are mostly still in the sample stage, mainstream or traditional lighting products in the market, but the LED stage of the product will soon be full arrival. Once the LED into the product stage, IEC / EN 62471 must be mandatory to execution, related testing laboratories should have the ability to match or photobiological safety hazards may occur.

Comment:

Indeed, the led driver 120w    into the interior lighting, security issues will become more prominent, if made of spotlights, table lamps, flashlights, laser lecture pen, will cause the interest of the child, its security has become more important . For example, a small laser lecture pen if exposed directly to the child's eyes, it will damage the retina of the eye of the child. LED illumination radiation intensity of the harm is an objective reality, is the most protective part.

Of course, the correct detection LED lighting evaluation of the radiation intensity is very important, very difficult. Even if the LED Floodlight 80W   module to achieve the requirements of the lighting does not necessarily meet the requirements; lighting should also consider the light distribution, maximum intensity direction than the human eye is very easy to identify, we must seriously look for. These are not just domestic issues, but also the international detection in the field bottleneck.

LED Spotlight 30W   is about to enter the home lighting on the occasion, I hope the entire industry can be developed as soon as the correct means of detection, and specify a qualified laboratory testing, so in order to minimize the harm from the potential to radically.

0

led power 50w  in sunny chen的 博客

Posted by amsunny May 25, 2012

In the global fight against the greenhouse effect, the environmental craze, led 1w replacement light source development in leaps and bounds development, not only the continuation of the environmental protection of the LED light source, long life, small size advantages, coupled with the growing maturity of high-brightness, high power LED technology, but also LEDreplace the daily light availability increased dramatically, becoming the first choice for energy conservation, alternative light source of high energy consumption ...

LED light source has a number of environmental advantages, but early products in the design of heat treatment and high brightness, there are still some technical bottlenecks could not break through, but under the continuous improvement of the LED chip manufacturing process, the existing lighting with the led power 50w   light output lumens more nearly in everyday lighting needs, coupled with the component design of the IC solid form, so that the LED light source designed to add more flexibility and advantages.

led 10w   light source is not easy to damage the long life advantages, Excluding composition, compared to traditional high-energy tungsten (incandescent) / halogen / high pressure sodium, mercury pollution concerns CCFL fluorescent lamps LED performance is quite excellent new choice of alternative light source.

However, in order to different everyday lighting applications, also for the luminous efficiency of light-shaped, thermal design and the overall use of cost and number of applications continued to improve the design of LED products, LED lighting is more practical value, rather than just show the environmental demands of the decorations.

High Power LED 50W source, differences in material properties of the component itself, coupled with the light-emitting principle is different from the traditional lighting, light shape if not addressed, and improved lighting quality For light LED to replace the general day-to-day applications, there are still a number of restrictions, CRI illumination shape, color lighting, power conversion efficiency ... key issues need to strengthen through the optical physical design of the chip manufacturing process improvements or fixtures to further meet the needs of the general lighting.

LED solid state lighting is still the problem of high cost

In the actual lighting applications market, led power 10w  solid state lighting there are still high-priced, high-cost limit, and want to accelerate the popularity of LED lighting applications in a short time, and related businesses still have the cost of components, production technology, validation criteria ... project, one by one to improve cost efficiency.

0

When I ran out of time to solder together my 7-segment name badge, I decided to just pack the hrmshield for Maker Faire Bay Area as I planned to go to Jeri Ellsworth's Bring-A-Hack dinner.  I was hesitant to do so as I still need to make a case for it, but it all worked out very well.  I was fortunate to meet Ian and Skyler from Dangerous Prototypes who were a blast to hang out with.  They were making a video of projects at Maker Faire and I ended up being in it, at around 2 minute mark:

 

 

I'd like to thank Eric Boyd for the HeartSpark, Jimmie Rodgers for the OpenHeart and Adafruit for the logger shield.  I wouldn't have even attempted this project if I didn't have their existing projects to leverage.

 

Cheers,

Drew

0

Howdy,

 

I was excited to see the video answers from Eben Upton of Raspberry Pi posted today:

 

 

Ian and Skyler from Dangerous Prototypes were a blast to hangout with at Maker Faire, and they've just released a nicely edited 10 minute video on the Faire which offers many tips for prospective exhibitors:

 

 

Dangerous Prototypes also made a nice video of different projects people brought to Maker Faire and the Bring-A-Hack after party (my hrmshield is at ~2min ):

 

 

Tested.com also has a nice montage of Maker Faire action:

 

 

MakerBot TV provides another glimpse of the Faire including their ingenious Robot Petting Zoo:

 

 

Finally, with so much going on at Maker Faire, I had to make the tough choice to skip many of the interesting talks that were held throughout both days.  Thankfully many of them can now be watched on FORA.tv:

 

http://fora.tv/conference/Maker_Faire_Bay_Area_2012

 

 

Cheers,

Drew

0

Chip-making giant ARM has claimed that despite stiff competition from Intel, it expects to establish a significant footing in the lucrative PC and server markets. Intel, of course, has a strong hold on the smartphone market and has significant financial muscle to call on.

 

However, Warren East, the Chief Executive Officer of ARM Holdings, explained that the firm has good reason to feel optimistic about its medium to long-term outlook. "Companies making processors based on ARM cores will take between ten to 20 per cent of the notebook PC market in 2014 or 2015," he commented. "That would be much higher penetration than Intel would make into the smartphone market."

 

ARM and Intel have been the most prominent forces in the mobile phone and PC markets for a number of years now. However, they both intend to broaden their horizons and move in on the turf of rival firms. They are not in direct competition with each other, though, as Intel supplies chips while ARM licences the processor core to chip-making partners.

 

Mr East speculated that Intel will enjoy a reasonable level of success in the smartphone market, but argued that its penetration rate will peak at around ten per cent. "It's going to be quite hard for Intel to be much more than just one of several players. But they'll be a perfectly credible player," Mr East remarked.

 

He observed that ARM has a distinct advantage in that its processors will be lower in cost than those from Intel. Consequently, Mr East added, ARM can rightly expect to see its market share steadily increase over the coming years.

1

CCI25052012_00000.bmp.jpg

I would like to present my rugged, solar powered battery operated, remote cotrolled motor controller with the following features.

 

Picaxe 28x1 controller

amplified current sensing, for two motor feeds

solar panel input and solar regulator including low voltage protection

remote control receiver with code switches

facility for limit switches

extra control inputs isolated by optocoupler

 

regards

 

Daveyc

0

LED 10w in 淘 源的 博客

Posted by TAOYUAN May 24, 2012

   LED electroluminescence principle of solid semiconductor light source, with rich colors, compact, high brightness, long life, low operating voltage, safe to use, fast response, 0 to 100% adjustable light of LED 10w  output, impact resistance and anti-vibration many advantages, including ultraviolet and infrared radiation. The application range is gradually expanding, with a good prospect. The high cost of a single package of high-power high-brightness LED and a point source, therefore from a wide range of practical and still have time. Into the practical power of the single high-brightness  is very small in most of the actual use of the occasion need light-emitting plane, must be arranged in accordance with the requirements of multiple LED 120w  combination, on the one hand to meet a wider range than the high brightness, dynamic display, the color changes and other application requirements, matched with the LED drive drive the other hand, to meet the matching requirements. Common form of connection Applications by a number of LEDs arranged in accordance with certain laws and the combination of a common form of connection, there are four main, respectively, are described below. 1, a whole series of Generally simple series connection method LED1-n-connected end to end, the current flowing through the LED work equal. For the same specifications and batch  , the voltage on the single LED  3w may have slight differences, but the LED is a current device, thus ensuring their luminous intensity is consistent. Therefore, the simple form of LED series circuit is simple, and convenient links. However, due to the LED1-n-two of the series form, when one   open-circuit fault occurs, will cause the  high power LED light string off, affecting the use of reliability. Series with bypass links as the 1.1 improvements. Each LED in parallel in this way the breakdown voltage slightly higher than the LED  operating voltage of Zener diode D1-n. LED work properly, due to the D1-n is not conducting, the current flowing through the LED1-n string, and equal, normal light LED1-n-string; when LED1-n-string in the damage caused by a light string is open, because D1 The turn-of-n to ensure that the current flows through the LED string, so only the failure of the high power  LED 1w fails, the entire light string is not extinguished. Relative to a connection, greatly increased the use of reliability.

0

StarCore technology offers fully scalable and flexible solutions at low cost, these high-performance low power programmable devices for baseband, aerospace, defense, medical and test and measurement solutions allow to get to market faster.

 

CodeWarrior for StarCore is based on the Eclipse platform, enabling support of eclipse community which leverages larger ecosystem, and provides a framework that combines build, debug, simulation, and analysis tools.

 

Definitely, creating applications for complex multi-core DSP targets is overwhelming without the best development tools. CodeWarrior Development Studio for StarCore 10.2.10 meets this challenge by providing you with some new cool features:

- Updated SmartDSP Operative System

- Improved Debugger Motor

- Continued support to MSC815x family

- Continued support to PSC 9131

- Preliminary (lightly tested) support for PSC 9132

 

The CodeWarrior Developer Studio for StarCore 10.2.10 is ready for digital processing!

Start designing now with CW10.2.10 now!

http://www.freescale.com/files/graphic/tn/CW_Thumb_NEW.jpg

1

samsung-graphene-device-structure-1.jpg

Samsung graphene "miracle material" (via Samsung)

 

Graphene is back on the scene again, and this time it was sighted in the R&D labs at the Samsung Institute of Technology. SAIT recently announced that they have developed a new transistor architecture using the ‘miracle material.' Conventional silicon transistors have just about reached their speed limit even with a size reduction or shortening the connections the electrons have to travel, so in order to increase the electrons speed a new semiconductor material is needed.

 

Graphene (or even better; silicene) is thought to be the obvious solution since it has a high electron mobility capability 200 times that of silicon, but it does present one problem in that current can’t be switched off (typical gate of 1’s and 0’s except without the 0’s). Scientists have accomplished turning graphene into a zero-gap semiconductor to overcome this problem. However that comes with a price: speed reduction.

 

The engineers at the SAIT R&D labs have succeeded in creating a device, called ‘Barristor’ (graphene-silicon Schottky barrier), which can switch off the current with no speed reduction in electron flow. The device can turn electrical current on or off based on raising the height of the barrier (hence the name) by using a metallic semiconductor interface which prevents the current from flowing to the silicon. These barriers are normally used in diodes but have now been adapted by SAIT (9 patents alone for the Graphene Barristor) to develop graphene transistors.

 

This means that future electronics such as CPU’s will become infinitely faster (think 10-20GHz) over current processors with an overall reduction in size. If Samsung is successful in bringing the new transistors to the consumer market, it would be feasible to have an ultra-fast desktop computer the size of a smartphone in your pocket!

 

Cabe

http://twitter.com/Cabe_e14

1

300dpi_PI_OSRAM_Elektronniy_Svet_Stadion_Kiev_image2.jpg

One of the LED bars. (via OSRAM & Elektronnyi Svet)

 

Football (soccer) fans can feel safer while attending the European Football Chanpionships being held at the Olympic Stadium in Kiev (Ukraine) thanks to Osram Opto Semiconductors. The company recently won a bid (chosen by Elektronnyi Svet Ltd.) to outfit the stadium with their line of Golden Dragon Plus LED’s which will replace the out-dated conventional lighting being currently used.

 

The Golden Dragon line features efficient light dispersion with a beam-angle of 1700 and feature a silicon dome, ThinGaN LED structure and provide up to 203 lm at 1000mA using less power consumption over other LEDs. Elektronnyi Svet outfitted the handrails next to the steps leading up to the entrance to the stadium using 16,000 of Osram’s LEDs (almost one mile if laid end to end) making it safer for football fans to navigate.

 

While safety is certainly a welcomed aspect while attending any sporting venue, aesthetics help keep the fans interested which is why the stadiums 14 bar areas feature 12,000 (combined) of Osram’s Golden Dragon series 4-colored LED modules (3000 in all) to light up the bar counters. The individually controlled LED modules feature red, green, blue and white lights capable of generating just about any color imaginable while remaining ‘robust’ enough to handle any intoxicated fans. The new LED lights were chosen as a testament to energy-efficient technology commitment the Ukraine is currently undergoing, as well as providing the fans a safe and enjoyable environment for the UEFA final championship games (starting on July 1, 2012).

 

Cabe

http://twitter.com/Cabe_e14