Skip navigation

community

Wireless

5 Posts tagged with the sensor tag
0

Announced as ‘ground-breaking’, a new wireless sensor system for industrial measurement and control has been announced by the Deeter Group.

600x600 - Deeter Wirless Sensor System.JPGAt the centre of the new system is the simple-to-use basestation, designed to receive data from remote wireless devices such as the Deeter liquid vertical sensor (LVCS-RF). The basestation converts remote sensor input signals into industry standard process outputs. The basestation acts as the coordinator for an IEEE 802.15.4 wireless sensor network. It operates on one of 16 radio frequency channels available in the 2.4GHz ISM band. The high-power transceiver can achieve a range of greater than 1km, subject to local environmental factors. The internationally recognised IEEE 802.15.4 protocol allows several wireless sensor networks to share the same wireless spectrum without interference.

 

The basestation provides four open-collector transistor outputs which may be used to drive external relays for pumps and alarms or Deeter’s dual-level controller. Continuous analogue sensor data such as liquid level is output using a 4 to 20mA current-loop driver which enables interfacing with industrial process controllers or the Deeter Group’s range of current-loop indicators. A serial communications channel provides full-duplex RS232 and half-duplex RS485 transceivers allowing software to be developed for linking to PCs, data-loggers, PLCs or other proprietary equipment.

 

The basestation has three internal push-button switches and a 2-line by 16-character LCD. The buttons are accessible with the lid removed and are used in conjunction with the display to select installation options during initial setup. Once the system has been installed it will continue to operate without any further need for user intervention. The Base Station is housed in a rugged ABS enclosure with an external antenna. It has cable glands for power input and signal outputs and is supplied with an external, wall mounted, universal AC input power supply.

The LVCS-RF is designed to measure a continuous liquid level and transmit this information by radio to a Deeter wireless basestation at regular intervals. The device is battery powered and transmits wireless sensor data using the IEEE802.15.4 protocol operating in the 2.4GHz frequency band. The transmission range is up to 1Km in ideal line-of-sight conditions. The operating temperature range is -20C to +70C.

The LVCS-RF circuitry is housed in an IP65 rated die-cast aluminium head with an external antenna. An optional 3m extension lead and bracket are available for mounting the antenna in a position more favourable to wireless communication should the need arise. The sensor circuit is fitted inside a food industry standard 316L stainless steel tube attached to the head, with a 55mm magnetic ball-float. Standard sensing lengths are 250mm, 500mm, 750mm and 1m. Custom lengths and materials are available on request, says the company.

0

RFID item-level tagging

Posted by Eavesdropper Feb 14, 2011

1006090_RR-RRET.jpg

Finally, per item RFID tagging, UHF tags to be exact. Can you go through a checkout without putting all your items on the conveyor belt? ABI Research things it will happen soon. Bill Arnold of ABI says, "RFID systems allow apparel retailers to get a better handle on inventory, reducing costs and preventing out of stock situations that result in loss of sales. The growth in retail item-level tagging is huge, both in shipments and in total spending. The average growth rate is close to 60% for the next three years. In fact, the number of tags that will be used for retail ILT in apparel alone is likely to exceed the total number consumed over the past five years for all RFID markets combined."

Major retailors are pushing hard to use RFID. We will see more security use and checkot use later in 2011. Tyco Retail Solutions and Checkpoint are leading the way.



Eavesdropper

0

73099.jpg

 

A perimeter-protection system created by a team from the USC Viterbi School of Engineering took Best Paper prize at the IEEE Homeland Security Conference in November 2010, and is now moving to deployment at a Florida airport, while also being considered for further installations by the Transportation Security Administration.  This smart sensor system recognizes spatio-temporal sensor patterns of perimeter intrusion by foot, by fence, and by vehicle for the purpose of protecting remote fenced or virtual perimeters against unauthorized access or terrorist attack on TSA airport property. The system’s novel approach allows target intrusion sounds to be identified by users with specific needs. For example, at airports, the sensors were trained to ignore typical fence manipulation (kicking, leaning, shaking) by visitors who gather at end-of-runway fence lines and watch landings and take-offs. However, the system actively raises alerts if the fence is climbed or if someone attempts to breach the perimeter. In turn, the ground sensors ignore the presence of large jets, but raise alerts for human footsteps in unauthorized areas and can be programmed to either raise alerts or to simply report the presence of vehicles in certain protected areas. For more information please visit: http://viterbi.usc.edu/news/news/2011/smart-usc-fences.htm


Eavesdropper

0

OpenPicus, the italian open source platform made for wireless smart sensors and actuators, definitely takes off with a thick list of juicy news ready to be downloaded on 20th Jan 2011 (10am italian time)


The open source platform is mature and offers to the developers:

  • The new IDE, easy to use and Free to download
  • Software Framework: your Apps can control the functions of the Protocol and of hardware, but you don't need to be an expert of both.
  • Apps Source Code (such as wireless Webserver)
  • Video guide for the IDE and a Manual for the Framework

openpicus LOGO.jpg

OpenPicus started in March 2010, it was just an idea and a Blog. Today FlyPort module (the first Wi-Fi smart module, AKA Picus) is more and more the core of lot of Wireless applications, from sensors to robotics. Very innovative the smart Campus program: they give FREE Starter kits for Universities.

 

 


 

0

A new tag from Numerex and Savi Technology can intelligently determine whether to communicate via an active RFID network or satellite communications, thereby promising more thorough, end-to-end visibility in a global supply chain.

 

 

By Beth Bacheldor

 

Feb. 24, 2009—Numerex, an Atlanta-based provider of fixed and mobile machine-to-machine wireless solutions and network services, and RFID systems supplier Savi Technology have unveiled an intelligent hybrid tag that combines active RFID, satellite communications and Global Positioning System (GPS) technologies. The tag is designed to track goods anywhere within a global supply chain, whether they are waiting in a warehouse, being loaded onto a ship or sitting in a desert at a bare-bones military outpost.

 

The tag, known as the ST-694 GlobalTag, has been in development since the summer of 2007, as part of a cooperative research and development contract for the U.S Transportation Command(USTRANSCOM), the U.S. Department of Defense (DOD) group responsible for creating and implementing global deployment and distribution solutions for the U.S. military and government.

 

"The DOD has a mandate for an asset tag that can be used to track assets end-to-end," says Pierre Parent, Numerex's VP and general manager of satellite solutions, "which includes the entire time that asset is in the supply chain—from the time it is packed up in a container, loaded onto a ship, unloaded and delivered."

 

Radio frequency identification works well to track goods, Parent says, as long as there are RFID interrogators located at various points along the supply chain to capture tag reads. But the U.S. military shipments are often beyond the reach of an RFID reader—the typical RFID read range for the ST-694 GlobalTag, for instance, is 100 meters (328 feet). When goods are moved into desert or mountainous regions to support troops in battle, that's where they can be misplaced and become vulnerable to theft.

 

Therefore, Savi Technology and Numerex opted to marry satellite and GPS tracking with active RFID into a single device controlled by one microprocessor. Not only can the tag automatically and intelligently switch between active RFID and satellite communications as necessary, but the data can be viewed using a single back-end system.

 

The ST-694 includes an active Savi tag that complies with ISO 18000-7, the standard for real-time locating systems that employ active tags operating at 433 MHz. The ST-694 also includes the SX1, a tag unveiled one year ago by Orbit One, a division of Numerex. The SX1, which comes with a field-replaceable lithium battery, an internal motion sensor and an integrated GPS chipset, communicates with Globalstar's low Earth orbit (LEO) satellites (see Orbit One Launches Satellite-Based RFID Service).

 

The SX1 tag is programmed to activate several times per day, then send its GPS-determined location information (latitude and longitude) to the nearest LEO satellite. Whether operating as an active RFID tag or as a satellite tag, the ST-694 transmits its unique ID number. The active RFID tag serves as the master component in the ST-694, leveraging a set of algorithms developed by Savi that can intelligently determine whether to operate in active RFID or satellite communications mode.

 

"When the tag is in the supply chain where there are nearby RFID readers," Parent says, "the tag will automatically shut off the satellite controller. And the tag is smart enough to know, when a container leaves a depot and is not within range of an RFID reader, to automatically flip on the satellite controller." Each time the tag communicates with the Globalstar satellite system, however, a fee is charged.

 

Additionally, the ST-694 comes equipped with a motion sensor. In the event that motion is detected for at least a half-hour, the sensor will automatically instruct the tag to operate in satellite communications mode.

 

"The tag always wants to use the RFID system, if it is available, because the RFID readers are an already installed system, and there is no cost," Parent states. "If the tag has to use a satellite, of course, there are costs."

 

There are auto-ID systems currently on the market that support cellular and satellite communications, as well as others that leverage active RFID and satellite technology. The DOD, for example, recently deployed a solution leveraging devices that act like RFID tags and communicate via satellite and cellular communications, that is helping ensure troops in Iraq receive their necessary supplies. This is being achieved thanks to a remote tracking solution implemented and managed by Impeva Labs, a provider of asset-management systems, and logistics provider Agility (see U.S. Army Achieves Real-Time Visibility of Supply Trucks Traveling in the Middle East).

 

In addition, agriculture technology firm TekVet, offers an RFID cattle-tracking system that utilizes active 418 MHz RFID tags, sensors that monitor an animal's internal temperature and transceivers to transmit each tag's unique serial number, as along with the animal's temperature, to an Internet server hosted by IBM. Communication between the transceivers, which can be attached to poles or other fixed structures, and the Internet server is conducted via a 900 MHz private satellite communication network (see TekVet-IBM Cattle Tracker Uses Active RFID Tags, Satellite Communication).

 

There have also been prototype hybrid tags that combine RFID and satellite communications. In 2005, in fact, the Department of Defense tested a version that included a Savi active tag (see DOD Tries Tags That Phone Home).

 

A year ago, Siemens IT Solutions and Services conducted a proof-of-technology test on a solution that combined active RFID transponders and sensors with GSM and GPRS telecommunications technology installed on ships. The solution communicated the RFID and sensor data to a satellite telecommunications service operated by Inmarsat (see Cargo-Tracking System Combines RFID, Sensors, GSM and Satellite).

 

The new ST-694 tag is still a few months away from commercial availability, and pricing has yet to be determined. The tag will first have to undergo a series of tests to ensure it meets DOD requirements, including environmental tests and Hazards of Electromagnetic Radiation to Ordnance (HERO) testing to make sure the system won't accidentally detonate explosives. Once that has been completed, Numerex, Savi and USTRANSCOM intend to deploy the tags in a variety of military exercises and environments, as part of concept-of-operations testing.

 

"Testing in the lab can be quite extensive," Parent indicates, "but is never as thorough as testing in the real world."

 

 

http://www.rfidjournal.com/article/view/4635/1