Skip navigation

community

Wireless

5 Posts tagged with the transmission tag
2

35626web.jpg

Ashutosh Sabharwal (via Rice University)

 

Full duplex Wireless Communication means getting your cake while you're eating it too. Ashutosh Sabharwal, a brilliant professor from Rice University, has made an amazing breakthrough in wireless data communications world of possibilities. The concept is like two people screaming at the same time in a large arena very far away from each other, but how can they hear each other? The answer is canceling out the sound of the screams coming from the sender so that the only sound they can hear is the sound of the other person's voice.

 

Sabharwal explained, "We send two signals such that they cancel each other at the receiving antenna -- the device ears. The canceling effect is purely local, so the other node can still hear what we're sending." These extra antennas send out canceling frequencies from the sending receiver.

 

Sabharwal continued, "We repurposed antenna technology called MIMO, which are common in today's devices. MIMO stands for 'multiple-input multiple-output' and it uses several antennas to improve overall performance. We took advantage of the multiple antennas for our full-duplex scheme, which is the main reason why all wireless carriers are very comfortable with our technology."


 

Rice University's idea was conceived and tested some months ago.

 

 

Now the team is back with a new goal, Sabharwal stated that their technology could be added to all cell towers, and no additional structures will be needed.  They have already "attracted the attention of just about every wireless company in the world." No wonder, the possibility of doubling the data throughput is quite exciting.

 

This technology will not be available until carriers upgraded their speed to "4 1/2G" or "5G" speeds, but the team is hopeful that this will be available in the next couple of years. Sabharwal is head of the WARP project at Rice University the acronym WARP stands for wireless open-access research platform. This enables them to be able to experience full-duplex wireless communication.

 

Eavesdropper

0

marvel-logo.jpg


Get ready for blazing fast data transfer from a single chip for all cell communication networks.

 

Marvell Co-Founder Weili Dai proclaimed, "The World Modem is another game-changing breakthrough...  As a leader in China's 3G standard TD-SCDMA technologies, Marvell has enabled the delivery of a wide array of affordable, advanced consumer devices – including smart phones, tablets and mobile hot spot devices – to China, the world's largest mobile market. Building on that foundation, Marvell is now leading the way to a new era of seamless global connectivity for the masses with the industry's first single chip 2G/3G/4G modem with support for FDD-LTE, TDD-LTE, HSPA+, TD-SCDMA, and EDGE."

 

Combining 3GPP R9 Cat 4 FDD-LTE (Frequency Division Duplexing Long Term Evolution) and TDD-LTE (Time Division Duplexing Long Term Evolution) with R8 DC-HSPA+ (Dual Carrier Evolved High-Speed Packet Access) for both WB-CDMA (Wideband Code Division Multiple Access) and TD-SCDMA (Time Division Synchronous Code Division Multiple Access) standards and EDGE (Enhanced Data rates for GSM Evolution) will deliver the highest data rate available in any given geography.

 

Dai continues on about the new single-chip world modem and its future applications, "I envision a time soon when a truly affordable global communications network helps to bring our world closer as consumers from every walk of life enjoy uninterrupted access to all services, applications and the worldwide cloud from any device they choose anywhere they roam. I am proud of Marvell's global team of engineers for their pioneering work and I am excited by all the potential applications our customers will have to use this versatile and affordable new technology to make the world a better place for everyone." This low-cost extremely versatile and reliable modem is easily adaptable to any network so keep your eyes peeled at Marvell.

 

It looks like WiMax is the loser in the 4G race, according to Marvell.

 

Eavesdropper

0

Announced as ‘ground-breaking’, a new wireless sensor system for industrial measurement and control has been announced by the Deeter Group.

600x600 - Deeter Wirless Sensor System.JPGAt the centre of the new system is the simple-to-use basestation, designed to receive data from remote wireless devices such as the Deeter liquid vertical sensor (LVCS-RF). The basestation converts remote sensor input signals into industry standard process outputs. The basestation acts as the coordinator for an IEEE 802.15.4 wireless sensor network. It operates on one of 16 radio frequency channels available in the 2.4GHz ISM band. The high-power transceiver can achieve a range of greater than 1km, subject to local environmental factors. The internationally recognised IEEE 802.15.4 protocol allows several wireless sensor networks to share the same wireless spectrum without interference.

 

The basestation provides four open-collector transistor outputs which may be used to drive external relays for pumps and alarms or Deeter’s dual-level controller. Continuous analogue sensor data such as liquid level is output using a 4 to 20mA current-loop driver which enables interfacing with industrial process controllers or the Deeter Group’s range of current-loop indicators. A serial communications channel provides full-duplex RS232 and half-duplex RS485 transceivers allowing software to be developed for linking to PCs, data-loggers, PLCs or other proprietary equipment.

 

The basestation has three internal push-button switches and a 2-line by 16-character LCD. The buttons are accessible with the lid removed and are used in conjunction with the display to select installation options during initial setup. Once the system has been installed it will continue to operate without any further need for user intervention. The Base Station is housed in a rugged ABS enclosure with an external antenna. It has cable glands for power input and signal outputs and is supplied with an external, wall mounted, universal AC input power supply.

The LVCS-RF is designed to measure a continuous liquid level and transmit this information by radio to a Deeter wireless basestation at regular intervals. The device is battery powered and transmits wireless sensor data using the IEEE802.15.4 protocol operating in the 2.4GHz frequency band. The transmission range is up to 1Km in ideal line-of-sight conditions. The operating temperature range is -20C to +70C.

The LVCS-RF circuitry is housed in an IP65 rated die-cast aluminium head with an external antenna. An optional 3m extension lead and bracket are available for mounting the antenna in a position more favourable to wireless communication should the need arise. The sensor circuit is fitted inside a food industry standard 316L stainless steel tube attached to the head, with a 55mm magnetic ball-float. Standard sensing lengths are 250mm, 500mm, 750mm and 1m. Custom lengths and materials are available on request, says the company.

0

With the switch over to digital television, a now-painless transition in hindsight, the 50 - 700 Mhz bands were freed. This band was absorbed into what is known as White Space, all un-used frequencies allocated to broadcasting services, but not locally used (wikipedia). Eight companies, Microsoft, Google, Dell, HP, Intel, Philips, Earthlink, and Samsung Electro-Mechanics, formed the White Space Coalition (WSC) and set out to use the frequencies to deliver high speed internet in 2009. Their efforts were temporarily slowed by the FCC due to strict emission rules that make Wi-Fi devices useless. Further issues arise as the National Association of Broadcasters claimed the proposed devices used in accessing the internet through the spectrum had been proven to interfere with the television channels. A lawsuit has been filed in the matter.

 

Eventually the WSC will provide wide range internet through the white space. In places where broadband is limited, spotty, or non-existent (rural areas for example) the new service will reach. This tech will have a greater reach than all WiFi or cellular signals can achieve. The FCC has approved the concept of internet in those frequencies, we just have to wade through the red-tape and compliance problems first. A monumental internet access change is imminent.

 

A thought occurs; remember pirate television? Where people would try and broadcast video over the regular television channels. Since all the stations are somewhat free at the moment, is it a playground for pirate television? Now I have to find an old TV-set.

 

One of the greatest such hijacks was from 1987 during a Doctor Who show on WTTW (Channel 11 in Chicago). I was actually watching that very show. For censor purposes, I am only adding a link to that hijack. This was not recorded by me, I did not have a VCR at the time. It was too expensive. Thankfully, someone did capture the moment. Those were good days, indeed.

 

Cabe

4

2way2.JPG2way1.JPG

 

Two way, simultaneous, wireless communications over a single channel has been demonstrated by Stanford's researching engineers Jung Il Choi, Mayank Jain, and Kannan Srinivasan.



"Textbooks say you can't do it," said Philip Levis, assistant professor of computer science and of electrical engineering. "The new system completely reworks our assumptions about how wireless networks can be designed." But wait, I can talk and listen on my cell phone! The research team claims the way companies achieve this effect is much more costly and cumbersome than there method.

 


Transmission of a radio signal is much more powerful than what the device needs to listen to. Levis explains, "When a radio is transmitting, its own transmission is millions, billions of times stronger than anything else it might hear [from another radio], It's trying to hear a whisper while you yourself are shouting." They defeated this issue with a simple idea: "What if radios could do the same thing our brains do when we listen and talk simultaneously: screen out the sound of our own voice?" Similar to noise cancelling headphones, the transmitter filters out what it is sending. Immediately the incoming signal can be heard.



Levis explains a major use of the technology in the future, " With current systems, if two aircraft try to call the control tower at the same time on the same frequency, neither will get through. Levis says these blocked transmissions have caused aircraft collisions, which the new system would help prevent."

The now patented technology has the potential to double data rates in every communication system. The team continues to work towards extending the range and power of their device.



Eavesdropper