Skip navigation

community

Wireless

15 Posts tagged with the wireless tag
2

35626web.jpg

Ashutosh Sabharwal (via Rice University)

 

Full duplex Wireless Communication means getting your cake while you're eating it too. Ashutosh Sabharwal, a brilliant professor from Rice University, has made an amazing breakthrough in wireless data communications world of possibilities. The concept is like two people screaming at the same time in a large arena very far away from each other, but how can they hear each other? The answer is canceling out the sound of the screams coming from the sender so that the only sound they can hear is the sound of the other person's voice.

 

Sabharwal explained, "We send two signals such that they cancel each other at the receiving antenna -- the device ears. The canceling effect is purely local, so the other node can still hear what we're sending." These extra antennas send out canceling frequencies from the sending receiver.

 

Sabharwal continued, "We repurposed antenna technology called MIMO, which are common in today's devices. MIMO stands for 'multiple-input multiple-output' and it uses several antennas to improve overall performance. We took advantage of the multiple antennas for our full-duplex scheme, which is the main reason why all wireless carriers are very comfortable with our technology."


 

Rice University's idea was conceived and tested some months ago.

 

 

Now the team is back with a new goal, Sabharwal stated that their technology could be added to all cell towers, and no additional structures will be needed.  They have already "attracted the attention of just about every wireless company in the world." No wonder, the possibility of doubling the data throughput is quite exciting.

 

This technology will not be available until carriers upgraded their speed to "4 1/2G" or "5G" speeds, but the team is hopeful that this will be available in the next couple of years. Sabharwal is head of the WARP project at Rice University the acronym WARP stands for wireless open-access research platform. This enables them to be able to experience full-duplex wireless communication.

 

Eavesdropper

0

marvel-logo.jpg


Get ready for blazing fast data transfer from a single chip for all cell communication networks.

 

Marvell Co-Founder Weili Dai proclaimed, "The World Modem is another game-changing breakthrough...  As a leader in China's 3G standard TD-SCDMA technologies, Marvell has enabled the delivery of a wide array of affordable, advanced consumer devices – including smart phones, tablets and mobile hot spot devices – to China, the world's largest mobile market. Building on that foundation, Marvell is now leading the way to a new era of seamless global connectivity for the masses with the industry's first single chip 2G/3G/4G modem with support for FDD-LTE, TDD-LTE, HSPA+, TD-SCDMA, and EDGE."

 

Combining 3GPP R9 Cat 4 FDD-LTE (Frequency Division Duplexing Long Term Evolution) and TDD-LTE (Time Division Duplexing Long Term Evolution) with R8 DC-HSPA+ (Dual Carrier Evolved High-Speed Packet Access) for both WB-CDMA (Wideband Code Division Multiple Access) and TD-SCDMA (Time Division Synchronous Code Division Multiple Access) standards and EDGE (Enhanced Data rates for GSM Evolution) will deliver the highest data rate available in any given geography.

 

Dai continues on about the new single-chip world modem and its future applications, "I envision a time soon when a truly affordable global communications network helps to bring our world closer as consumers from every walk of life enjoy uninterrupted access to all services, applications and the worldwide cloud from any device they choose anywhere they roam. I am proud of Marvell's global team of engineers for their pioneering work and I am excited by all the potential applications our customers will have to use this versatile and affordable new technology to make the world a better place for everyone." This low-cost extremely versatile and reliable modem is easily adaptable to any network so keep your eyes peeled at Marvell.

 

It looks like WiMax is the loser in the 4G race, according to Marvell.

 

Eavesdropper

0

Announced as ‘ground-breaking’, a new wireless sensor system for industrial measurement and control has been announced by the Deeter Group.

600x600 - Deeter Wirless Sensor System.JPGAt the centre of the new system is the simple-to-use basestation, designed to receive data from remote wireless devices such as the Deeter liquid vertical sensor (LVCS-RF). The basestation converts remote sensor input signals into industry standard process outputs. The basestation acts as the coordinator for an IEEE 802.15.4 wireless sensor network. It operates on one of 16 radio frequency channels available in the 2.4GHz ISM band. The high-power transceiver can achieve a range of greater than 1km, subject to local environmental factors. The internationally recognised IEEE 802.15.4 protocol allows several wireless sensor networks to share the same wireless spectrum without interference.

 

The basestation provides four open-collector transistor outputs which may be used to drive external relays for pumps and alarms or Deeter’s dual-level controller. Continuous analogue sensor data such as liquid level is output using a 4 to 20mA current-loop driver which enables interfacing with industrial process controllers or the Deeter Group’s range of current-loop indicators. A serial communications channel provides full-duplex RS232 and half-duplex RS485 transceivers allowing software to be developed for linking to PCs, data-loggers, PLCs or other proprietary equipment.

 

The basestation has three internal push-button switches and a 2-line by 16-character LCD. The buttons are accessible with the lid removed and are used in conjunction with the display to select installation options during initial setup. Once the system has been installed it will continue to operate without any further need for user intervention. The Base Station is housed in a rugged ABS enclosure with an external antenna. It has cable glands for power input and signal outputs and is supplied with an external, wall mounted, universal AC input power supply.

The LVCS-RF is designed to measure a continuous liquid level and transmit this information by radio to a Deeter wireless basestation at regular intervals. The device is battery powered and transmits wireless sensor data using the IEEE802.15.4 protocol operating in the 2.4GHz frequency band. The transmission range is up to 1Km in ideal line-of-sight conditions. The operating temperature range is -20C to +70C.

The LVCS-RF circuitry is housed in an IP65 rated die-cast aluminium head with an external antenna. An optional 3m extension lead and bracket are available for mounting the antenna in a position more favourable to wireless communication should the need arise. The sensor circuit is fitted inside a food industry standard 316L stainless steel tube attached to the head, with a 55mm magnetic ball-float. Standard sensing lengths are 250mm, 500mm, 750mm and 1m. Custom lengths and materials are available on request, says the company.

0

With the switch over to digital television, a now-painless transition in hindsight, the 50 - 700 Mhz bands were freed. This band was absorbed into what is known as White Space, all un-used frequencies allocated to broadcasting services, but not locally used (wikipedia). Eight companies, Microsoft, Google, Dell, HP, Intel, Philips, Earthlink, and Samsung Electro-Mechanics, formed the White Space Coalition (WSC) and set out to use the frequencies to deliver high speed internet in 2009. Their efforts were temporarily slowed by the FCC due to strict emission rules that make Wi-Fi devices useless. Further issues arise as the National Association of Broadcasters claimed the proposed devices used in accessing the internet through the spectrum had been proven to interfere with the television channels. A lawsuit has been filed in the matter.

 

Eventually the WSC will provide wide range internet through the white space. In places where broadband is limited, spotty, or non-existent (rural areas for example) the new service will reach. This tech will have a greater reach than all WiFi or cellular signals can achieve. The FCC has approved the concept of internet in those frequencies, we just have to wade through the red-tape and compliance problems first. A monumental internet access change is imminent.

 

A thought occurs; remember pirate television? Where people would try and broadcast video over the regular television channels. Since all the stations are somewhat free at the moment, is it a playground for pirate television? Now I have to find an old TV-set.

 

One of the greatest such hijacks was from 1987 during a Doctor Who show on WTTW (Channel 11 in Chicago). I was actually watching that very show. For censor purposes, I am only adding a link to that hijack. This was not recorded by me, I did not have a VCR at the time. It was too expensive. Thankfully, someone did capture the moment. Those were good days, indeed.

 

Cabe

3

solar-contactless-charging-table-panasonic-1.jpgsolar-contactless-charging-table-panasonic-2.jpg

 

Add a little art-deco, some solar panels, and a special battery and starts inductively charging devices. Panasonic is releasing a small charging table, which looks like something that belongs at a coffee shop, sometime this year in Japan. The key to this table, no need for 3rd party adapters and accessories. The inductive charging coupling circuit will be built into the battery. Place a phone on the table, it will charge. Place a bare battery on the table, it will also charge. Panasonic may produce batteries for the world's most popular phone to work with their table, and the tech may be licensed out. The solar panels allow the table to be moved anywhere. However, in most cases outdoor tables have umbrellas over them. However, some indoor light energy could be recovered by these tables.

 

The table was demonstrated at the Retail Tech Expo in London. Another example of the new environmental conscious Japan.

 

Eavesdropper

0

everyday.JPG

I have to know how you all feel about broadcasting your every move on the internet, do you do it? Foursquare, Facebook, etc let's everyone know where you are and what you are up to. In some cases, giving criminals ample information to rob your house or find your for some nefarious reason. But in an ideal, happy, rainbow, world that isn't a concern. It is actually fun to become "mayor" of the local coffee shop. A new company is going to challenge how far you are willing to go. Green Goose is allowing you to place wireless transmitters on everything you move in a type of real world/online game. You can score points by brushing your teeth at a particular time, drinking enough water, exercise, take vitamins, etc in hope to "level up." Founder Brian Krejcarek hopes to partner with real world companies to give away prizes and gifts based on your performance. For now though, your efforts are just to be "top player." Each wireless transmitter costs $4 each, and will start being available Feb 28th 2011. It looks as though the transmitting devices may be RFID and/or Zigbee. The idea does sound like a good way to stay motivated. See more at their website.


Eavesdropper

4

2way2.JPG2way1.JPG

 

Two way, simultaneous, wireless communications over a single channel has been demonstrated by Stanford's researching engineers Jung Il Choi, Mayank Jain, and Kannan Srinivasan.



"Textbooks say you can't do it," said Philip Levis, assistant professor of computer science and of electrical engineering. "The new system completely reworks our assumptions about how wireless networks can be designed." But wait, I can talk and listen on my cell phone! The research team claims the way companies achieve this effect is much more costly and cumbersome than there method.

 


Transmission of a radio signal is much more powerful than what the device needs to listen to. Levis explains, "When a radio is transmitting, its own transmission is millions, billions of times stronger than anything else it might hear [from another radio], It's trying to hear a whisper while you yourself are shouting." They defeated this issue with a simple idea: "What if radios could do the same thing our brains do when we listen and talk simultaneously: screen out the sound of our own voice?" Similar to noise cancelling headphones, the transmitter filters out what it is sending. Immediately the incoming signal can be heard.



Levis explains a major use of the technology in the future, " With current systems, if two aircraft try to call the control tower at the same time on the same frequency, neither will get through. Levis says these blocked transmissions have caused aircraft collisions, which the new system would help prevent."

The now patented technology has the potential to double data rates in every communication system. The team continues to work towards extending the range and power of their device.



Eavesdropper

0

DSC04562low.jpg

Imec saw a need in the market, inexpensive digital interface for radio networks, and filled it. With their development it looks like LTE has won the battle for 4G supremacy. The accelerated deployment of broadband personal communication coupled with the continuously increasing demand for large data rates results in an increasing spectrum scarcity. A dynamic access to the available spectrum would increase the throughput efficiency significantly. In licensed bands scenarios, dynamic spectrum access would for example allow personal mobile terminals to seamlessly set-up and maintain a reliable wireless connection. In unlicensed bands (the crowded 2.4 GHz band), it would bring great added value to products for which interruptions in the connectivity cannot be tolerated, for safety reasons in a control system (surveillance camera’s), or for comfort reasons in real-time applications (wireless conferencing, hearing aids,...) as it would improve connectivity even in the presence of many competing and interfering networks. Imec’s new spectrum sensing component was designed as a versatile digital engine to meet a wide variety of use cases, at low cost and low power overhead. The chip, which hosts a dedicated ASIP (application-specific integrated processor), can perform both flexible synchronization and spectrum sensing for high-throughput WLAN (802.11a-n), cellular standards (including the recent 3GPP-LTE), and digital broadcasting standards. The novel spectrum sensing component connects to imec’s in-house designed analog reconfigurable radio chip (SCALDIO) and imec’s programmable digital baseband platform conceived for 4G seamless connectivity (COBRA). As such, imec’s complete reconfigurable radio solutions enable multimode communication with efficient use of the spectrum.


Eavesdropper

0

3-D movies on cell phone

Posted by Eavesdropper Feb 15, 2011

mwc20113dfil.jpg

At the Mobile World Congress in Barcelona, German researchers demonstrated a mobile radio standard of LTE-Advanced video coding techique called Multiview Video Coding (MVC). The goal is 3D films on cell phones. Despite recent reports of children and adults having eye strain from using the Nintendo 3D gaming device the 3DS, Researchers  at the Fraunhofer Institute for Telecommunications,  Heinrich-Hertz-Institute, HHI in Berlin have decided to go ahead on this project. The have created a compression algorithm that works well with HD video. Thomas  Schierl is a scientist at the HHI explains, “MVC is used to pack  together the two images needed for the stereoscopic 3-D effect to  measurably reduce the film's bit rate,.The 2-D and 3-D bit streams  divided up by MVC can be prioritized for each user at the air interface  to support different services, thus opening up a completely new field  for business models.” A novelty or a new standard indeed, it's going to happen.


With Sprint possibly switching from WiMAX to LTE, this will most definitely be in our forecast.


Eavesdropper

0

Bell_Labs_Antenna_CUBE.jpg

 

The world of mobile communications moves fast. With new mobile devices, new applications and ever-growing and changing consumer demands the wireless networks in use today have to evolve. Rather than take an incremental approach to meet these challenges, Bell Labs took a leap and developed a radically new approach to wireless technology. In order to do this, Tod Sizer, head of Bell Labs Wireless Research, challenged his team to think not just ‘outside the box’, but to think ‘inside the cube’. In six short months, the team developed a cube-shaped antenna that would fit in the palm of a hand, and was ready to test it with customers. “There are many different types and sizes of base stations, from very small to very large, depending on where they are located, such as in an urban or rural area. I realized that we needed to design a new and flexible type of antenna array for different environments - including one designed to the smallest possible size ( ‘invisible antennas’) in order to be flexible enough to meet the growing needs of all of our wireless service provider customers,” said Sizer. A radio antenna element is a component of an antenna system that transmits signals from the wireless base station to a wireless end-user using a mobile phone, smart device or laptop. By reducing the size of the element itself, an antenna array can be scaled to fit any wireless need simply by adding more of these elements to the array. Bell Labs wireless researchers weren’t daunted by the challenge of building something that was roughly ten percent of its current size. Several wireless research teams in Stuttgart and Ireland focused on different aspects of the problem, combining their unique areas of expertise to quickly resolve a myriad of technical challenges to reduce the antenna element’s size, improve energy efficiency and lower manufacturing expenses. The clever architecture of this new antenna is but one of the innovations critical to realizing Alcatel-Lucent’s unique lightRadio portfolio.


Eavesdropper

0

73099.jpg

 

A perimeter-protection system created by a team from the USC Viterbi School of Engineering took Best Paper prize at the IEEE Homeland Security Conference in November 2010, and is now moving to deployment at a Florida airport, while also being considered for further installations by the Transportation Security Administration.  This smart sensor system recognizes spatio-temporal sensor patterns of perimeter intrusion by foot, by fence, and by vehicle for the purpose of protecting remote fenced or virtual perimeters against unauthorized access or terrorist attack on TSA airport property. The system’s novel approach allows target intrusion sounds to be identified by users with specific needs. For example, at airports, the sensors were trained to ignore typical fence manipulation (kicking, leaning, shaking) by visitors who gather at end-of-runway fence lines and watch landings and take-offs. However, the system actively raises alerts if the fence is climbed or if someone attempts to breach the perimeter. In turn, the ground sensors ignore the presence of large jets, but raise alerts for human footsteps in unauthorized areas and can be programmed to either raise alerts or to simply report the presence of vehicles in certain protected areas. For more information please visit: http://viterbi.usc.edu/news/news/2011/smart-usc-fences.htm


Eavesdropper

0

mattel-hot-wheels-video-racer-1.jpg

 

At this year’s Computer Electronics Show in Las Vegas, toy company Mattel Inc. unveiled a unique and creative way to use a video camera.  They put a miniature camera into a Hot Wheels car that captures up to 60fps of video, so that you, or anyone else can see what it’s like to drive a car at 1:64 the scale.  In other words, you will have the point-of-view of a Hot Wheels driver without using a shrink-ray. You can watch the video from the car on either a TV or PC thanks to a USB cable, and if you have neither, the car also has an LCD screen on the bottom that you can watch from. The car also has on-board memory but can only hold about 12 minutes of video. The Video Racer will be available this fall for around $59.99. This brings me back to when I was a kid and wanted to be able to drive my basket full of awesome vehicles. Then again, my Hot Wheels always ended up crashing from the seemingly impossible 2 story jumps off of the second floor of my parent’s house. Check out the video for Mattel’s demonstration. For more information visit: http://www.mattel.com/


Eavesdropper

0

OpenPicus, the italian open source platform made for wireless smart sensors and actuators, definitely takes off with a thick list of juicy news ready to be downloaded on 20th Jan 2011 (10am italian time)


The open source platform is mature and offers to the developers:

  • The new IDE, easy to use and Free to download
  • Software Framework: your Apps can control the functions of the Protocol and of hardware, but you don't need to be an expert of both.
  • Apps Source Code (such as wireless Webserver)
  • Video guide for the IDE and a Manual for the Framework

openpicus LOGO.jpg

OpenPicus started in March 2010, it was just an idea and a Blog. Today FlyPort module (the first Wi-Fi smart module, AKA Picus) is more and more the core of lot of Wireless applications, from sensors to robotics. Very innovative the smart Campus program: they give FREE Starter kits for Universities.

 

 


 

0

Looking for a small form factor to connect your embedded design to Internet ?

 

The Flyport open source plaform enable riskfree development, royalty free TCP/IP libraries usage.

It is based on the FCC certified WiFi module MRF24WB0MA.

 

To get immedialtely started with Flyport just download all what you need from Openpicus community.

 

regards

1

From Microwave Engineering

By Jean-Pierre Joosting

Microwave Engineering

Octorber 21,2009

Cambridge, UK — Cambridge Consultants has unveiled VenaHub, a data collection and aggregation system that promises to simplify personal health management in a connected health environment. VenaHub employs a small pocket device to capture data from a user's ecosystem of wireless medical devices, which it then integrates into a customisable online health information portal.

 

Anticipating growing consumer demand for low-cost home health management devices, this launch addresses the need for a simple, consumer friendly and cost effective means to enable proactive self-management of chronic diseases. The system builds on the momentum of a Vena-enabled inhaler prototype launched by Cambridge Consultants in spring 2009, and the deployment of Vena-enabled weight-scales and blood pressure monitors by A&D Medical in August 2009.

 

"Current solutions in the telehealth space are expensive, which means none of the parties involved want to pay for them, whether they are an insurer, hospital or patient," said Mike Dunkley, Vice President at Cambridge Consultants. "But the novel, compact, and portable VenaHub is cheap and can plug into the USB port of any PC. Critically, it can also collect data from devices even when it's not plugged into a computer. This technology could not only disrupt the current medical home market, but could overcome the reimbursement barrier that has prevented connected health solutions from being widely deployed."

 

The vision for VenaHub's web interface is much like an app-enabled phone or PDA where users would be able to customise different applications to suit their own needs and conditions. These applications could be created by the device makers themselves, or by third parties who develop meaningful and engaging applications using patient-specific or helpful corollary medical or wellness information.

 

For example, an asthmatic patient could tailor their portal to see various types of information — charts of their recent inhaler use, reminders for refilling prescriptions or doctor's appointments, lung function data via a peak flow chart — all juxtaposed against the coming week's pollen forecast.

 

The wireless technology at the core of VenaHub is based on Cambridge Consultants' Vena wireless healthcare device platform, which implements the standards selected by the Continua Health Alliance to empower patients to manage health and wellness anytime, anywhere. It embeds the Bluetooth™ Health Device Profile (HDP) optimised for the secure transport of medical data, onto a single chip at an affordable price.

 

Vena also offers the IEEE 11073 standards for compatible exchange of information between health devices. VenaHub demonstrates how simple wireless technologies can be deployed to provide consumers with a tool they can use effectively at home with minimal effort and expense to manage chronic conditions like diabetes or Congestive Heart Failure as well as interact with their healthcare network. VenaHub can also be used for fitness and wellness applications.