Load Google Translate If you need help on anything technical relating to VCC or Optoelectronics products, please post your question here!
Don't forget to sign up for email notifications under the "Actions" box so you'll see when I answer your question.
I have extensive experience with Electro-mechanical assembly as well as significant knowledge of optoelectronics.
If not already, you'll need to or ![]()
to ask your question. Otherwise, click reply below. |
Hello Orlando
I am constructing a visual light communication system for indoor communication. My transmitter is an RGB LED panel (50 LEDs for now am planning to make a bigger panel) mounted on the ceiling and serial data is modulated onto the LED light. The three colors in the LED are for creating three communication channels that can be separated by the use of color filters at the receiver. The receiver is placed at the table top about 2 m from the ceiling. I had been using a photo transistor that is part of a photo interruptor at the receiver side and displaying the data onto a computer. It is working fine upto 28800 bps but only after the light is focused by the use of a convex lens onto the detector so difficult when the receiver is mobile.
I need a detector (photo diode or photo transistor whichever is better) that can give me some freedom in movement, the data rate of at least 14400 bps is enough for me. Could you suggest me a better option ?
Your help is appreciated..
Natasha
P.S. The area of movement is round about a square of side 200 cm.
Hello Natasha,
I understand your application, in short, light is being converted to a signal in order to display on a panel.
For example, a wall mounted map display with lights behind it indicating where calls are being made from.
Your best solution would be a photo-diode and National Semi has a great online design website which
will narrow down to what would fit best, http://www.national.com/analog/led. In the right-hand
box, WEBENCH Designer, click on Sensors, Photodiode Sensor, then My Design, and you
are set.
If you have any additional questions, please contact me.
Orlando
Hello Natasha,
I think, if I understood your issue correctly, this is due to not having enough light hitting the detector. There are number of factors that can paly a role here, starting from beam angle of the LEDs. The gain setting on the detector can also paly a role. As a check, you can take the detector closer to the light source and see if that helps. If it is the amount of light that is not sufficient for the detector, this test will help. If it helps, you can find a detector that has the feature to set the gain of the internal trans imp. amp (amplify the light before processing) externally and have the issue solved. Avago Tech or TAOS will have RGB sensors that you can use. I hope this helps.
Hello Orlando
Thanks for your suggestion. But the WEBENCH Designer does not have many photodiodes according to my requirement i.e. in visual range. Also it focuses on the design of amplifiers and ADC or DAC converters not the photodiodes.
natasha
P.S. I have attached the system block diagram and the experimental setup in this post. I am transmitting text from a PC to another PC.
Hello Muhinthan
I have attached the system block diagram and the experimental setup in this the post just before. If it is the issue of less light hitting the detector, will increasing the number of LEDs and using a detector with larger surface area solve the problem in some extent ?
Thanks
Natasha
Hi Natasha,
I would start with taking the detector closer to the LEDs and see if that makes any improvements. Can you tell me what LED are you using? Also, having a 2m distance between the source and detector makes me think that unless you have a very narrow view angle LED, it will be difficult to direct all the light to the detector without the use of some kinds of collimator. Let's start with what I have said and we can go from there.
Muhinthan
Hallo Orlando,
i'm a FSE at Farnell.
So many times customers coming up with a question about a component they are currently investigating for.
I still don't know a good portal to search ( and find ) components by specs.
I.E. a customer is lookig for an Infrared LED with high output
- roundabout 740nm
- fast <= 12-15ns
- 100mA
any idea or suggestions ?
thx in andvance
Cheers
Goetz
Hallo Goetz,
Currently there seems to be only one LED search portal available, it is
thru www.globalspec.com
Other than that, Google seems to be your best option.
Best regards,
Orlando
HI Orlando;
I am trying to identify a small laser that I can use to position a small router tool or drill. Ideally the spot needs to be 1mm or less and adjustable focus between 10 – 20 mm. The machine chuck can accept 8mm diameter bits but we can manufacture our own holder. Would you be able to suggest a suitable part for this application?
Thanks.
Hello Orlando
I am looking for an 850nm optical receiver (ST connector) that has an output that changes state when the optical power received is below a threshold level. The thershold level must be adjustable. This is needed to monitor the optical link and detect if the link degrades due to aging or other fault. There is an IC that could fit the bill, the ML4622 but I don't seem to be able to find a supplier or any pricing information. can you recommend an alternative?
Regards
Nico
Hallo Natasha,
which kind of "modulation" do you perform to get the data onto the LED current?
Maybe you could increase the sensitivity by using a clever method of modulation.
Are you using any kind of hand shaking?
Greets Ingo.
Dear Orlando
I would appreciate if you could give some advice on Fiber optic temperature measurement sensors and converters. We are interested to know if Newark has any experience with these and what the pros and cons may be.
We have applications in MV power electronics and these appear to give good isolation and reliable readings.
Paul
Bonjour Orlando,
Je travaille actuellement sur une tourelle laser pour la Coupe d'Europe de Robotique. En fait, un laser est installé sur un moteur, et tourne à une vitesse d'environ 10Hz.
Mon probleme est la reception de ce laser avec un circuit simple (c'est un prototype, le circuit réel sera fait avec une photodiode et un circuit compliqué).
Le laser illumine le phototransistor (mon choix actuel) durant 30 µs environ.
Je dois détecter cette lumière (650nm) et faire un front montant en 5V.
Connaissez vous un CI ou un circuit simple qui puisse m'aider ?
Merci
Cordialement,
--------
Hello Orlando,
I am working on a turret laser for the European Robotic Cup. In fact, a laser is mounted above a motor and turn at about 10 Hz.
My problem is to receive this laser with a simple circuit (it's a prototype, the real circuit will be made with a photodiode and a complicated circuit).
The laser illuminates the phototransistor (my present choice) during about 30 µs.
I have to detect this illumination (650nm) and make a 5V rising edge output.
Do you know a IC or circuit that can help me ?
Thank you
Best Regards,
© 2009 Premier Farnell plc. All Rights Reserved
Premier Farnell plc, registered in England and Wales (no 00876412), registered office: Farnell House, Forge Lane, Leeds LS12 2NE