Skip navigation

community

4971 Views 14 Replies Latest reply: Aug 16, 2011 10:03 PM by lahcen005 RSS
Currently Being Moderated

Aug 16, 2010 9:58 AM

mbed review - summary

mbed.jpgWhat advantages does the mbed offer, and what are its limitations?


I’ve already covered my experiments with the mbed in some detail, but here I’ll try to summarise.

The mbed is aimed at people who want a fast way to prototype micro-controller applications.
Getting  started is as easy as the mbed ad claims; I had the sample blinking LED  program running within a minute of opening the box. Another two  minutes, and I’d modified the code, compiled and downloaded it, and was  watching all four LEDS blink in sequence.

There’s  more to life than blinking LEDs, and it took some while to explore the  mbed’s capabilities. I quickly felt comfortable with the development  environment, from which you can create, edit, install and publish your  code, and import code published by others. The development process is as  simple and smooth as it is with the Arduino. Since the compiler is  web-based there is no software setup and you know you are always using  the latest version of the development environment.

Like  the Arduino development environment, the mbed has no debugger. I found  myself making liberal use of printf statements which output via the USB  link to the PC.

The  web-based compiler is reached from the mbed wiki. There is a lot of  content but the wiki is well-structured and easy to navigate. The wiki  contains
  • forums for queries, help, bug reports and suggestions for improvement,
  • a handbook section which documents the mbed’s core libraries,
  • a cookbook where users can publish additional code and
  • notebooks where users can document work in progress and publish if they wish.
The  forums are lively, friendly and helpful. The mbed team are quick to  respond to questions and comments, and there are a lot of other  experienced users who are happy to share their expertise. The  signal-to-noise ratio in the forums is very high.

The  libraries are generally of high quality and the documentation is  excellent. The mbed team have set the bar high and contributors have  tried to match their standard. Core libraries cover most of the mbed’s  peripherals, including I2C, SPI, CAN, Ethernet and the mbed’s local  filesystem. The LPC1768FBD100,551 has a few additional capabilities: some of these  (Quadrature encoding, I2S) have user libraries under development. User  libraries also cover common peripheral devices like LCDs, Port Extenders  and Sensors.

The  mbed’s capabilities gave me a much richer environment that I am used to  with the Arduino, and I found good use for the mbed’s greater memory,  flash capacity and speed.

Of  course the mbed has some limitations. Some potential users are anxious  about the need to store their source code on the web. Others are  concerned that the core libraries are not currently open source.  Publishing a library is not yet as smooth as it should be, and I found  no way of versioning my software.

There’s  been a steady stream of requests to open up the libraries, and it seems  that the delay is more to do with development priorities that with any  objection in principle.

Once  the libraries have been opened up it should be a simple matter for  developers to switch to the open-source gcc-based ARM toolchain if they  want. That in turn would open the door to debugger integration and to  the use of a multi-tasking kernel like FreeRTOS.

These  are exciting possibilities, but they are enhancements to an already  outstanding product. I expect to use the mbed as my preferred  prototyping platform for a long time to come.

Attributes

  • Currently Being Moderated
    1. Aug 17, 2010 5:03 AM (in response to romilly)
    Re: mbed review - summary

    Very good review alltogether, Romilly, much appreciated.

     

    Keep up the good work with possible future reviews and projects

     

     

    Elias

  • Currently Being Moderated
    3. Aug 24, 2010 4:01 AM (in response to romilly)
    Re: mbed review - summary
    Thanks Romilly, great review!
  • Currently Being Moderated
    5. Aug 24, 2010 4:28 AM (in response to romilly)
    Re: mbed review - summary

    Hi Romilly,

     

    I agree with you about the golden age for accessable hardware. I think it also opens up a really big question. Is the age of circuit design, if not over, relegated to a very specialist role? A step up from the mbed, Amicus etc are single board computers. These are getting more specialised, smaller and cheaper. Why spend the money creating a unique design when you could have a ready made board delivered to your workplace? Is software design the new embeded design? I know that for larger volumes making your own circuits will always be practical, but I think the cost barrier to using SBCs is being lowered all the time, so many medium/small volume designs could become practical with almost no hardware design at all

     

    I'm sure that shouldn't be a problem, I'll forward your request to our product guys

  • Currently Being Moderated
    7. Aug 24, 2010 5:39 AM (in response to romilly)
    Re: mbed review - summary
    You are correct about hobbyists, I've been very surprised with the amount I've come into contact with since element14 launched. In fact I am meant to be going to the Leeds Hackspace tonight
  • Currently Being Moderated
    8. Aug 24, 2010 10:33 AM (in response to Alistair Winning)
    Re: mbed review - summary

    Hi guys,

     

    I have a small CNC mill for PCB prototyping and SMD soldering equipment (everything hobbyist price class) so once I have my workshop set-up I can also join discussions in that area.

     

    I make the design with EAGLE and export it to g-code with Pcb-gcode.

     

    The miller is controlled with EMC2.

     

     

    Let me know if this would be useful.

     

     

     

    Elias

  • Currently Being Moderated
    10. Aug 24, 2010 10:55 AM (in response to romilly)
    Re: mbed review - summary

    Thanks, Romilly

     

    We just bought a house with my girl friend so I'm finally getting a proper space.

     

    Have to still stick some wallpaper on the insulation and put on vinyl flooring and then I can start filling it up with my toys

     

     

     

    Elias

  • Currently Being Moderated
    12. Aug 24, 2010 2:26 PM (in response to Alistair Winning)
    Re: mbed review - summary

    It would be good to hear what Hackspace Leeds is like

  • Currently Being Moderated
    13. Aug 25, 2010 3:10 AM (in response to Zad)
    Re: mbed review - summary

    Hi Mike,

     

    Something came up last night and I couldn't go. I will be there next week with a colleague. Here is the link to their site if you are interested in coming along http://leeds.hackspace.org.uk/meetups

  • Currently Being Moderated
    14. Aug 16, 2011 10:03 PM (in response to romilly)
    Re: mbed review - summary

    Great review keep-up the good work. I've worked with mbed board it was easy to use and to program. thank you

     

    Lahcen

Related Content


Related Products
Discussions
  • Retrieving data ...

Bookmarked By (0)