Load Google Translate hello there, those green laser effects at night clubs, concerts, fairgrounds etc, instead of being a straight beam and dot like a laser pointer they are dispersed in a kind of wide flat fan like effect, can anyone explain how this is achieved, i should add it appears constant not one beam being scanned accross rather the fan effect can be moved almost as if its a solid item when of course its just a light beam, thanks
The "skyscan" effect you are referring to, Is the result of the laser being bounced off of a mirror within the unit. It is yet one single beam, just mirrored off of a surface the is rotating at a very high rate of speed.
© 2009 Premier Farnell plc. All Rights Reserved
Premier Farnell plc, registered in England and Wales (no 00876412), registered office: Farnell House, Forge Lane, Leeds LS12 2NE