Skip navigation

community

667 Views 12 Replies Latest reply: Mar 19, 2012 12:20 PM by ehagerman2 RSS
Currently Being Moderated

Jul 14, 2011 2:02 PM

Have a question about solid state relays and their applications? Ask me!

If you need help on solid state relays and their applications, please post your question here by hitting "Reply"!


Make sure your personal email notifications preference is set up appropriately--so you'll see when Pete answers your question.

 

Pete Bamburak

 

Pete Bamburak

As the Field Applications Sales Engineer for Crydom North America, Pete offers 26 years of expertise and experience in solid state relay use and applications.


 

If not already, you'll need to

login_exprt3.png or register_exprrt3.png

 


to ask your question.

Otherwise, click reply below.

Attributes

  • To Pete,


    Hi i am a student from UTHM Malaysia currently i am doing a degree electrical and electronic research, so i might want to ask sir technically about solid state relay first is about the Switching Mode of the Solid State Relay. There are 5 types as shown in the Element14. so can Sir practically about all those type of mode in application uses?

     

    Such as:

    1) AC Switch

    2) DC Switch

    3) Non-zero crossing

    4) Random Turn On

    5) Zero Crossing

     

    i don't know which type suitable to my research product Mr Pete, but i prefer a switching mode that are able to response instantly to OFF the AC terminal when detect a low voltage signal on the DC terminal. Please let me know if Mr Pete have any ideas which type of switching mode relevant or suitable to my research...

     

    Thanks and regard,

    Vincent Lee

  • Sir Pete, thank for the information given above. your guidance is very professional and technical....

     

    however i would like to ask more questions about the as below:

     

    Relay Terminals

    Cage Clamp

    Push In

    Surface Mount

    Through Hole

     

    Contact Configuration

    SPST

    SPST-NC

    SPST-NO

     

    MSL

         MSL 2A - 4 weeks

     

    SVHC

    No SVHC (15-Dec-2010)

    No SVHC (19-Dec-2011)

    No SVHC (20-Jun-2011)

     

    these are the parameter when choosing the solid state relay property at

    http://my.element14.com/jsp/search/browse.jsp?N=2105+204034&Ntk=gensearch&Ntt=solid+state+relay&Ntx=mode+matchallpartial

     

    i am not very clear about these parameters when selecting the SSR, so i would like to ask Sir Pete for more simple and technical explaination...sorry for any trouble that i causes to you Sir.

     

    thank and regard

    Vincent Lee

  • Mr Pete,

    ok....thank Mr Pete

     

    so what is the different between SPST-NO, (single pole normally open and SPST-NC, (single pole normally closed)? sorry i cant found any relevant of this details on wiki or other sources. and again i would like to ask Mr Pete about this.

  • thanks Mr Pete,

     

    a very last question....the Load Current of the SSR mean the

     

    1)The SSR maximum load current of 12A which is in range 0-12A allow to load?


    or


    2)the SSR can allow only 12A current to the load?

     

    Regard

    Vincent Lee

  • What kind of SSR do I need for this application?  Is a 240V output too much to use on 110V device when my input is all 110V, using this device as a the on and off indicator.  SSR NEEDED.bmp

  • Thanks for the info Pete.  I will check out the Switches and Relays!

Related Content


Related Products
Discussions
  • Retrieving data ...

Bookmarked By (0)