Skip navigation

community

924 Views 2 Replies Latest reply: Jul 25, 2011 12:04 PM by MAb RSS
Currently Being Moderated

May 16, 2011 9:42 AM

Ready to participate to a robot design challenge?

It's like Legos for adults

 

"Make it Challenge" is the name of the contest launched by Freescale Semiconductor. This challenge will be part of the Freescale Technology Forum in  (June 20-23, 2011 -San Antonio).

During the on-site design competition, contestants will have the opportunity to participate in one of two tracks, Mechatronics Robot or Tower System,  each of which provides a different choice of tools with which to build an application. Contestants must complete 1 of 2 training classes  (online or onsite at FTF) and will then be given a certificate to select  tools and create their own unique design in the Make It Lab during FTF  Americas.

 

 

 

Each track will award one prize each to first, second and third place  winning contestants. A Grand Prize winning contestant will also be  selected from the two first prize winners.

 

What is the goal of the contest ?

Demonstrate your design & innovation skills, your creativity!  The Tower Mechatronics Board can be used in Freescale’s Mechatronics Robot kit, which competitors will use to create a cool, fun, walking, sensing operational robot in a 30-hour period. You'll use ColdFire and Kinetis ARM Cortex-M4  Microcontrollers, Freescale’s Tower ecosystem, CodeWarrior Development  Environment, IAR Embedded Workbench.

 

Freescale's Robot Kit that operates with the Tower System Mechatronics Board is an easy-to-use mechatronics development and demonstration platform. This toolset allows for the science of combining mechanics, electronics, and software into an integrated system. The kit includes four PWM controlled servos (actuators), metal legs, and the Tower System Mechatronics board that has a 3-axis accelerometer and a 12 channel touch sensor.  Through building the kit, you can experience what the 4 degree of freedom bipedal walking robot can do.   The Tower System Mechatronics board is programmable in C/C++ using CodeWarrior and an on-board OSBDM flash programming tool.  For fast prototyping or for individuals without C/C++ experience, the Tower System Mechatronics Board is supported by the Robot Vision Toolkit and RobotSee (a language as simple as BASIC with the power of C).

 

Want to register? http://www.freescale.com/makeitchallenge

 

Read an article on the Challenge on Freescale blogs here

 

Find more information on the contest on Freescale.com here

Attributes

Related Content


Related Products
Discussions
  • Retrieving data ...

Bookmarked By (0)

Legend

  • Correct Answers - 50 points
  • Helpful Answers - 25 points