Skip navigation

community

4151 Views 13 Replies Latest reply: Jul 28, 2011 8:19 PM by nidou113 RSS
Currently Being Moderated

Sep 1, 2010 8:12 AM

How to use GSM/GPRS module

Hi,

 

I am a student and I am working on a data acquisition board that would implement a GPRS?GSM module. I will use it to send messages to a mobile phone.

Can anyone suggest me a schematic or at least a good supported module.

I've been searching, but none of the devices found have a good documentation.

I would like to use an ATMEGA uController.

 

I have found a nice schematic but I do not understand it entirely.

 

Thanks for the help

Attachments:

Attributes

  • Currently Being Moderated
    1. Sep 1, 2010 1:29 PM (in response to muntean.n.a)
    Re: How to use GSM/GPRS module

    LS Research may help you.

    http://www.lsr.com/products/radio_modules/

     

    Also,

    Call the guys at NextGen RF in Weaseca MN, USA.  they can help too.

    http://www.nextgenrf.com/

     

    Good Luck ,

    bernard...

  • Currently Being Moderated
    2. Sep 9, 2010 12:41 AM (in response to muntean.n.a)
    Re: How to use GSM/GPRS module

    Hi, I saw your other post about this.

     

    The SIM300 is easy to use with the AVR devices. Pay careful attention to the datasheets for the SIM300 modules though as I see on the schematic for the link you posted that they connect +5V to the GSM module. This is likely to destroy it as the max voltage is 4.5V. Ideally you want to use 4.0V and this is what I use with the SIM300 modules and they work very well. They are remarkably cheap too.

     

    Be careful also on the TXD and any input lines etc as these are not rated for anything above 3.0V so use a resistor inline to limit the current with your micro running on 3.3V and you should eb OK. This has been working for me for a number of months wtih no issues.

     

    Driving them is easy and they have a very nice TCP/IP implementation so you can even use GPRS with the AVR with no need for a TCP stack on the AVR. Just use AT commands to setup the PPP dialup over GPRS and then the TCP connection to whatever you want to connect to.

     

    If simply want to send and receive SMS, then that is just as simple to do via the AT commands.

     

    Good luck with your project. If you get it all working you will learn valuable leasons on how to get a GSM module to work with microcontrollers. There is lots of potential for remote applications once you do.

     

    Regards,

    Dave...

  • Currently Being Moderated
    4. Sep 9, 2010 8:01 AM (in response to muntean.n.a)
    Re: How to use GSM/GPRS module

    Hi Andexandru,

     

    Which country are you located in?

     

    I am located in Indonesia and use a supplier from Singapore. (I am an expat from Scotland living and working here)

     

    Simcom have a very large worldwide network of distributors who you should be able to purchase from, hopefully there is one local to you saving you from purchasing overseas.

     

     

    Dave...

  • Currently Being Moderated
    6. Sep 13, 2010 8:24 AM (in response to muntean.n.a)
    Re: How to use GSM/GPRS module

    Check with the distributor as I was told that some SIM300 models are on end of line.

     

    If you want a DIP type, the nearest you will get is the SIM300C or SIM340C (Quad band) which have 1.27mm pitch connectors. The SIM300D is not recommended for hand soldering as the antenna connections are under the unit and require reflow soldering. It is much smaller than the other modules.

     

    I have managed to solder the 0.5mm pitch connector for the SIM300 and SIM340. You just need a good soldering iron and some solder wick to clean them up.

     

    Your prices sound about right for the region. Is this from a Romanian distributor?

     

    Dave...

  • Currently Being Moderated
    8. Sep 13, 2010 4:46 PM (in response to muntean.n.a)
    Re: How to use GSM/GPRS module
    i have a good ebook about GSM and the microcontroller ,but it's in french
  • Currently Being Moderated
    9. Sep 13, 2010 11:21 PM (in response to muntean.n.a)
    Re: How to use GSM/GPRS module

    Hi Alexandru,

     

    They all seem to be very similar hardware wise but please check the datasheet for the one you want to use and make sure you follow the guidelines.

     

    For control, you need the following as a minimum:

     

    Power ON control (use the circuit they provide in the HW manual. Do not connect an IO pin direct the module as the input has to be open collector)

     

    LED status out. Design this in as it allows you to see what the module is doing. The LED is great for feedback as it pulses during data connections and during network registration.

     

    Use RTS and CTS if you can but I have it working without. Depends on your processor speed. I have TCP/IP working at 57600 bps without any issues.

     

    Watch your IO pins from the processor to the modem to make sure the limits are not exceeded. If you processor is running at 5V DO NOT connect direct to the GSM module. The Analog Devices ADMU bus isolators are ideal for this. I use them with a Telit modem and it works perfectly. You can power the ADMU from the VDD output from the modem as this will be at the same voltage as the IO pins.

     

    Good luck.

    Dave...

    PS.. When you do your software, write code to read the registration onto the network and read the signal strength. If the module is not registered, sending SMS or trying to connect over GPRS will not work. It takes a few seconds from power on before the module is registered on the network.

  • Currently Being Moderated
    12. Sep 15, 2010 10:16 AM (in response to muntean.n.a)
    Re: How to use GSM/GPRS module

    It's a french ebook;

     

    here is the link :http://hotfile.com/dl/68939447/17bdd46/algeria-educ.rar.html

     

    it's named  (Interfaces GSM - Montages pour téléphones portables  2e édition - ETSF) the english translation is (GSM Interfacing :schematic for mobilephone ,second edition).

  • Currently Being Moderated
    13. Jul 28, 2011 8:19 PM (in response to maqtech)
    Re: How to use GSM/GPRS module

    please send me the book he wants to interface gsm not work is the pdf endomage in my e mail nidou125@hotmail.fr

Related Content


Related Products
Discussions
  • Retrieving data ...

Bookmarked By (0)

Legend

  • Correct Answers - 50 points
  • Helpful Answers - 25 points