Skip navigation

community

460 Views 1 Reply Latest reply: Aug 27, 2011 10:42 AM by saturation RSS
Currently Being Moderated

Aug 26, 2011 10:06 AM

Does process really matter?

  1. 1.   What is a product process map?

  • A tool that visually represents the activities, connections and flows that are happening to a product, service or information as it moves through a process.

  1. 2.   Why use a product process map?

  • Organizes the information that was gathered during direct observation into a visual illustration of the current state of the process.  Meaningful improvements will only happen when you truly understand how the process really occurs currently.
  • To identify opportunities to reduce waste and non-value added activities.
  • To create a more efficient and streamlined process.
  • Make processes adaptable to change.
  • To identify the gap between the current reality and ideal state.
  • To establish high agreement on how the process currently functions and how it should function.
  • Enable learning.

  1. 3.   What factors are critical for product process map success?

  • The map is used in parallel with the activity map.
  • The map follows and focuses on the product, not the people.
  • Team directly observes and documents the activities, connections and flows of the process.
  • Team identifies the scope of the process to be studied and clearly defines boundary points.
  • Team identifies one common flow through the process and does not focus on exceptions such as ‘sometimes it does this.’
  • The map isn’t stagnant.  The process or product will often change and morph into another form over time.

Attributes

  • Currently Being Moderated
    1. Aug 27, 2011 10:42 AM (in response to Tom@Bbite)
    Re: Does process really matter?

    The larger the project the more it matters coordinating people, equipment and time.  Look at Firefox, how very complex its gotten; its process lists are public.  Likewise from spacecraft to a DMM, all are complex enough to require tracking methods that are independent of the people involved.

Related Content


Related Products
Discussions
  • Retrieving data ...

Bookmarked By (0)