Skip navigation

community

496 Views 1 Reply Latest reply: Sep 8, 2011 4:46 PM by Eavesdropper RSS
Currently Being Moderated

Sep 8, 2011 3:37 PM

Voltage Regulating in data acquisition project

In a data acquisition project I am currently working on, I have several IR sensors that require a strict 5V input (1.5mA supply current). The problem is that my DAQ recorder supplies ~5V (I measure around 4.8V usually) of unregulated voltage, which causes these sensitive sensors to go haywire.

 

What would be a more appropriate/simple/cheap/small packaging approach:

 

A) step up the 4.8V to a regulated 5V?
B) step down my 13V battery (which powers the rest of the systems) to a regulated 5V?
C) Other

 

In the case of B, would I need to protect my sensors from the powerful battery since they have such a small supply current?

 

Thanks.

Attributes

  • Currently Being Moderated
    1. Sep 8, 2011 4:46 PM (in response to sonikin)
    Re: Voltage Regulating in data acquisition project

    Welcome to element14!

     

    The IR sensors output an analog signal based on their readings. So, power them with their own source. Or, as you said in "B" regular the source 13V to what you need.

     

    Use some voltage regulators (easiest solution)

     

    A 7805 would do the trick.

     

    Alternatively, consider a second "off-the-shelf" regulated 5V power supply to add to your system. Many cell-phone chargers are 5V, so check them out.

     

    E

Related Content


Related Products
Discussions
  • Retrieving data ...

Bookmarked By (0)

Legend

  • Correct Answers - 50 points
  • Helpful Answers - 25 points