Load Google Translate Hello Orlando,
Can you suggest any sensors for Pulse Oximetry. will be helpful if all emitters and dectectors embedded in single chip
Thank U
Best regards
Orlando,
How can you choose the most electrically efficient LED easily? I spent a week going over hundreds of LED specs to calculate the results, and I do not plan to do this again when the next wave of new LEDs hits the industry.
Thanks ahead of time.
E
my kids are involved in FIRST robotics. This years parts box included 3 Allen-Bradley 42EF-D1MNAK-A2 line sensors. The kids' team would like to get a few more of these. Does newark.com carry these or the equivalent from another manufacturer?
Thanks
Jeff
Hello Orlando.
I need to buy an Incremental Optical encoder in order to control a DC motor.
I need it to be cheap and indeed i found some encoders but they all have mechanical "ticks" (like the feeling of a volume control in a digital radio used in any car) which make them suitable for dashboards but not to motion control.
all the "smooth spinning" encoders i found cost about or more than 100$.
Is there any cheap option (roughly about the same price than the "tick" encoders) in farnell or any other small quantities vendor?
The motor i'm talking about does not spin very fast therefore max RPM as well as PPR are not very critical parameters.
The supply voltage must be 5v or similar.
could you supply me also with a part number for a matching mechanical axis coupling?
Best Regards
hey,i have done 8x8 LED matrix but when i go for moving a string on matrix,one row goes very low light emmiting condition
and when i give derect ground to this row,i enlightens very efficiently.
can you tell me what may be the reason?
hi shivang, i think i understand your problem, but not sure what the best solution is.:
are your forcing the current from all 8 leds trough one resistor?
is so, you are increasing the voltage drop on that paticular resistor alowing less voltage for the leds to shine. in other words, you´re "choking the current".
the more leds turned on in one row, the less voltage each led will have. thus less current, less shine.
i would eliminate the resistor and connect directly to ground and relay on fast switching times to avoid excess current / led burnout.
in other words, turning leds on and off rapidly should do the trick, i started with on-times of .5ms and off-times of 100 ms and gradually increased the on-times to give more brightness.
like i said, this works, but not sure if it is the best solution.
"led matrix scan method on pic Assembler"
im trying to control a led matriz myself, pretty sucessfull so far. but im stuck!
i cant get the scan method to work on pic assembler. cant work out the algorithm. i even tried fooling around with the indirect adressing register.
i was forced to use the much less elegant "frames" approach. where i switch back and forth between "l" and " _ " frames to make a "L".
i know the scan method allows for near unlimited number of columns and i have seen examples of C, but i cant get it right on assembler. is it possible? or do i have to use C?
I need data sheet for IC OZ9981GN tanks I have many esquematics diagrams for tv I kan send tanks
© 2009 Premier Farnell plc. All Rights Reserved
Premier Farnell plc, registered in England and Wales (no 00876412), registered office: Farnell House, Forge Lane, Leeds LS12 2NE