10 Replies Latest reply: Oct 13, 2011 3:45 AM by Richard_H RSS

I'm confused about adding NETS

jeffm5457

I'm confused, should I be using the Wire command to connect components in the schematic or using the Net command. One tutorial says use wire, another says use net. I tried a small schematic using both and then converted the schematic to a board and all wire showed up. I guess I don't understand the difference. Any help would sure be appreciated because I think i am trying to make this more difficult that it should be.

Thanks,

 

Jeff

  • 1. AW: I'm confused about adding NETS
    rafetjos

    Net is for the electrical connection of parts, Wire is intended to draw

    graphical stuff like borders for a partial circuit etc. The name is

    ambiguous, also the layer 91 used for it.

    The behavior is different from Net, so try the following:

    open a sch

    add 3 resistors (see screenshot "wire-tool")

    use the Wire-button & connect R1, R2 & R3.

    You will see:

    no auto-junction, no auto-end of the wire, only 2x click will end the wire.

     

    Now use the Net-button & try the same (see screenshot "net-tool")

    You will see:

    auto-end of the net & auto-junction

    HTH

    r

     

  • 2. Re: I'm confused about adding NETS

    Am 11.10.2011 10:04, schrieb Ing. J.M. Rafetseder:

    Net is for the electrical connection of parts, Wire is intended to draw

    graphical stuff like borders for a partial circuit etc. The name is

    ambiguous, also the layer 91 used for it.

    The behavior is different from Net, so try the following:

    open a sch

    add 3 resistors (see screenshot "wire-tool")

    use the Wire-button & connect R1, R2 & R3.

    You will see:

    no auto-junction, no auto-end of the wire, only 2x click will end the wire.

     

    Now use the Net-button & try the same (see screenshot "net-tool")

    You will see:

    auto-end of the net & auto-junction

    HTH

    r

     

    Excellent explanation. Cadsoft should use it in the tutorial, with your

    permission of course

     

    --

    Mit freundlichen Grüßen / With best regards

     

    Joern Paschedag

     

  • 3. AW: I'm confused about adding NETS
    rafetjos

    THX,

    You have to learn this when teaching eagle in a technical school in austria

    ( if you are interested in other documents: www.htlwien10.at  schüler ->

    unterrichtsmaterial -> eagle -> dokumentation)

    r

     

     

  • 4. Re: I'm confused about adding NETS

    Element 14 User wrote on Mon, 10 October 2011 20:58

    I'm confused, should I be using the Wire command to connect components

    in the schematic or using the Net command.

     

    Always use NET to make schematic connections.

     

    The command names in Eagle are perfectly logical.  WIRE is used to draw

    lines except when they respresent wires, then you use NET.

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

  • 5. Re: I'm confused about adding NETS
    Richard_H

    Am 11.10.2011 14:11, schrieb Ing. J.M. Rafetseder:

    THX,

    You have to learn this when teaching eagle in a technical school in

    austria ( if you are interested in other documents: www.htlwien10.at

    schüler -> unterrichtsmaterial -> eagle -> dokumentation)

    r

     

    Hi R,

     

    wanted to check the lin kwww.htlwien10.at , but it does not work.....

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

      CadSoft Support -- hotline@cadsoft.de

      FAQ: http://www.cadsoft.de/training/faq/

     

     

  • 6. Re: I'm confused about adding NETS

    I'm also learning - I understand the explanation and agree that for

    electrical connections NET is more convenient with "Auto End" and "dot on

    junctions" but at the end of the project is there does not appear to be any

    electrical difference in fact if I draw a new wire by itself then another

    wire to connect into an existing NET it gives the option of using the new

    Net$ name or adopt the name of the N$n to which we are connecting.

     

    So in summary it would appear that if I had earlier in a project used wire

    then I don't need to go back & redraw as long as the N$n ar correctly

    connected.

     

    Well that it how I see it and welcome comment.

     

    This was an excellent question to be raised in the first place.

     

    --

    Regards

     

    Ray B

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

  • 7. Re: I'm confused about adding NETS

    On 10/11/2011 08:29 AM, Olin Lathrop wrote:

    Element 14 User wrote on Mon, 10 October 2011 20:58

    >> I'm confused, should I be using the Wire command to connect components

    >> in the schematic or using the Net command.

     

    Always use NET to make schematic connections.

     

    The command names in Eagle are perfectly logical.  WIRE is used to draw

    lines except when they respresent wires, then you use NET.

     

    touche! That's good, Olin.

     

    Jeff, Also be advised that CUT doesn't cut - it copies.

     

     

  • 8. AW: I'm confused about adding NETS
    rafetjos

    over the day it didn't work (server breakdown?) but now it works again. I'm

    sorry you cannot open the folders, they are at the moment only for teachers

    & students (login required). I'll talk to the webmaster maybe he can make a

    change.

    r

     

     

  • 9. OT AW: I'm confused about adding NETS
    rafetjos

    hi,

    now the server is ok, i checked it. no password required

    r

     

     

  • 10. Re: OT AW: I'm confused about adding NETS
    Richard_H

    Am 12.10.2011 21:06, schrieb Ing. J.M. Rafetseder:

    hi,

    now the server is ok, i checked it. no password required

    r

     

    Thanks for the info. There is really lot of information about

    EAGLE.... Well done, thank you!

     

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

      CadSoft Support -- hotline@cadsoft.de

      FAQ: http://www.cadsoft.de/training/faq/