Load Google Translate I have been looking for information regarding the Energy Related Products Directive. My business is fans and motors and I hoped I might be able to find out if there was a defined Specific Fan Power a motor/fan had to achieve. All I find is references to various exemptions and no facts. I am familiar with Building Regulations Part L2 which refers to SFP as Watts/Litres per sec. There are statements saying 50 or 60% of the motors commonly used today will be outlawed by new efficiency requirements but exactly how are they defined?
Hi,
I work at ebmpapst and we have a page that explains this including a download to read though. Have a read and if this helps.
http://www.ebmpapst-ec.co.uk/erp-2015-your-questions-answered
Thanks
Paul
We put this to our consultants, see below:
Paul
Thank you for taking the trouble to reply, This is an interesting document. It would be good to see a definable figure like SFP in the ErPD but maybe that will come.
Chris
Thank you for this document I am still working through it and to understand the concept of air power. SFP is litres of air per Watt so cannot easily have a conversion factor. It will be interesting to see what the Building Regulations Engineers make of it.
I've been looking at this too and from what I've read the legislation, whilst trying to address the amount of power wasted by inefficient motors, is based on being able to measure motor efficiency. So it seems that where a motor is assembled into a system that uses the motor output power for mechanical work, and where the motor can not be removed from this load and tested independantly, then it is exempt. I may be over generalising this though.
It makes sense to test only what can be tested....a gearbox that can not be removed will sap power and make the motor look less efficient, a fan will load the motor etc....and then you have invertors to drive motors at variable speed which are also not 100% efficient so variable drive motors that have intergrated controllers are also excluded!
So, in my interpretation only simple AC motors are included where they are a component that can function and be tested independently.
Surely the legislators (or I) have missed the point.
Hi Chris
From reading the reply's looks like this is a little more complex than it first looks. So I have spoken to Geoff Lockwood our Technical Director who is involved in these sorts of regulations all the time. He has forwarded me the following message to post that hopefully should help.
There is not a defined Specific Fan Power (SFP) target within the new Energy related Products (ErP) regulations for fans. The measure of SFP is not a term to define the efficiency of the fan it is a term that defines the energy consumption of a system related to a specific volume flow where a fan or fans are installed. The ErP is a directive that sets out to define the efficiency of many products (not systems), one of which is fans, and therefore uses the standard term of fan efficiency based on air power out divided by electrical power into the motor or drive. There is no cross reference from fan efficiency to SFP.
There is a Fan Manufacturers Association (FMA) guidance note, GN04, that gives explanation to fan efficiency and SFP - http://www.feta.co.uk/fma/downloads/FMA%20GN4%20Fan%20Efficiency-v2.pdf
Specific fan power is calculated by the equation Pe/V, where Pe is electrical power input in Watts and V is volume flow in l/s. So one way to reduce the SFP figure is to improve the impeller and motor efficiency and hence reduce the Pe value. But an alternative way to reduce the SFP figure is to reduce the resistance to the flow of air in the system; air power is volume flow times pressure loss, so keeping the same volume flow and reducing the pressure loss reduces the air power and a reduction in the air power leads to a reduction in power input and therefore a reduction of the SFP figure.
We find that the most significant way to reduce SFP figures is to ensure the fans are selected to operate at peak efficiency, are installed correctly (avoiding losses) and that the system loses are reduced through good system design. There is an joint FMA and CIBSE application guide that gives good advice - http://www.feta.co.uk/fma/fma-01.htm
There is a new International Standard, ISO12759 – fans – efficiency classification for fans, that has been produced to support the ErP regulations. This explains how the fan efficiency is calculated, relates it to the efficiency grades referred to in Annex I table 1 and 2, and gives worked examples. It has been approved by ISO members and is likely to be published January or February 2011. The FMA has already given some training to the industry and is likely to provide further advice via seminars.
The ErP fan regulations have been approved by the EU commission and are expected to be published this month.
Regarding the impact we, ebm-papst, believe about 30% of the products currently on the market will not meet the requirements, typically fans driven by low efficient shaded pole motors.
Regarding the comment ‘only simple AC motors are included’. Assuming that this comment refers to the ErP regulations for fans, then this is not a correct assumption. All electric motors types driving fans are within the scope. In general DC motors and EC motors easily exceed the limits. If the reference is to the ErP regulation for motors, then yes this is true and the EU has missed the point. Those regulations are for motors >0.75 kW and AC induction motors only.
I would like to point out that the fan regulations considers fans/motors with integrated drives/controls and gives them an advantage.
He has also told me that the ISO standard can be found here
And that it should also appear on the BSI site soon.
Thanks
Paul
Hi Paul,
Can you please tell me if this ErP directive affects mechanical power transmissions products like- bearings and couplings.
Are bearings and couplings within the scope of ErP directive?
Please reply.
Thanks,
Gaurav
Hi Gaurav
Not specifically but they could be part of something that is in scope such as a washing machine or a motor.
As you know the original scope was "any product that when in use, depends on, generates, transfers or
measures energy (electric, fossil fuel or renewable) although this maybe subject to future developments.
If you go to the menu at the top left of the legislation page you will find, under ErP, the October
E-Book covering this interesting subject.
Best wishes
Gary
© 2009 Premier Farnell plc. All Rights Reserved
Premier Farnell plc, registered in England and Wales (no 00876412), registered office: Farnell House, Forge Lane, Leeds LS12 2NE