Skip navigation

community

582 Views 6 Replies Latest reply: Jan 16, 2012 6:10 AM by RWM RSS
Currently Being Moderated

Jan 5, 2012 12:14 AM

can someone check the math on this one?

I had a real cool electronics "aha moment" this afternoon.  A package came from Amazon.com with a 16V 4A laptop power supply.        When I ordered it I had the impression that the output was AC.        Boy, was I surprised.  I need it to power a 315 MHz wireless home       security system which I had previously opened the enclosure and       inspected because it did not power on.  Turns out the wall       transformer was DOA.  That xfmr was hard wired to the main board       and there is an  fuse on the board.  I noticed that the 16V AC was       going straight into the board and that four fat rectification       diodes were sitting there.  So, I said: okay, that is a bridge       rectifier for converting it to DC and I observed some nice big       capacitors too - obviously the power supply.
So ,today, when the laptop power supply came and I looked hard at       the label, it was telling me 16V 4 amps DC with the center       positive on the barrel connector.  I frowned and my brain started       percolating like one of those old coffee pots.  I tested the       output voltage with a DVM and confirmed it was functional before doing the       Frankenstein routine on it.  It was fine.  So I proceeded to wire       the 16V DC output into the 16 V AC input and ... drum roll please       ...  it works great!   I even used wire nuts and shrink tubing.
So my question to you is "In your expert opinion, is this setup       stable for long term operation?" I have a  feeling that a 14 volt       4 amp
DC laptop       supply would work just as well.  Care to clue me in on the math?

Attributes

  • Currently Being Moderated
    1. Jan 5, 2012 5:46 AM (in response to billabott)
    Re: can someone check the math on this one?

    If this solution works now should work also long term. However, schematics would be interesting to check if power supply is adequate because 16V AC after rectification and filtering can reach about 20V DC (depends on load). 16V DC is slighty lower but I think this security system has some regulator because most security systems needs 12V DC.

  • Currently Being Moderated
    4. Jan 7, 2012 5:39 PM (in response to billabott)
    Re: can someone check the math on this one?

    Maximum charging current for this battery (8Ah) is 2.4A. In security systems battery acts as buffer (constant voltage charging) and power supply should have current limiter. If there was previously used 1.2Ah battery, circuit should limit current to about 0.4A. I think all should work until next battery change after 3-5 years

  • Currently Being Moderated
    6. Jan 16, 2012 6:10 AM (in response to billabott)
    Re: can someone check the math on this one?

    I think this will work long time.

Related Content


Related Products
Discussions
  • Retrieving data ...

Bookmarked By (0)