Load Google Translate Can anybody help on this? For medium voltage applications, say 100V~ 600V, what is the benefit of using an electro-mechanical relay as opposed to electronic switches, either a thyristor/IGBT/MOSFET? Reliability, voltage isolation, safety issues? There are many advantages to using an electronic switch in terms of speed, avoiding spikes, power consumption, propensity to failure, cost, etc..? So would there be any reason to use an electro-mechanical relay over semiconductor based switches? Thanks so much.. BTW, the application does not involve switched mode power supply or anything that needs any speed in switching. I would really appreciate if anyone can help.
One reason you might want to use a relay is if the circuit being controlled needs to be electrically isolated rather than just being "off".
Electronic switches do not completely isolate and will allow a small leakage current to flow when they are "off".
Consider both relay/contactor and solid state in some designs - you have the best of both worlds.
Switch the relay with no/low current.
© 2009 Premier Farnell plc. All Rights Reserved
Premier Farnell plc, registered in England and Wales (no 00876412), registered office: Farnell House, Forge Lane, Leeds LS12 2NE