Skip navigation

community

1 2 3 4 5 6 Previous Next 6847 Views 86 Replies Latest reply: Apr 1, 2012 10:08 PM by dus_SL RSS Go to original post
  • Extreme Gratitude...I will follow up on this.

     

    Frank

    /*********************/

  • Hello Frank,

     

    Unless there is a very good reason to restrict your choice to Microchip parts you should also look at the motor control offering from TI and ST - both of whom offer a wide range of processors and motor control development kits and applications data.

    An ST solution would most likely be ARM Cortex based whereas TI's motor control stuff could be MSP430, ARM or C2000 DSP based.

    Very low operating power is not usually important in motor controllers (because the motor uses so much power compared with the micro !).

  • I'm using this in a temp control app (not motor control) and running off

    battery power.

    MSP430 from TI looks good...so does the PIC16F1823-I/P from Microchip.

    But the PIC16F1823-I/P has a full H-bridge output...MSP430 has PWM but not 4

    lines.

    I can still prog the MSP430 to do what I want, but its cumbersome.

    Frank

  • Paul, I was steering towards Microchip's PIC16F1823-I/P.

    It was a full H-bridge...but I'm actually going to use this in a

    temperature control app.

    Hence, switching between polarities (such as motor control) at a fast rate,

    is not going to happen. But I will switch polarities for temperature

    control...just 2 minutes apart

    (real big deadtime). I was going to program the delay via firmware.

     

    The only other option was using TI's MSP430 as I only needed a serial

    2-wire digital

    display...but coding the PWM outputs as a full bridge is cumbersome in the

    code.

     

    Frank

  • Hey Paul,

     

    I am starting out with Embedded "stuff" and I had a question. What's the deal with the various manfuactuers in terms of the chips? I want to design something that uses an ARM7 or above and I see that you can get the processor chip from Atmel, Philips, Samsung, etc.

     

    What motiviates a circuit designer to use one brand over another?

     

    Also, we would like to work in the .net MF environment. If you know of any procs that have a ported .mf framework, any insight would be appreciated. I looked at the other IDEs and don't really want to use assembly or an Embedded brand derivative of C for development. After like 8 languages, it gets crazy to go after more if you know what I mean.

     

    Many Thanks!

    Ed

  • You don't really give enough detail about the kind of work you plan to make any but the most general advice possible. Embedded covers everything from very simple (like a relay timer with 2 logic level inputs and 2 outputs) to very complex (like a network router or a Satnav).

    If you come back with a bit more detail I'll try to help.

     

    Regardless of the size of the job I would think very carefully about the .Net Micro Framework. I think it would be fair to say that this has not been the succes that MS hoped it would be (and they have "open sourced" it). There are very few ports and it looks far too resource hungry for simple applications. For applications which are more like an embedded PC I think you would probably be better off with WinCe (or Windows Embedded Compact 7 as we are meant to call it ) which would allow you to stick with Visual Studio type development tools and keep you in the mainstream of the MS eco system.

     

    The good news (if you go that way) is that modern (Cortex) ARM micros are programmed in standard C and the use of assembler is not required.

     

    Michael Kellett

  • Some information to consider:

    ARM Holdings

     

    "ARM Holdings is the world's leading semiconductor intellectual property  (IP) supplier and as such is at the heart of the development of digital  electronic products."

     

    "The ARM business model involves the designing and licensing of IP rather  than the manufacturing and selling of actual semiconductor chips. We  license IP to a network of Partners, which includes the world's leading semiconductor and systems companies."

     

    Take a look at the links below and the columns for Memory, Peripherals, & Embedded Interface.  These are all features in addition to the processor core.

    168 Product results found for “arm7”

     

    Also see this Wikipedia article.

    The .NET Micro Framework is currently supported on ARM architecture processors (including ARM7 and ARM9)

     

    For development tools please look here.

  • @Tech_Support

     

    I think Ed is aware that ARM are a nice bunch of jolly chaps. His problem is deciding which ARM licensee (if any) to buy chips from. I think we need to know more about his application before we give too much advice.

  • In my case, we buy a product manufactured by others and programmed by others per our spec. The device uses an ARM5 processor. We wanted to refresh and change a bunch of different things to "do it ourselves". So, on the surface, anything greater than an ARM5 in terms of feature-set, speed, etc. is better.

     

    Other than using ther standard IO (Analogs & Digitals; I need 12 analog inputs and 8 digital inputs with 8 digital outputs), we need to have ethernet (10/100) and at least one serial port. There is no external display requirement so we won't have to worry about that.

     

    Ultimately, think of the application as one where we are using a serial port to read/control the analogs and digitals of the proc and an ethernet port that allows the same along with a CLI and a small web server. There is more in terms of whats connecting to the analogs and digitals but until I can get this going, that part of the concept is moot. I can verify the values with a meter on the output and short the digitals to test the inputs.

     

    I get what you are saying about the .net CF. I see that it tends to take up a lot of overhead. My concern with going with a standard C implementation is everything has to be created from scratch. For instance, if I want a simple web server, I would have to decode the HTML and then respond back per HTML standards. With a .net implementation, it can handle the actual back and forth syntax for me.

     

    Are there C libraries available that handle that type of stuff that you know of?

     

    Also, if we went that route, what IDE would be used for Standard C?

     

    If we went with a WinCe implementation, does that require Microsoft licensing?

     

    Sorry for all the questions but I am trying to rapidly wrap my head around this.

     

    Thanks so much!

    Ed

  • Hello Ed,

    There are several ARM Cortex micro controllers which support the kind of IO and Ethernet you describe. You need to look carefully to see that the peripherals are good enough. ST, NXP and TI (Luminary) all offer potentially suitable devices. Some of the TI Cortex M3 parts have on chip ethernet MAC and PHY which can be good, NXP and ST parts need an off chip PHY.

    My experience is with the Keil(ARM) tool set which is quite pricey but works. You code in C but they offer libraries for a basic real time scheduler and very basic web support. You have spotted the gap in this approach compared with .net (or similar)  - once you get into serious web serving you are going to have  a lot to do yourself. It all comes down to volumes - if you are going to make tens of thousands it may well be worth the software effort to use a cheap micro - if the volumes are low then Wince (or similar) on a bigger processor makes more sense.

    I don't know enough about your application to call it one way or annother but I feel that if that web server thing might grow you could save yourselves a lot of grief with a big OS, on the other hand the micro controllers coded in C are much easier to deal with for simple IO.

    It's never easy ! (and if it was no one would pay you to do it)

     

    Michael Kellett

  • @Paul,

     

    The .net, for me, is because I already use about 6 programming languages daily. Adding one more has implications in terms of cost of the IDE, ramp up time in terms of using the IDE and the associated language requried, etc.

     

    I have explained the choice of ARM above; in short it's because of what's in our product already. Also, from what I have seen, it's the "in fashion" proc. Having said that, since I am just starting out, I want a proc that I can scale up or down as needed.

     

    I read your article (thanks for the link) and I agree that I don't want to go overboard on the proc if I don't need to. However, in my opinion, there are other factors than just what you are trying to physically do with the proc. For instance, if you create a design using a proc that totally fit your requirement but was in high demand and not easily available vs. one that was a bit more than you need and readlily available (at a small price difference), you may go with that, right?

Related Content


Related Products
Discussions
  • Retrieving data ...

Bookmarked By (1)