Skip navigation

community

277 Views 1 Reply Latest reply: Feb 8, 2012 6:00 PM by eric.lieser RSS
Currently Being Moderated

Jan 19, 2012 10:23 AM

RE: MOSFET IGBT Driver UCC27423

...  So to reduce part$ count, I thought it might be possible to have this driver chip with 2 output pins control 3 IGBT gates (normally full off) with output pinA and 1 IGBT gate (normally full on) with the output pinB.  It is my understanding that the gates are very high impedance so it might not make much difference to pinA if it controls one or three gates.  Has anybody done this successfully?  This is my first go around with IGBTs.

-  thanks.

Attributes

  • Currently Being Moderated
    1. Feb 8, 2012 6:00 PM (in response to billabott)
    Re: RE: MOSFET IGBT Driver UCC27423

    You are correct.  The gate is high impediance once the switch is on or off, but during the transitions there is current flow to charge/discharge the capacitance of the gate.  That's why you need a gate resistor between your driver chip and the discrete, to control the turn on/off speed.  Look a the spec sheet and you'll see that a smaller Rg results in faster switching (but more EMI). 

     

    So as to controlling 3 IGBTs with one driver output.  Yes it will work, but there may be issues with timing if that is critical in your circuit.  If the IGBTs are different, or the gate resistors are, then they will turn on/off at different speeds possibly causing problems.  Also if you are switching at very high frequency you need to make sure the driver chip can handle the power required. 

     

    If you're running below 10 kHz and all the IGBTs are the same, I would reccommend increasing the Rg from the spec sheet, but other than that it should work just fine.

Related Content


Related Products
Discussions
  • Retrieving data ...

Bookmarked By (0)