Load Google Translate Hi,
I need a PLCC which is compatible with this socket:
http://il.farnell.com/3m/8484-21b1-rk-tp/socket-ic-plcc-84way/dp/1183025
Basically I need the chip carrier to meet these requirements:
1) Number of pins: 84
2) Body size: 1.15inch X 1.15inch
3) Cavity size: 1.4cmX1.4cm (approximately 0.55inch X 0.55inch)
4) conductive bottom
5) Pitch spacing: 1.27mm (0.05inch)
Do you have an idea from where can I purchase 10 chip carriers like those?
Thanks,
Gilad Cohen
Just for clarification,
By noting "Conductive bottom" I meant conductive bottom of the cavity. The back side of the chip carrier suppose to be an insulator.
© 2009 Premier Farnell plc. All Rights Reserved
Premier Farnell plc, registered in England and Wales (no 00876412), registered office: Farnell House, Forge Lane, Leeds LS12 2NE