Skip navigation

community

6214 Views 13 Replies Latest reply: Feb 1, 2010 4:03 AM by Alistair Winning RSS
Currently Being Moderated

Jan 25, 2010 11:21 AM

Agilent U1253A Multimeter Video Review

The EEVblog page is here:

http://www.eevblog.com/2010/01/24/eevblog-56-agilent-u1253a-oled-multimeter-review-teardown/

 

Agilent U1253A

Attributes

  • Currently Being Moderated
    1. Jan 25, 2010 4:18 AM (in response to EEVblog)
    Re: Agilent U1253A Multimeter Video Review
    Top notch again Dave! There are about four people around me watching it now. Looks a really nice instrument, great measurement capabilities. Does the meter not work while its charging? I thought with a low battery life you'd want to be able to test while its hooked up
  • Currently Being Moderated
    2. Jan 25, 2010 4:55 AM (in response to EEVblog)
    Re: Agilent U1253A Multimeter Video Review
    Another good review.  Love the style and enthusiasm. Thanks!
  • Currently Being Moderated
    4. Jan 26, 2010 2:53 AM (in response to EEVblog)
    Re: Agilent U1253A Multimeter Video Review

    Thanks for the review - I didn't watch all the way until the end because once you had told us how it charged (through the measuring terminals so you can't use + charge) I decided it was a waste of space.

     

    An 8 hour battery life is bad enough but if you were caught short at least you would expect to use it plugged in - who can afford to loose an hour or so because a battery runs down !?

     

    The rattle, silly battery contacts, cheapo sockets and inaccessible fuses just add more poo to the ice cream !

  • Currently Being Moderated
    5. Jan 27, 2010 10:21 AM (in response to EEVblog)
    Re: Agilent U1253A Multimeter Video Review

    Yeah,  great review!

     

    Bottom line, I'd rather squint than change the batteries.  Esp for that kind of dough. :-)

  • Currently Being Moderated
    8. Jan 28, 2010 7:21 PM (in response to EEVblog)
    Re: Agilent U1253A Multimeter Video Review

    I have been writing up a review of the Altera Nios II Evaluation Kit, and these videos and responses have made me think quite a bit about what I have written, and the way I have written it. No videos for me I'm afraid (although I have done a few short silent videos of the product itself) but I think some editing is going to happen before i dare show it to the world.

     

    Anyway, I think the cause of all the commotion has been the shock at seeing how a modern piece of HP (Agilent) test equipment looks when compared to the 'old' stuff. I get the impression that all the engineering effort has gone into the fashionable software area and the hardware design has been farmed out somewhere. I don't care where something is made and designed, but the hardware design does look like it was done by inexperienced people who don't especially care about doing things the best way. It smacks of being a marketing-led product, rather like GM and Chrysler were, not engineering-led.

     

    One of my hates is the cheap squishy rubber buttons many manufacturers use. Perfectly acceptable on budget gear (heaven knows I have specced it myself) but not on quality stuff. Change those, do a bit of PCB re-design, put in a decent Li-Po battery that can run it for a working week (hey, if my cheap phone can have a battery like this, I'm sure this meter can) , get rid of the cheesy tunes is plays and put in a good fast continuity tester and they could charge a chunk more cash for it.

     

    How about adding an induction coupled charge/run dock powered by USB? They could run out the logger data that way without any spike problems. They could probably even charge $50 more for that too!

  • Currently Being Moderated
    9. Jan 29, 2010 4:00 AM (in response to Zad)
    Re: Agilent U1253A Multimeter Video Review

    Hi Mike,

     

    I wouldn't be too overawed at Dave's review, I'm sure he'll admit himself it does take practise to get to that type of standard. I'm sure our readers are interested in hearing about the Altera kit, what it does, and of course what it doesn't do than the actual presentation.

     

    We did do a RoadTest of the U1253A DMM in the Tech First Journal originally, and there are two reviews posted here, I'll link them here so people can maybe get another perspective, although I think they also backs Dave's thumbs up conclusion.

     

    http://www.element-14.com/community/thread/1528?tstart=0

    http://www.element-14.com/community/thread/1527?tstart=0

     

    Dave,

     

    Just a small point, but do you think you concentrate too much on the name? I know Agilent are huge, but if the DMM cost the same price and was unbadged would you have come to the same conclusion?

  • Currently Being Moderated
    10. Jan 29, 2010 7:58 AM (in response to EEVblog)
    Re: Agilent U1253A Multimeter Video Review

    Dave,

     

    I have to admit I was a bit surprised about the thumbs up initially, but on reflection I think I see your point, (more or less) on the whole the negatives aren't show stoppers, it still works, provides accurate fast readings is usable (for 6-8 hours) and brings some nifty additional features.

     

    I think the performance of the display outdoors is a little disappointing, it is after all a ruggedized handheld device, so field use would I presume be a large part of where you would expect it to get used. The battery life seems a bit of an issue, but I suppose 6-8 hours gets you through the average working day, and I guess if you get in to the habit of charging it in your down time, it's workable if not desirable. I assume you can also use a standard PP3 to get you out of a fix if the battery dies. Having read the manual briefly, looks to me like the things out of action while it charges, why not supply with two batteries and a separate recharger (ideally one that will work from the mains and a cigarette lighter socket).

     

    The rattles a bit of an oversight, maybe they should have used sprung connectors rather than cable, but if it really bugs you, you can pack it yourself, I notice the box you had for the U1253A was a little beaten up, I'm guessing it wasn't new, maybe it originally had a little foam filler to stop the rattle and someone's removed it.


    I was a bit concerned by the argument that a market leader is somehow entitled to the benefit of the doubt. Big guys shouldn't get an easier time of it, every manufacturer should be judge equally on the evidence avaible, they should either all get the benefit of the doubt, or none of them should.

     

    I'll be interested to see the review of the new meter, to see if any of the negative issues discussed in your review have been addressed. Will it still get a thumbs up if changes are just cosmetic and the negatives remain?

  • Currently Being Moderated
    13. Feb 1, 2010 4:03 AM (in response to EEVblog)
    Re: Agilent U1253A Multimeter Video Review

    Thanks for that Dave,

     

    I can see where you are coming from. It's just my opinion that things do change over time, and the market leaders need to stay at the top of their game to keep and improve their market share and profits. There are a bunch of no name manufacturers that are up and coming and Agilent has to see them as a challenge, because one day they will have a name if they can keep up quality and keep down costs.

     

    Showing my age now, but I remember in the 70s when made in Japan, or made in Hong Kong was another way of saying cheap and shoddy. Now our AV equipment, vehicles, white goods etc etc are almost all manufactured in these areas. When I was looking for a new TV recently I read a lot of magazines on equipment, and the highest rated 32" LCD TV was a Samsung. Who'd have thought 20 - 30 years ago that a Korean manufacturer would be the best quality TV manufacturer in the world, and the old western quality TV makers like Pye and Ferguson are defunct?

Related Content


Related Products
Discussions
  • Retrieving data ...

Bookmarked By (1)