Skip navigation

community

2317 Views 2 Replies Latest reply: Feb 23, 2010 12:04 PM by tbaldes RSS
Currently Being Moderated

Jan 26, 2010 7:22 AM

Real instruments or virtual?

National Instruments Releases Enhanced 6.6 GHz PXI  Express RF Modular Instruments

New RF List Mode and 300 Microsecond Tuning Time Significantly Improve  Measurement Speed

National Instruments introduced two new PXI Express RF modular  instruments for automated wireless device test. The NI PXIe-5663E 6.6 GHz vector  signal analyzer (VSA) and the NI PXIe-5673E 6.6 GHz vector signal generator  (VSG) significantly improve automated test times for a wide range of devices  that use the latest wireless standards including wireless local area network  (WLAN), WiMAX and GSM/EDGE/WCDMA. The instruments' new RF list mode feature  provides deterministic power and frequency sequencing functionality to help  engineers make RF configuration changes more quickly during a test.  Additionally, the new wide-loop bandwidth mode further improves measurement  speed by reducing local oscillator settling times down to 300 microseconds or  less.

 

 

 

 

 

 

 

 

 

I was just reading the NI press release above and was wondering how many engineers actually prefer virtual instruments, and how many prefer real instruments in their workspace? Are there any real differences in measurementcapability/price/features? Why would you choose one over the other?

 

I'm guessing Dave definitely prefers physical equipment, as when you've riipped one PC to pieces, you have done them all!

Attributes

  • Currently Being Moderated
    1. Jan 26, 2010 8:09 AM (in response to Alistair Winning)
    Re: Real instruments or virtual?

    I'm not sure it's question of prefer, virtual or (synthetic) instruments are really aimed at a different part of the market to bench instruments.

     

    Historically test systems were created using a collection of bench instruments which were equipped with some kind of programmable interface, typically GPIB (HPIB) all bundled into a rack. This is all well and good, but tends to result in a system which has a large foot, issues around long term support and other difficulties, such as keep the firmware on all these differing systems up to date. In addition there's is effectively a lot of repetition of capabilities, in terms of signal conditioning, samplers, detectors etc.

     

    What many people wanted (the DOD for example) was a system that would reduce the total cost of ownership, reduce develop and
    deploy time, reduce the physical footprint, reduce the logistics effort in terms of decreased spares, support systems and training, provide greater flexibility through systems that are interoperable among U.S. and allied services and Improve the overall quality of testing. (Agilent Technologies. (2006) Using Synthetic Instruments in Your Test System).

     

    In order to address this, companies like Agilent (formerly Hewlett Packard), National Instruments etc started to produce a range of instruments which leveraged off existing industry standards to create small form factor instruments typically in a card and cage form, VXI, PXI etc. These are not always complete instruments, many are effectively subsystems of an instrument, such that a system can be configured to be for example a spectrum analyser, or a network analyser via software control and switching of the signal paths, virtual instruments (HP's Modular Measuement Sysems is another example).

     

    Now on a bench, in an RD lab, you probably don't really want something like this. You don't want to invest in a card cage and have all your test equipment effectively tied together, you might want your function generator and scope to be in two different places for example, very difficult if there in the same PXI frame. Further more, if you just wanted an Arb or scope, having to buy a mainframe to house it in and power it is a lot of additional expense. LXi, which is a new(ish) standard for programmable instruments avoids this in much the same way as GPIB did, in that it is predominantly a LAN port on a standard bench instrument, so the instrument can be part of a system or not, but that just gets you back to the huge test systems consisting of discrete bench instruments (though you can of course mix discrete and virtual instruments should you so choose).

     

    So as I said at the begining the question isn't about prefer, it's about what are you going to be doing with it. If it's ATE machine on a production line or a support system on a trolley for an aircraft, you might prefer a synthetic or virtual instrument, if it's in the lab, almost certainly not.

     

    Incidentally, some virtual instruments are created by simply (more or less) removing the screen and keypad from an existing bench instrument design and putting it in a smaller box, but curiously even though your getting less, there usually more expensive, go figure?

  • Currently Being Moderated
    2. Feb 23, 2010 12:04 PM (in response to Alistair Winning)
    Re: Real instruments or virtual?

    Hi,

     

    virtual instruments - as far as NI is involved - doesn't necessarily mean hardware rather than software.

     

    NI has become market leader with it's unique graphical programming language G, which is heart of LabVIEW.

     

    The block diagramms (called virtual instruments) within the graphical programming language, LabVIEW,

    are the key to applications you've never dreamt of. NI's hardware portfolio - to be understood as I/Os - just completes their offer.

     

    Therefore "virtual" is just the programming, "real" is the hardware.

     

    Best regards

    Thomas

Related Content


Related Products
Discussions
  • Retrieving data ...

Bookmarked By (0)