Skip navigation

community

1 2 Previous Next 7273 Views 21 Replies Latest reply: Sep 19, 2011 9:42 PM by Luismasg RSS
Currently Being Moderated

Oct 8, 2010 9:27 AM

Have a question about LED Optoelectronics?  Ask me!

If you need help on anything technical relating to VCC or Optoelectronics products, please post your question here!


Don't forget to sign up for email notifications under the "Actions" box so you'll see when I answer your question.

 

OrlandoDiaz.jpg

Orlando Diaz

I have extensive experience with Electro-mechanical assembly as well as significant knowledge of optoelectronics.

 

If not already, you'll need to

login_exprt3.png or register_exprrt3.png

 


to ask your question.

Otherwise, click reply below.

Attributes

  • Hello Orlando

    I am constructing a visual light communication system for indoor communication. My transmitter is an RGB LED panel (50 LEDs for now am planning to make a bigger panel) mounted on the ceiling and serial data is modulated onto the LED light. The three colors in the LED are for creating three communication channels that can be separated by the use of color filters at the receiver. The receiver is placed at the table top about 2 m from the ceiling. I had been using a photo transistor that is part of a photo interruptor at the receiver side and displaying the data onto a computer. It is working fine upto 28800 bps but only after the light is focused by the use of a convex lens onto the detector so difficult when the receiver is mobile.

     

    I need a detector (photo diode or photo transistor whichever is better) that can give me some freedom in movement, the data rate of at least 14400 bps is enough for me. Could you suggest me a better option ?

     

    Your help is appreciated..

    Natasha

     

    P.S. The area of movement is round about a square of side 200 cm.

  • Currently Being Moderated
    3. Feb 10, 2010 11:03 AM (in response to Orlando_Diaz)
    Re: Have a question about optoelectronics?  Ask me!

    Hello Natasha,

     

    I think, if I understood your issue correctly, this is due to not having enough light hitting the detector. There are number of factors that can paly a role here, starting from beam angle of the LEDs. The gain setting on the detector can also paly a role. As a check, you can take the detector closer to the light source and see if that helps. If it is the amount of light that is not sufficient for the detector, this test will help. If it helps, you can find a detector that has the feature to set the gain of the internal trans imp. amp (amplify the light before processing) externally and have the issue solved. Avago Tech or TAOS will have RGB sensors that you can use. I hope this helps.

  • Hello Orlando

    Thanks for your suggestion. But the WEBENCH Designer does not have many photodiodes according to my requirement i.e. in visual range. Also it focuses on the design of amplifiers and ADC or DAC converters not the photodiodes.

    natasha

     

    P.S. I have attached  the system block diagram and the experimental setup in this post. I am transmitting text from a PC to another PC.

    Attachments:
  • Currently Being Moderated
    5. Feb 11, 2010 2:20 AM (in response to Muhinthan)
    Re: Have a question about optoelectronics?  Ask me!

    Hello Muhinthan

    I have attached the system block diagram and the experimental setup in this the post just before. If it is the issue of less light hitting the detector, will increasing the number of LEDs and using a detector with larger surface area solve the problem in some extent ?

    Thanks

    Natasha

  • Hi Natasha,

     

    I would start with taking the detector closer to the LEDs and see if that makes any improvements. Can you tell me what  LED are you using? Also, having a 2m distance between the source and detector makes me think that unless you have a very narrow view angle LED, it will be difficult to direct all the light to the detector without the use of some kinds of collimator. Let's start with what I have said and we can go from there.

     

    Muhinthan

  • Hallo Orlando,

     

    i'm a FSE at Farnell.

    So many times customers coming up with a question about a component they are currently investigating for.

    I still don't know a good portal to search ( and find ) components by specs. 

     

     

    I.E.   a customer is lookig for an   Infrared LED with high output  

            

                  -  roundabout   740nm

                  -  fast    <= 12-15ns

                  -  100mA

     

    any idea or suggestions ? 

     

     

     

    thx in andvance

     

    Cheers

     

    Goetz

  • Hello Orlando,

    I am looking for a high power (~45mW) LED with very short switching times (~12ns) like the "OSRAM SFH 4650", but with a wavelength smaller than 750nm.
    I can't find such fast LED with that wavelength. Do you know any?

    Thanks for your support,
    Sebastian
  • HI Orlando;

     

    I am trying to identify a small laser that I can use to position a small router tool or drill. Ideally the spot needs to be 1mm or less and adjustable focus between 10 – 20 mm. The machine chuck can accept 8mm diameter bits but we can manufacture our own holder. Would you be able to suggest a suitable part for this application?

    Thanks.

  • Hello Orlando

    I am looking for an 850nm optical receiver (ST connector) that has an output that changes state when the optical power received is below a threshold level. The thershold level must be adjustable. This is needed to monitor the optical link and detect if the link degrades due to aging or other fault. There is an IC that could fit the bill, the ML4622 but I don't seem to be able to find a supplier or any pricing information. can you recommend an alternative?

    Regards

    Nico

  • Hallo Natasha,

     

    which kind of "modulation" do you perform to get the data onto the LED current?

    Maybe you could increase the sensitivity by using a clever method of modulation.

    Are you using any kind of hand shaking?

     

    Greets Ingo.

  • Dear Orlando

     

    I would appreciate if you could give some advice on Fiber optic temperature measurement sensors and converters.   We are interested to know if Newark has any experience with these and what the pros and cons may be.

     

    We have applications in MV power electronics and these appear to give good isolation and reliable readings.

     

    Paul

  • Bonjour Orlando,

     

    Je travaille actuellement sur une tourelle laser pour la Coupe d'Europe de Robotique. En fait, un laser est installé sur un moteur, et tourne à une vitesse d'environ 10Hz.

    Mon probleme est la reception de ce laser avec un circuit simple (c'est un prototype, le circuit réel sera fait avec une photodiode et un circuit compliqué).

    Le laser illumine le phototransistor (mon choix actuel) durant 30 µs environ.

    Je dois détecter cette lumière (650nm) et faire un front montant en 5V.

    Connaissez vous un CI ou un circuit simple qui puisse m'aider ?

     

    Merci

    Cordialement,

    --------

    Hello Orlando,

     

    I am working on a turret laser for the European Robotic Cup. In fact, a laser is mounted above a motor and turn at about 10 Hz.

    My problem is to receive this laser with a simple circuit (it's a prototype, the real circuit will be made with a photodiode and a complicated circuit).

    The laser illuminates the phototransistor (my present choice) during about 30 µs.

    I have to detect this illumination (650nm) and make a 5V rising edge output.

    Do you know a IC or circuit that can help me ?

     

    Thank you

    Best Regards,


     


1 2 Previous Next

Related Content


Related Products
Discussions
  • Retrieving data ...

Bookmarked By (0)