0 Replies Latest reply: Dec 29, 2012 11:45 AM by mgmetrojim RSS

Configuring a WiPi when the WiFi network is not encrypted


How do I configure the wireless settings if my network does not use encryption?  I use MAC filtering to only allow devices to connect to my network.  I have followed the installation instructions and edited the interfaces file so that it now reads


auto lo


iface lo inet loopback

iface eth0 inet dhcp

auto wlan0

iface wlan0 inet dhcp

ssid cheescake


But this appears not to work. When booting it renames wlan0 to wlan1 (and I used ifconfig to get the MAC address of the WiPi device wlan1 so I can configure my router) but it fails with the lines


Cannot find device "wlan0"

Bind socket to interface : No Such Device

Failed to bring up wlan0.



What do I need to type in the interfaces file to configure my device please?