4 Replies Latest reply: Feb 4, 2013 3:27 AM by slave13 RSS

Battery Question

slave13 Level 2

Hello can someone help me with this question that i have about this battery that i got out of my UPS the battery(12v 7.2a) is dead and will not take a charge.I was wondering is this battery like the ones that are in laptops and power tool and flash lights with those 12 and 6 volt batteries or is it like the ones in a car?

  • 1. Re: Battery Question
    michaelkellett Level 15

    The battery from your UPS will probably be a sealed lead acid type (so not the same as laptop, power tool or car !) but before you replace it you must find out for sure. What does it say on it ? I have replaced the batteries in quite  a few low cost UPS with cheap lead acid batteries with no problems.

    Farnell don't sell really cheap lead acid batteries so in the UK I would go to Rapid Electronics - they do a range of "Haze" sealed lead acid batteries at £11.76 for a 12V 7.5AH part. You need to choose one that is the right chemistry and the right physical size. These batteries are not as good as the ones Farnell sell but are probably about the same qulaity as those fitted in a cheap UPS in the first place.

     

    MK

  • 2. Re: Battery Question
    slave13 Level 2

    ya it saids sealed lead acid battery and on a label it said that it is a sealed non spillable lead acid battery. so does that mean that if i was to try and open it i would probably end up getting burn from acid and i should just leave them alone and take them to the recycling place and let them deal with them. i have opened many of those laptop and power tool batteries with no problems.

  • 3. Re: Battery Question
    michaelkellett Level 15

    Do not open up a sealed lead acid battery  - there is nothing you can do in there except injure yourself.

     

    You should not open up lithium ion batteries either.

     

    Why would you want to ?

     

    MK

  • 4. Re: Battery Question
    slave13 Level 2

    i didn't mean the battery i mean the case that they are in, like laptop batteries are a case with batteries/cells attach to one another inside the case.