Load Google Translate Do you have a question about eXtreme Low Power? Please post your question here!
Don't forget to sign up for email notifications under the "Actions" box so you'll see when Rishi answers your question.
Rishi Vasuki
Rishi has been with Microchip Technology since 2001. He has experience in developing portable music players and designing a wide variety of embedded applications (audio, security, motor control, power supplies and smart sensor). His current focus includes PIC(R) XLP MCUs for eXtreme Low Power applications as well as Microchip's mTouch solutions using 8-bit PIC18 & 16-bit PIC24 MCUs.
If not already, you'll need to or ![]()
to ask your question. Otherwise, click reply below. |
Hi,
just wondering have you come acros this article http://www.techonline.com/learning/techpaper/220301083 ?
Is mentioned that Microchip nano XLP might not be having the lowest sleep current in some situation. Do give me your thoughts.
But of cos correct me if I am wrong.
Cheers
Edmund
Hi,
any opinions from anyone ?
Cheers
Edmund
Unfortunately Microchip do not manufacture these sort of devices , yes we could offer a small MCU and our MCP1630 MCP1630 to provide a regulated output but we have no solution to dropping from main voltage . Hope this helps ?
Mike
You are going to struggle with this:
Your spec requires a mains input 19.2W, 48V output supply with 95% efficiency and in a volume of 26.88cc with a very unfortunate shape.
Farnell have an XP Power part giving 25W a 85% efficiency (Part number 1580485) but the volume is 84cc. They have an open frame version (1580478) where you can see all the parts.
To meet your spec you will need to improve efficiency and get down to about 1/3 of the volume of a commercially availble part - it may be possible but it won't be cheap !!!
May I suggest you go back one step and tell us what you are trying to do - perhaps a bit of lateral thinking may help solve your problem.
Hi,
Not sure whoom to ask.
We ordered one of My Passport Essential Ultra-portable hard drives (320GB) for one of our Mac computers. However this hard drive was not working and after scientist complained we tried to run test this on PC. However our PC cannot recognize the hardware and sometimes won’t even react when we plug in the Hard drive. I’m testing it now. The light appears to switch on and there is movements in the case but no pop up window or any message that HD was connected to computer. I was looking for driver on the internet but I can not find any. I was thinking if this might be error in firmware. Is there any link I could try to update it?
Many thanks,
Michal
Hi,
I believe this WD external drive is not Mac compatible. You may need their newest version that is.
Here is the website for details: http://www.wdc.com/en/
Regards, Mel
Hi,
I am considering a DSPic for a grid tied inverter. The inverter has a 400VDC input (input source solar DC/DC converter). Is the DSPic ever used for such an application? I know it has been used for AC induction motor control and AC/DC power supplies. My application will be a mix of both application. Grid Inverters have similar control loops (park - clark vector transformations) as motors and same circuits (full bridge) as power supplies. If anyone has information on the use of DSPic for these devices please share.
Best regards,
Enrico Migchels
Hi Enrico,
There are 2 keys application targets in dsPIC30/33 families :
* MOTOR control (references with "MC" at the end like DSPIC33FJ256MC710A-I/PF. DSPIC33FJ256MC710A-I/PF. : http://www.microchip.com/dscMOTOR
* SMPS & energy conversion (references with "GS" at the end like dsPIC33FJ64GS610 http://www.microchip.com/SMPS . On this previous link you should find the information you're looking for.
There are several applications notes showing implementation of Parke & Clarke transformation (Vector control).
I recommend the use of dsPIC33 dsPIC33 family which is more powerful (40MIPS) than dsPIC30 dsPIC30 and especially some devices have on-chip DMA which reduces CPU load as peripheral read / write dual PORT RAM without CPU assistance.
You may also want to ask precise questions on Microchip dsPIC dedicated forums : http://www.microchip.com/forums/tt.aspx?forumid=178
regards
Hi Rishi,
I wanted to know if you had any experience using MPLAB and the Pickit family of low cost programmers under Linux? Does Microchip have any plans to port MPLAB to Linux and Mac?
I was considering going from Windows to Linux permanently and I just wanted to make sure I could still run MPLAB to program my Dspics. I'm currently running the latest version of Ubuntu 10.04 Lucid Lynx.
Thanks for your time.
Regards,
Jorge Garcia
Hi Rishi....
I have a fishing boat that I can steer electronically: if A is logic high, the boat turns slowly to port; if B is high, it turns to starboard; if both are the same (high or low) the pilot motor stops. But I want to rig it as fully hands-off. I am looking at an angular rate sensor gyroscope. Isn't there some way that I can use it to provide the logic to hold the boat on a steady heading? I have all the servo parts working fine. Many thanks for your help, or, if I have attacked the wrong expert, can you shift this problem to another one....
Bruce
Dear Rishi,
Im final year student and doing a project for button detection.
I want to program PIC18F452 PIC18F452 using mlab version 8.3.3 and CSS C- compiler.
Actually Im beginner.
What should I do?
Could you teach me and give me a basic example to make sure that I already used the right software and compiler.Im really blurr about that.
Thank you for your help.
Hi Saara....
I have Sure Electronics dual-axis magnetic sensor module with UART and I²C interface. Can you recommend a µcontroller or processor to use with it to develop a magnetic compass project?
Many thanks...
Bruce Matthews
831 484-9006
© 2009 Premier Farnell plc. All Rights Reserved
Premier Farnell plc, registered in England and Wales (no 00876412), registered office: Farnell House, Forge Lane, Leeds LS12 2NE