Load Google Translate TDK-Lambda LS100-12
- Excellent housing and heatsnik, strong and easy to mount. Easy to open. Good cooling
- At first look I thought I'll find something loose inside but was L6 and L8 - small ferrite rings.- Good quality components (Rubycon MXG and YXH capacitors...)
- 3 year warranty
Some tests:
| Param. | Specs. | Found |
|---|---|---|
| Out Voltage Range | 10,8-13,2v | 9,2-14,3v /4,5A |
| Load Regulation | 96mV | 100mV @ 8,6A, 10mV@4A |
| Short circuit test | max 30s | 5s, 10s .... ok |
Noise: with 8,5 - 5 - 4,5 - 3,5A no noise, with 110mA - some noise. Still searching...
A very good product at a fair price.
Thanks for ... opportunity and PSU.
I agree with Danteo. Good power supply at a fair price.
I am away from home most of the time so I have been using it as a "portable" prototyping power supply for my personnal projects for about two weeks now. I take it with me in my suite case with the parts I need. It is pretty light weight for the rated output and came with a nice little box I use to protect it while travelling. The only thing is I don't have a portable oscilloscope si I didn't check the load regulation. I am working on a project with microcontrollers and power LEDs so the 8,5 amp capacity is very interesting. I didn't take it to more than 2 amps yet, but I sure will!
It makes it possible for me to work on projects I have been delaying for a long time because of the lack of time. For the price, I should have bought it before!
Mario
After more than 1 month from the first power-on:
- stable voltage
- no excessive heat
- no problems after short-circuits
- no problems after long no-load time
A good, reliable power source.
© 2009 Premier Farnell plc. All Rights Reserved
Premier Farnell plc, registered in England and Wales (no 00876412), registered office: Farnell House, Forge Lane, Leeds LS12 2NE