Skip navigation

community

Energy Micro

10 Posts tagged with the energy tag
0

Atollic TrueSTUDIO for ARM C/C++ development tool now supports the Giant Gecko and Leopard Gecko series of ARM-based microcontroller devices from Energy Micro, including 160 devices in the Tiny Gecko, Gecko, Giant Gecko and Leopard Gecko families.

 

http://www.energymicro.com/news-technical-archive/atollic-truestudio-for-giant-and-leopard-cortex-m3

Atollic_TrueSTUDIO_EFM32_Gecko.jpg

Atollic TrueSTUDIO is a world-class development and debugging tool that offers a state-of-the-art editor, an optimizing C/C++ compiler and a multiprocessor-aware debugger with real-time tracing. The tool suite delivers a leap in software development team collaboration and developer productivity, and offers advanced features including ARM build and debug tools, system analysis and real-time tracing using Serial Wire Viewer (SWV) technology, and graphical-UML diagram editors for model-based design and architecture.

0

Energy Micro software tool takes the guesswork out of battery life predictions

Read the full story here!


 

Called the energyAware™ Battery Estimator, this free tool provides a full simulation of total system energy usage, that takes into account actual battery source, MCU energy modes, peripherals employed and external circuit components. In simulation mode, system battery voltage output is displayed against time (years) in graph format, with the battery capacity rating (mAh), average MCU current consumption (µA) and estimated system operating time (years) shown numerically alongside. The set-up of a complete system simulation, its energy modes, their related operating times and associated peripheral functions and external component current consumption is via an intuitive GUI, comprising simple drop-down menus, slider bars and checkboxes. Battery Estimator can today model the performance of the seven most popular battery cell types, arranged in single cell or user-defined multiple cell series- or parallel-connected configurations. The tool allows the selection and analysis of all five energy modes of the EFM32 Gecko MCU used with the complete range of low power peripheral functions available as well as high frequency and low frequency clocks. The facility to factor in the current consumption from any external power hungry components, such as LCDs or speakers for example, further increases the accuracy of the battery life prediction.
0

The new EFM32 Giant Gecko development kit includes J-Trace, Geckos used in Electronic Paper Displays, EFM32 development on Linux

This episode contains a sneak peek at the new Giant Gecko development kit which at less than 350 dollars has all features you could think of, including enhanced debugging with built in SEGGER J-Trace.

We also look at an electronic paper display application and the new Linux tools for EFM32.

http://energymicro.com/company/newsletter

0

Energy Micro adds 12 devices to its Cortex-M3 microcontroller range for energy friendly applications

Oslo, Norway, July 12, 2011 – Energy Micro, the energy friendly microcontroller company, has announced availability of its EFM32 Gecko and Tiny Gecko product lines in a QFP64 package. The new 64-pin devices are particularly popular in the growing smart metering market, in addition to energy sensitive applications like building automation, security systems and portable health and fitness equipment.

The introduction of the larger I/O count package adds 12 new product variants to the company’s ARM® Cortex™-M3 based microcontroller portfolio. The EFM32G232, EFM32G842, EFM32TG232 and EFM32TG842, which are available in various configurations of Flash memory ranging from 8 to 128 KB and RAM from 2 to 16 KB, offer the same energy saving Gecko technology as other package options in the EFM32 MCU range. In application benchmark tests, this low current performance, combined with a wake-up time of 2µs has enabled the EFM32 microcontrollers to extend battery cell life by a factor of at least four.

Designed to significantly reduce current consumption, the EFM32 Gecko and Tiny Gecko microcontrollers operate in active mode typically 160µA per MHz executing code from Flash, 900nA in deep sleep mode and 20nA in shut off mode. The EFM32 Tiny Gecko family now also features the LESENSE low energy sensor interface, which enables autonomous monitoring of up to 16 external sensors in the microcontroller’s sub microamp Deep Sleep mode.

Andreas Koller, VP of World-Wide Sales and Marketing at Energy Micro said, "We have responded to the needs of our customers, and the introduction of the new QFP64 devices give engineers even more choices for applications where energy efficient design and proven packages are critical."

EFM32 Gecko and Tiny Gecko microcontrollers in QFP64 are available now and pricing starts at $1.49 each in 100k quantities. Technical data is available via Simplicity Studio, Energy Micro’s new online software console.

http://cdn.energymicro.com/web/press/EM061_QFP64/EFM32_Tiny_Gecko_QFP64.jpg

0

Energy Micro has announced advance details of its forthcoming energy friendly radio (EFR®) product family. Complementing the company’s EFM®32 Gecko microcontrollers, EFR4D Draco high performance radio solutions will consume only 25% of the energy of competing products. Based on an ARM® Cortex™-M0 core, Draco system-on-chip (SoC) radios will achieve receive and transmit current consumption as low as 5mA and 6mA respectively.

To maximise design flexibility, the EFR4D Draco product family will be offering users 3 alternative and cost effective radio device implementations:

  • transceiver only, supported by EFM32 for protocol stack and user application;
  • combined transceiver and protocol stack, supported by EFM32 for user application; and
  • complete SoC solution, integrating transceiver, protocol stack and user application in a single EFR4D.

 

The radio performance of the EFR4D products will also be higher than existing alternatives, with a maximum output power of +17dBm at 868MHz for example, receive sensitivity of typically -121dbm, FSK 1.2kbps and high receiver selectivity, blocking and image rejection capability. EFR4D will also be handling more frequency bands and radio protocols than competing products. The products will span the complete RF spectrum between 167MHz and 2500MHz and will support the industry’s broadest range of radio protocols, including IEEE 802.15.4, Bluetooth LE and Wireless M-Bus. EFR will also readily suit customers’ proprietary protocols. More information at www.energymicro.com

 

EM050_EFR1.jpg

0

Energy Micro is to extend the reach of its ultra low power EFM32 Gecko microcontroller family with the introduction of an ARM® Cortex-M0™ based product line and has improved the low power performance of its forthcoming Cortex-M3™ based Tiny Gecko devices. The new introductions will boost the company’s Energy Friendly Microcontroller portfolio to more than 100 products.

The Cortex-M0 based Zero Gecko microcontroller line of 20 new products will provide Energy Micro’s lowest cost energy friendly microcontroller solution. Pin and software compatible with the companion M3 based products, Zero will also achieve the same four times improvement in energy consumption when compared to alternative M0 based microcontrollers.

Scheduled to enter volume production during Q2’2011, the bigger M3 based Tiny Gecko microcontroller product line now being sampled by customers is achieving a current consumption performance of 160µA per MHz. This improves on the previously announced figure, and is due to enhancements in energy aware design techniques and chip architecture.Further information is available at www.energymicro.com/products.

EM049_Zero_Tiny.jpg

0

Energy Micro news

Posted by energymicro Aug 5, 2010
Energy Micro appointment drives sales
On August 3rd 2010 Energy Micro announced the appointment of Jürgen Hoika as VP Sales for Europe, Middle East and Africa (EMEA). Jürgen Hoika joins Energy Micro from Infineon Technologies, and his extensive market knowledge and proven customer focus will help boost Energy Micro's presence in Europe and inspire even more customers to discover how EFM32 Gecko microcontrollers can support whole new generations of energy sensitive products. Read more here.

Energy Micro targets South Asia Pacific with Apps-Connect appointment
On August 5th 2010 Energy Micro announced Apps-Connect as a distributor for its growing family of ARM® Cortex™-M3 based low power EFM32 Gecko microcontrollers in the ASEAN region and India. Read more here.

Energy Micro signs distribution agreement with RTI in China
On July 29th 2010 Energy Micro announced RTI Holdings as a distributor in Hong Kong and the People's Republic of China. RTI will distribute the complete family of ARM® Cortex™-M3-based low power EFM32 Gecko microcontrollers. Read more here.

Energy Micro is a finalist in the e-Legacy Awards
Energy Micro has been named one of the finalist in the Environmental Design category in the annual e-Legacy Awards. The winners are selected via a public on-line vote, and Energy Micro would appreciate your vote!

 

 

Upcoming EFM32 events
Meet Energy Miro at the following events and get more information about the EFM32 microcontrollers:

 

AVNET MEMEC TECHTOUR 2010
  • 14.09.2010 - Berlin
CODICO MIKROKONTROLLER SEMINAR 2010
  • 27.09.2010 - Zurich
  • 28.09.2010 - Stuttgart
  • 29.09.2010 - Frankfurt
  • 30.09.2010 - Nuremberg
  • 01.10.2010 - Wien
  • 08.11.2010 - Munich
ESC Boston 2010
  • 20.- 23.09.2010 - Hynes Convention Center - Booth Number 601
Electronica, Germany
  • 9.- 12.11.2010 - New Munich Trade Fair - Booth Number A4.349

 

energyAware Designer

The energyAware Designer contains functionality that aids, visualize and generate code templates for the EFM32 microcontrollers pin configuration. See the Designer video here.

 


Do you want to work for Energy Micro?
We continue to expand our dedicated EFM32 team, and are looking for the following persons:
  • Regional Sales Manager
  • Field Application Engineer
  • RF and Analog Design Engineer
  • Software Engineer
  • Test Engineer
0

The free energyAware Designer from Energy Micro makes microcontroller design easy!

 

The energyAware Designer contains functionality that aids, visualize and generate code templates for the low-power EFM32 Gecko microcontrollers. This makes it a breeze to resolve pin configuration conflicts and generate reports for documentation.

 

Download the free energyAware Designer http://www.energymicro.com/downloads/...

 

EFM32 Gecko microcontrollers are the world's most energy friendly microcontrollers, and are based on the 32-bit ARM Cortex™-M3 devices from Energy Micro. More information athttp://www.energymicro.com

 

0

Oslo, Norway, July 19th, 2010 – Energy Micro®, the energy friendly microcontroller company, has announced details of its EFM®32 Giant Gecko microcontroller family. For energy sensitive applications with high memory requirements, the 32-bit Giant Gecko (GG) will provide Flash configurations up to 1024KB with the added option of embedded USB connectivity.

 

There will be 48 EFM32GG microcontrollers offering a choice of 64, 128, 256, 512 and 1024 KB Flash memory blocks and a RAM of 32KB or 128KB. The microcontrollers’ pin and software compatibility with the existing Gecko product family means designers can develop products using the existing Gecko microcontroller and migrate to Giant Gecko when the higher memory parts enter production. Package options will include QFN64, QFP100 and BGA112.

 

Built around the energy-efficient ARM® Cortex™-M3 processor architecture, the Giant Gecko, Gecko and Tiny Gecko microcontrollers demonstrate an energy usage a quarter of that of alternative 8-, 16- or 32-bit microcontrollers. With a wake-up time of just 2µs and current consumption of 180µA per MHz executing code from Flash, 900nA in deep sleep mode and 20nA in shut off mode, the microcontrollers are proven capable of extending typical battery life by 300%.

 

The Giant Gecko’s embedded USB connectivity option will be USB2.0 compliant at full speed (12Mbit/s), integrating 2KB endpoint buffers and handling up to 10 endpoints. It will provide support for USB host and on-the-go configurations as well as bootloader over USB. Additional extended communication options offered by Giant Gecko will include dual I2C and up to 5 USART/UART serial interfaces.

 

Giant Gecko will feature the same selection of energy-saving peripherals as the companion Gecko and Tiny Gecko products. These include: an 8-channel, 12-bit ADC using 200µA at full resolution and 1Msamples/sec conversion rate, a 4x40 segment LCD controller using 900nA and a special Low Energy UART consuming just 100nA at 9600baud. In addition, for wireless encryption/decryption duties, an 128/256-bit AES accelerator block is also provided.

 

VELUX A/S, one of the strongest brands in the global building materials and home improvement industry, is a lead customer of the EFM32 Giant Gecko Microcontroller family. Bjarne Ravndal Andreasen, R&D manager at VELUX A/S said, “We have already successfully used the EFM32 Gecko Microcontroller in some of our electronic products. The EFM32 Giant Gecko family with 1MByte of Flash memory and full speed USB functionality will enable us to use EFM32 low energy microcontrollers in a wider range of electronic VELUX products.”

 

The EFM32 Giant Gecko from Energy Micro will begin sampling in Q1’2011 and pricing will start at $2.5 USD each in 100k quantities. Detailed datasheets on the Giant Gecko will be released November 1st 2010. Further information is available at www.energymicro.com.

 

For further information and reader enquiries:

 

Øyvind Borgan, Energy Micro AS, PO Box 4633, Nydalen, N-405 Oslo, Norway

o.borgan@energymicro.com

Tel:+47 23 00 98 00
Fax:+47 23 00 98 01
www.energymicro.com

 

For further information or to discuss feature article opportunities:

 

Rob Davies, Publitek Limited, 18 Brock Street, Bath, BA1 2LW, United Kingdom

rob.davies@publitek.com

Tel: +44 (0)1225 470 000
Fax: +44 (0)1225 470 047
www.publitek.com

 

About Energy Micro
Energy Micro develops, markets and sells the world's most energy friendly microcontrollers, based on the industry leading ARM® Cortex™-M3 32-bit architecture. The company was founded in 2007 by experienced semiconductor professionals with previous expertise from Chipcon, Texas Instruments, Atmel, Nordic Semiconductor. Energy Micro is backed by leading Nordic investors Northzone Ventures and Investinor. More information on Energy Micro is available at www.energymicro.com

 

About VELUX
VELUX creates better living environments with daylight and fresh air through the roof. Our product programme contains a wide range of roof windows and skylights, along with solutions for flat roofs.In addition, VELUX offers many types of decoration and sun screening, roller shutters, installation products, products for remote control and thermal solar panels for installation in roofs. VELUX, which has manufacturing companies in 11 countries and sales companies in just under 40 countries, is one of the strongest brands in the global building materials sector and its products are sold in most parts of the world. The VELUX Group has about 10,000 employees and is owned by VKR Holding A/S. VKR Holding A/S is a limited company wholly owned by foundations and family. www.velux.com

0

March 30 - April 1:Les Salons Solutions Electroniques, Porte de Versailles - Paris


Visit Via Design on stand C27 where you can see the energy friendly ARM Cortex-M3 EFM32 Gecko microcontrollers and development tools during the Les Salons Solutions Electroniques in Paris.