4 Replies Latest reply: Feb 12, 2015 4:02 PM by jeteste RSS

HPGL <-> Eagle conversion


Inkscape is great open source software (although it crashes frequently) which can import a bunch of formats including bitmap and DXF.

It can export into HPGL format, and the simple code below can be used to convert to Eagle script files.

I tried this with a DXF file from Solidworks and it worked well. Also it was possible to convert a bitmap image (Truetype

text) into line art using inkscape's 'trace bitmap' function, convert to HPGL and then convert to Eagle script format.

The code can be compiled using "g++ hpgl2eagle.c". To execute, type:

hpgl2eagle myinputfile.hpgl myoutputfile.scr


Source code is here because I have trouble uploading files to element14. If someone wants to enhance it or to generate an

executable and upload it somewhere that would be great (I tested on a MAC).

Hopefully one day someone can write an Inkscape plug-in that can import/export Eagle script files.