element14 adds 5 industry-firsts from Vishay Super 12 for applications in medical, CE and alternative energy
New series of P-channel MOSFETs, MEPIC and MELF resistors, and more, are available from element14 for electronics design and production
element14 has added several industry-first products to its portfolio of passives and semiconductors from Vishay Intertechnology, a world leader in discrete semiconductors and passive electronic components. The industry-firsts among the 2015 Super 12 include capacitors, resistors and MOSFETs and are suited for applications in the medical, consumer electronics, alternative energy, industrial, telecommunications, computing and automotive markets.
We offer a comprehensive portfolio from leading suppliers for customers who want the latest technologies for their product development and production. These industry-firsts from the Vishay Super 12 are among the world’s best products featured on our upgraded web site which makes reviewing, comparing and choosing products even faster and easier across the entire site.
The new series of p-channel MOSFETs, MEPIC and MELF resistors, and more from the Vishay Super 12 series are available from element14 for electronics design and production at http://sg.element14.com/vishay-super-12 :
An industry-first, polarized energy storage capacitor with high capacitance (up to 90 F) and the industry’s highest energy density (13 Ws/g), the Vishay 196 HVC ENYCAP™ series saves space as its low profile (2.5 mm) fits portable and compact designs.
The only E-field shielded IHLP® Power Inductor, the IHLE–4040DC-5A series of low profile, high current inductors handle high transient current spikes without saturation and are suited for engine and transmission control units, and LED drivers.
The Vishay MEPIC (Massive Electro-Pyrotechnic Initiator Chips) series of surface mount thin-film resistors is dedicated to pyrotechnic applications, and is the industry's first MEPIC resistor to be integrated on a PCB substrate to simplify the assembly process; available at http://sg.element14.com/2471609
An industry-first series of high-voltage SMD metal film resistors, the MMA0204 HV / MMB0207 HV high-voltage MELF Resistors with 500 V and 1000 V voltage ratings offers high-operating voltage up to 1 kV and high-surge capability up to 3 kV.
The Si7157DP features the lowest on-resistance for a p-channel MOSFET, down to 0.0016 ohms (max.), and is suited for applications with space constraints such as mobile computing, including as power management and load switching.
The 2015 Super 12 products provide a cross-section of Vishay’s very broad product portfolio. The Super 12 provide the industry-leading specifications that design engineers need to create new generations of end products. We are proud to partner with element14 as a preferred distributor for Vishay’s 2015 Super 12 products.
The Super 12 range is released annually by Vishay and consists of six semiconductors and six passive components which they perceive to be the best or first in the industry. Visit the Vishay Intertechnology store which carries over 40,000 products at http://sg.element14.com/vishay In addition, designers and professional buyers can participate in the world’s largest online community of engineers and electronics enthusiasts at http://www.element14.com/community/community/manufacturers/vishay
Farnell Global is a fast and reliable distributor of products and technology for electronic and industrial system design, maintenance and repair. From research and design through prototype to production, Farnell helps its customers access the products and services they need 24/7. With more than 80 years of experience, 47 localised websites, and a dedicated team of over 3,500 employees, Farnell provides every component its customers need to build the technology of tomorrow.
Farnell Global trades as Farnell in Europe, Newark in North America, and element14 in Asia Pacific. It also sells direct to consumers through its CPC business in the UK.
Farnell Global has been part of the established global technology distributor, Avnet (Nasdaq: AVT), since 2016. Today, this relationship allows the company to support its customers at every stage of the product life cycle, offering a truly unique distribution model, as well as expertise in end-to-end delivery and product design.
For more information, visit http://www.farnell.com/