Leeds,
20
June
2016
|
15:41
Europe/Amsterdam

element14 announces availability of NXP FRDM-KW40Z and USB-KW40Z to enable IoT projects

NXP FREEDOM development platform for kinetis kw40z30z20z.png

Global electronics distributor element14 today announces the addition of a new NXP® low-cost development platform to its extensive portfolio of products for the Internet of Things (IoT). The FRDM-KW40Z is enabled by the Kinetis® W series KW40Z/30Z/20Z (KW40Z) family and is ideal for applications in the IoT space, including home automation, building automation and healthcare.

Built on the ARM® Cortex®-M0+ processor, FRDM-KW40Z features an integrated 2.4 GHz transceiver supporting Bluetooth® Smart/Bluetooth®Low Energy (BLE) v4.1 and/or IEEE® 802.15.4standards. The kit contains two boards, enabling point-to-point, out of the box connectivity. Each board can be configured as a Freedom development board or as a Freedom shield for connection to a host processor.

The FRDM-KW40Z hardware is form-factor compatible with the Arduino R3 pin layout, providing a broad range of expansion board options. The FRDM-KW40Z also features a highly-sensitive, optimised 2.4 GHz radio with PCB F-antenna, which can be bypassed for connection to test equipment via SMA connection, multiple power supply options, push and capacitive touch buttons, switches, LEDs and integrated sensors.

The USB-KW40Z, also added to the Farnell element14 portfolio is the same development platform as the FRDM-KW40Z, but available on a convenient USB dongle form factor. The USB-KW40Z can be used as a Bluetooth® Smart/Bluetooth® Low Energy and/or IEEE® 802.15.4 packet sniffer or development board for optimal connectivity and efficiency.

The packet sniffers are essential for wireless network development, allowing over-the-air traffic monitoring, with the BLE and 802.15.4 protocols allowing the continued development of power efficient IoT applications, including BLE functionality in the health and fitness wearables. The 802.15.4 standard has been widely adopted as the premier ultra-low power, low-cost, mesh networking technology for home automation applications, with the possibility of more growth ahead due to increased adoption in commercial and industrial applications, such as lighting and building automation.

The growing demand for IoT applications is driving an increased need for development platforms that enable engineers to integrate low cost, low power network protocols into their designs. By introducing the FRDM-KW40Z and USB-KW40Z to our ever-expanding portfolio of IoT products and capabilities, we can give the engineering community access to the very latest technologies that will help them to push the boundaries of innovation in connectivity and IoT applications.
David Shen, Chief Technology Officer at Premier Farnell

The FRDM-KW40Z (priced from £126.80) and USB-KW40Z (priced from £59.39) are available from Farnell element14 in Europe, Newark element14 in North America, and element14 in Asia.

Get more details, downloads and participate in discussions on the element14 community.

Boilerplate

Farnell Global is a fast and reliable distributor of products and technology for electronic and industrial system design, maintenance and repair.  From research and design through prototype to production, Farnell helps its customers access the products and services they need 24/7.  With more than 80 years of experience, 47 localised websites, and a dedicated team of over 3,500 employees, Farnell provides every component its customers need to build the technology of tomorrow.

Farnell Global trades as Farnell in Europe, Newark in North America, and element14 in Asia Pacific.  It also sells direct to consumers through its CPC business in the UK.

Farnell Global has been part of the established global technology distributor, Avnet (Nasdaq: AVT), since 2016. Today, this relationship allows the company to support its customers at every stage of the product life cycle, offering a truly unique distribution model, as well as expertise in end-to-end delivery and product design.

For more information, visit http://www.farnell.com/