element14 expands exclusive range of ROHM automotive-qualified products
Over 250 ROHM products added exclusively to element14’s extensive automotive portfolio
element14 has expanded its portfolio of automotive-qualified products with the addition of over 250 new ROHM semiconductors. Exclusively available in-stock for same day dispatch from Farnell element14, the ranges include LSI, diodes, transistors and power management solutions, suited for the different automotive application segments.
To meet the increasing needs of digitisation in new automotive applications, ROHM is developing new products to deliver full system solutions. ROHM has strengthened its offering at Farnell element14 with ranges of products for use in applications including Automotive Cluster, Power, Head-up displays, Charger and Advanced Driver Assist Systems.
These are among the new ROHM automotive-qualified products available at element14:
- Ideal for automotive applications requiring a direct connection to the battery and low current consumption such as in the body, audio and navigation systems, the ROHM series of AEC-Q100 qualified LDO Voltage Regulators feature ultra-low quiescent current of 6μA (Typ.) and output current capability of 200mA.
- ROHM Silicon Carbide Schottky diodes feature a shorter recovery time and reduced temperature dependence, in addition to high-speed switching.
- The AEC-Q101 Zener single diodes from ROHM are compact; 2-pin mold high-density surface mount type, in SOD-523 (EMD2) package. Ideal for applications requiring constant voltage control, it can be mounted automatically using a chip mounter.
The new ranges of over 250 ROHM semiconductors are available from Farnell element14 in Europe, Newark element14 in North America and element14 in APAC.
Farnell Global is a fast and reliable distributor of products and technology for electronic and industrial system design, maintenance and repair. From research and design through prototype to production, Farnell helps its customers access the products and services they need 24/7. With more than 80 years of experience, 47 localised websites, and a dedicated team of over 3,500 employees, Farnell provides every component its customers need to build the technology of tomorrow.
Farnell Global trades as Farnell in Europe, Newark in North America, and element14 in Asia Pacific. It also sells direct to consumers through its CPC business in the UK.
Farnell Global has been part of the established global technology distributor, Avnet (Nasdaq: AVT), since 2016. Today, this relationship allows the company to support its customers at every stage of the product life cycle, offering a truly unique distribution model, as well as expertise in end-to-end delivery and product design.
For more information, visit http://www.farnell.com/