element14 is now stocking new high-performance power inductors from Panasonic Industry
Panasonic Industry Europe’s ETQP*M* Series of power inductors provide a high-quality design-in component for safety and efficiency in automotive applications such as, powertrain.

element14 is now shipping Panasonic Industry Europe’s (Panasonic) world-class high-performance ETQP*M* Series of power inductors designed for automotive, e-mobility and industrial applications.
The series is a significant addition to element14’s passive component portfolio and will help meet the growing demand for high power inductors. Customers can now accelerate new product development, reducing time-to-market while enjoying fast and reliable sourcing from element14.
The new power inductors will meet the increasing requirements for automotive safety measures, including advanced driver assistance systems (ADAS), steering control and braking systems. Automotive powertrain applications, such as engine and motor generators, drive train controllers and battery management electronic control units (ECUs) are also supported.
Panasonic’s new ETQP*M* Series are half the size of conventional ferrite technology inductors and 15% to 30% smaller than competitive iron core magnetic technology inductors on the market. The compact size and elegant design ensure easy integration to meet the current and power requirements of demanding applications. Moreover, a single inductor can often fulfil a wide range of power, current and mechanical requirements that would normally require many different components. The high-performance ETQP*M* Series can also help drive efficiency gains in manufacturing and industrial systems, with easy integration into factory automation applications and the design of collaboration robots (cobots).
Two market-leading products within the ETQP*M* Series, the ETQ-P5M470YFK and ETQ-P4M3R3YFN, are now available for fast delivery from element14. Key features include:
- High heat resistance: Operating temperature -40°C to +150°C (up to +180°C for short time), including self-heating
- High reliability: High vibration resistance is offered as a result of each product’s integral construction, designed to withstand the severe reliability conditions of automotive and other strenuous applications
- High bias current: Excellent inductance stability using ferrous alloy magnetic material
- Temperature stability: A variety inductance range of 0.33 μH to 100μH and offering excellent inductance stability
- Low audible (buzz) noise: The ETQP*M* Series features the new metal composite core technology from Panasonic Industry, suitable for filter, step-down and step-up circuits for DC/DC converters
- High efficiency: AEC-Q200 and RoHS compliant, the ETQP*M* Series offers low DC resistance of winding and low eddy-current loss of the core
Simon Meadmore, Vice President of Product and Supplier Management, at element14 says: “Automotive design is witnessing almost dizzying progress in the move to electrification. There is a clear trend toward more compact components which can save space, improve efficiency and reduce the weight of critical applications. Correspondingly, the demand for passive components such as power choke coils that can reliably withstand difficult automotive conditions is higher than ever – and it’s not only about construction toughness and heat resistance. The new ETQP*M* Series from Panasonic meets all of these key requirements for high-quality power inductors.”
Panasonic Industry Europe is driving industrial innovation, synergies and automation with an extensive range of business partners. Their portfolio of products and services includes components, devices, energy & building and automation. They service a wide range of industries including mobility, infrastructure, home & living, production & logistics and healthcare.
Panasonic Industry’s ETQP*M* Series of power inductors are available from stock at Farnell in EMEA and element14 in APAC.
About us
Farnell is a global technology leader with over 80 years in the high service distribution of technology products and solutions for electronic system design, production, maintenance and repair. Farnell uses this experience to support its broad customer base, from hobbyists to engineers, maintenance engineers and buyers as ‘The Development Distributor’, working with leading brands and start-ups to develop new products for market, and supporting the industry as it seeks to develop the current and next generation of engineers.
Farnell trades as Farnell in Europe, Newark in North America, and element14 throughout Asia Pacific. Farnell's global businesses are supported by a global supply chain of more than 3,500 suppliers and has an extensive inventory profile developed to anticipate and meet the needs of innovative customers everywhere. Farnell also sells direct to consumers through a network of resellers, and its CPC business in the UK.
Farnell is a business unit of Avnet (Nasdaq: AVT). Avnet is a global technology solutions provider with an extensive ecosystem that delivers design, product, marketing and supply chain expertise for customers at every stage of the lifecycle.
For more information, visit the website at http://www.farnell.com/corporate